<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8M-MINI internal RTC implementation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708337#M211163</link>
    <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;I do have an application where I want to use internal RTC of IMX8M-mini controller. I have used Yocto setup for the same.&lt;/P&gt;&lt;P&gt;Can you support how I can use internal RTC in my application&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Madhuri&lt;/P&gt;</description>
    <pubDate>Mon, 21 Aug 2023 12:02:46 GMT</pubDate>
    <dc:creator>AMBh</dc:creator>
    <dc:date>2023-08-21T12:02:46Z</dc:date>
    <item>
      <title>IMX8M-MINI internal RTC implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708337#M211163</link>
      <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;I do have an application where I want to use internal RTC of IMX8M-mini controller. I have used Yocto setup for the same.&lt;/P&gt;&lt;P&gt;Can you support how I can use internal RTC in my application&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Madhuri&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 12:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708337#M211163</guid>
      <dc:creator>AMBh</dc:creator>
      <dc:date>2023-08-21T12:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M-MINI internal RTC implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708431#M211170</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;DIV id="bodyDisplay_3" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;The MX8M Mini does not have an internal 32k ring oscillator,&amp;nbsp;and does not support the use of a crystal.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please see the datasheet, Section 3.1.4:&lt;/P&gt;
&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;
&lt;P&gt;The RTC_XTALI is used for low-frequency functions. It supplies the clock for wake-up circuit, power-down real time clock operation, and slow system and watch-dog counters. The clock input can only be connected to an external oscillator. RTC_XTALO should be directly connected to VDD_SNVS_0P8.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;and Section 3.4.2:&lt;/P&gt;
&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;
&lt;P&gt;An external 32.768 kHz oscillator is necessary.&amp;nbsp;&amp;nbsp; &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 21 Aug 2023 14:31:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708431#M211170</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-08-21T14:31:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M-MINI internal RTC implementation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708747#M211193</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply&lt;/P&gt;&lt;P&gt;Okay I got your point. I also used BD71847AMWV power management IC which has internal RTC. How to use it ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 05:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-MINI-internal-RTC-implementation/m-p/1708747#M211193</guid>
      <dc:creator>AMBh</dc:creator>
      <dc:date>2023-08-22T05:42:52Z</dc:date>
    </item>
  </channel>
</rss>