<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RMII interfaces on iMX93</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708295#M211157</link>
    <description>&lt;P&gt;which i.mx93evk do you use? 11x11, 9x9 or 14x14? as I known, 14x14 doesn't support RMII so far&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Aug 2023 10:43:03 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-08-21T10:43:03Z</dc:date>
    <item>
      <title>RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708217#M211141</link>
      <description>&lt;P&gt;The #iMX93 reference manual describes the RGMII interfaces supporting RMII operation but there is no concrete definition of the pinout of each interface in RMII mode.&lt;/P&gt;&lt;P&gt;Even searching through the pin mapping spreadsheet attached to the reference manual doesn't make it clear where the RMII clock and control signals appear.&lt;/P&gt;&lt;P&gt;Since we are using the iMX93 as an upgrade to a number of existing products we have to use RMII, it is not possible to change all our designs to RGMII.&lt;/P&gt;&lt;P&gt;Where can I find this information please?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 09:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708217#M211141</guid>
      <dc:creator>Gary_Aylward</dc:creator>
      <dc:date>2023-08-21T09:03:25Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708295#M211157</link>
      <description>&lt;P&gt;which i.mx93evk do you use? 11x11, 9x9 or 14x14? as I known, 14x14 doesn't support RMII so far&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 10:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708295#M211157</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-21T10:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708318#M211160</link>
      <description>&lt;P&gt;We are planning to use the Ka-Ro QS93 module which quotes i.MX9352. The Ka-Ro module brings out all the RGMII pins of both Ethernet ports but I can't find out whether the same pins are used when RMII mode is used.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 11:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1708318#M211160</guid>
      <dc:creator>Gary_Aylward</dc:creator>
      <dc:date>2023-08-21T11:07:49Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1711888#M211519</link>
      <description>&lt;P&gt;it seems imx93 doesn't support this so far, only Set eQOS to RGMII mode for 11x11 EVK&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx93-11x11-evk.dts" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx93-11x11-evk.dts&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 04:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1711888#M211519</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-28T04:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1712970#M211641</link>
      <description>&lt;P&gt;The iMX93 data sheet, IMX93IEC.pdf, Rev 1 04/2023 says:&lt;/P&gt;&lt;P&gt;Ethernet supports the following key features:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Support ENET AVB&lt;/LI&gt;&lt;LI&gt;Support IEEE 1588&lt;/LI&gt;&lt;LI&gt;Support Energy Efficient Ethernet (EEE)&lt;/LI&gt;&lt;LI&gt;1.8V/3.3V RMII operation, 1.8V RGMII operation&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think I've now found the solution buried in the datasheet, although it is not mentioned in the reference manual or the pin mapping spreadsheet attached to the manual.&lt;/P&gt;&lt;P&gt;Sections 4.12.2.1 and 4.12.3.1 define the signal mapping for RGMII and RMII mode for ENET2 and ENET1 respectively.&lt;/P&gt;&lt;P&gt;Hopefully this will be of use to someone else in the future...&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 08:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1712970#M211641</guid>
      <dc:creator>Gary_Aylward</dc:creator>
      <dc:date>2023-08-29T08:23:40Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1713664#M211704</link>
      <description>&lt;P&gt;yes, for pin mapping, you can refer to the data sheet, I thought you need set up this mode, current bsp doesn't support yet&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 04:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/1713664#M211704</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-30T04:00:17Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interfaces on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/2319268#M244072</link>
      <description>Thank god for you! Trying to get RMII working with the FEC port has been kicking my butt for weeks and IMX93IEC was the answer!</description>
      <pubDate>Wed, 18 Feb 2026 00:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RMII-interfaces-on-iMX93/m-p/2319268#M244072</guid>
      <dc:creator>davidpatton</dc:creator>
      <dc:date>2026-02-18T00:27:51Z</dc:date>
    </item>
  </channel>
</rss>