<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX93 and Linux BSP/eIQ for Automotive</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1707284#M211035</link>
    <description>&lt;P&gt;Hi Zhiming,&lt;/P&gt;&lt;P&gt;thank you for your reply. This was extremely helpful.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Aug 2023 06:34:14 GMT</pubDate>
    <dc:creator>ChristophF</dc:creator>
    <dc:date>2023-08-18T06:34:14Z</dc:date>
    <item>
      <title>i.MX93 and Linux BSP/eIQ for Automotive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1705442#M210871</link>
      <description>&lt;P&gt;I was given the task to clarify some basic questions regarding i.MX93 for the automotive market, that i was not able to clarify by the documentation, faq and the forums alone.&lt;/P&gt;&lt;P&gt;1. The i.MX93 is also marketed as an automotive variant, so is the NXP Automotive Linux BSP which is Automotive-SPICE (tailored for open source), IATF16949 and ISO9001 compliant, also available for the i.MX93?&lt;/P&gt;&lt;P&gt;2. I also saw that there is an ASPICE compliant automotive version of eIQ from NXP, is it possible to use this on i.MX93?&lt;/P&gt;&lt;P&gt;3. Is there any certification for i.MX93 for functional safety or is this processor just not the right pick for functional safety and we should wait for i.MX95 instead?&lt;/P&gt;&lt;P&gt;4. Is it possible to run the NXP eIQ inference engines for the i.MX93 on Linux only or could we choose to use a QNX or Autosar Adaptive instead and still run the eIQ inference?&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;P&gt;Christoph&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 06:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1705442#M210871</guid>
      <dc:creator>ChristophF</dc:creator>
      <dc:date>2023-08-16T06:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 and Linux BSP/eIQ for Automotive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1707127#M211019</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221733"&gt;@ChristophF&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Q1: It doesn't support&amp;nbsp;&lt;SPAN&gt;Automotive-SPICE IATF16949 or ISO9001 compliant.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Q2: No, the eIQ Auto only support S32 Automotive MCU/MPUs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Q3: No functional safety for i.MX93. Customer should wait for i.MX95 for functional safety.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Q4:&amp;nbsp;QNX or Autosar Adaptive will not support it. If customer can integrate the ethosu driver from Linux BSP, it's still possible to run ML models on NPU in systems.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Zhiming&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Aug 2023 02:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1707127#M211019</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-08-18T02:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 and Linux BSP/eIQ for Automotive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1707284#M211035</link>
      <description>&lt;P&gt;Hi Zhiming,&lt;/P&gt;&lt;P&gt;thank you for your reply. This was extremely helpful.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Aug 2023 06:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-and-Linux-BSP-eIQ-for-Automotive/m-p/1707284#M211035</guid>
      <dc:creator>ChristophF</dc:creator>
      <dc:date>2023-08-18T06:34:14Z</dc:date>
    </item>
  </channel>
</rss>