<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx-mkimage for building flash.bin for iMX93 u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1707045#M211017</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I can build the WIC file for the i.MX93 EVK using Yocto. I am trying now to build the flash.bin (u-boot) file for the same platform outside Yocto. Can anyone point out where to find the&amp;nbsp;imx-mkimage sources that will include support for iMX9?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to build successfully the u-boot.bin and related artifacts using u-boot source tree (&lt;A href="https://github.com/u-boot/u-boot.git)" target="_blank" rel="noopener"&gt;https://github.com/u-boot/u-boot.git)&lt;/A&gt;&amp;nbsp;with these commands:&lt;BR /&gt;make imx93_11x11_evk_defconfig&lt;BR /&gt;make&lt;/P&gt;&lt;P&gt;However, I am getting a Makefile errors when I try building the flash.bin:&lt;BR /&gt;make flash.bin&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;make[1]: *** No rule to make target 'u-boot.cnt'. Stop.&lt;BR /&gt;make: *** [Makefile:1520: u-boot.cnt] Error 2&lt;/P&gt;&lt;P&gt;Any idea how to build a single flash.bin, with no Yocto support, so it can be deployed to an eMMC or an SD.&lt;/P&gt;&lt;P&gt;Any input appreciated.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Thu, 17 Aug 2023 21:22:36 GMT</pubDate>
    <dc:creator>abt</dc:creator>
    <dc:date>2023-08-17T21:22:36Z</dc:date>
    <item>
      <title>imx-mkimage for building flash.bin for iMX93 u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1707045#M211017</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I can build the WIC file for the i.MX93 EVK using Yocto. I am trying now to build the flash.bin (u-boot) file for the same platform outside Yocto. Can anyone point out where to find the&amp;nbsp;imx-mkimage sources that will include support for iMX9?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to build successfully the u-boot.bin and related artifacts using u-boot source tree (&lt;A href="https://github.com/u-boot/u-boot.git)" target="_blank" rel="noopener"&gt;https://github.com/u-boot/u-boot.git)&lt;/A&gt;&amp;nbsp;with these commands:&lt;BR /&gt;make imx93_11x11_evk_defconfig&lt;BR /&gt;make&lt;/P&gt;&lt;P&gt;However, I am getting a Makefile errors when I try building the flash.bin:&lt;BR /&gt;make flash.bin&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;make[1]: *** No rule to make target 'u-boot.cnt'. Stop.&lt;BR /&gt;make: *** [Makefile:1520: u-boot.cnt] Error 2&lt;/P&gt;&lt;P&gt;Any idea how to build a single flash.bin, with no Yocto support, so it can be deployed to an eMMC or an SD.&lt;/P&gt;&lt;P&gt;Any input appreciated.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 21:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1707045#M211017</guid>
      <dc:creator>abt</dc:creator>
      <dc:date>2023-08-17T21:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: imx-mkimage for building flash.bin for iMX93 u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1707993#M211102</link>
      <description>&lt;P&gt;the imx-mkimage is from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/imx-mkimage/tree/lf-6.1.22_2.0.0" target="_blank"&gt;https://github.com/nxp-imx/imx-mkimage/tree/lf-6.1.22_2.0.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;pls refer to the chapter 4.5.13 How to build imx-boot image by using imx-mkimage&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 05:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1707993#M211102</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-21T05:21:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx-mkimage for building flash.bin for iMX93 u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1708482#M211175</link>
      <description>&lt;P&gt;Under section&amp;nbsp;4.5.13, for i.MX 93 in Step 3, it says:&amp;nbsp;&lt;EM&gt;Copy the image of Sentinel firmware container mx93a0-ahab-container.img to imx-mkimage/iMX9/&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I used&amp;nbsp;&lt;STRONG&gt;mx93a0-ahab-container.img&lt;/STRONG&gt; from the Yocto build results and was able to successfully build and deploy flash.bin.&lt;/P&gt;&lt;P&gt;Is there a way to build&amp;nbsp;&lt;STRONG&gt;mx93a0-ahab-container.img&lt;/STRONG&gt; artifact independently, outside of Yocto?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 16:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1708482#M211175</guid>
      <dc:creator>abt</dc:creator>
      <dc:date>2023-08-21T16:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx-mkimage for building flash.bin for iMX93 u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1711922#M211524</link>
      <description>&lt;P&gt;refer to the release note&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_0-1693200792171.png" style="width: 2025px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238216i7A1CE8D8CA8D962F/image-dimensions/2025x86?v=v2" width="2025" height="86" role="button" title="joanxie_0-1693200792171.png" alt="joanxie_0-1693200792171.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;you can use this command to download&lt;/P&gt;
&lt;P&gt;wget &lt;A href="https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/" target="_blank"&gt;https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/&lt;/A&gt;&amp;lt;package file name&amp;gt;&lt;/P&gt;
&lt;P&gt;you can find container images there&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 05:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-mkimage-for-building-flash-bin-for-iMX93-u-boot/m-p/1711922#M211524</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-28T05:34:38Z</dc:date>
    </item>
  </channel>
</rss>