<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: system freeze without logs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1705369#M210862</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for the reply,&lt;/P&gt;&lt;P&gt;locate_hole failed issue resolved, by giving the 128@25000 crashkernel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I m facing currently below error, please have look into it,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx7d:~# kexec -d --type zImage -p zImage --append="'cat /proc/cmdline' maxcpus=1 reset_devices"&lt;BR /&gt;Try gzip decompression.&lt;BR /&gt;Try LZMA decompression.&lt;BR /&gt;&lt;STRONG&gt;lzma_decompress_file: read on zImage of 65536 bytes failed&lt;/STRONG&gt;&lt;BR /&gt;kernel: 0x7676e008 kernel_size: 0x628c08&lt;BR /&gt;MEMORY RANGES&lt;BR /&gt;0000000080000000-00000000bfffffff (0)&lt;BR /&gt;zImage header: 0x016f2818 0x00000000 0x00628c08&lt;BR /&gt;zImage size 0x628c08, file size 0x628c08&lt;BR /&gt;zImage requires 0x00639c08 bytes&lt;BR /&gt;Reserved memory ranges&lt;BR /&gt;0000000083400000-00000000933fffff (0)&lt;BR /&gt;Coredump memory ranges&lt;BR /&gt;0000000080000000-00000000833fffff (0)&lt;BR /&gt;0000000093400000-00000000bfffffff (0)&lt;BR /&gt;kernel symbol _stext vaddr = 80008280&lt;BR /&gt;phys offset = 0x80000000, page offset = 80000000&lt;BR /&gt;Using 32-bit ELF core format&lt;BR /&gt;get_crash_notes_per_cpu: crash_notes addr = ab726568, size = 180&lt;BR /&gt;Elf header: p_type = 4, p_offset = 0xab726568 p_paddr = 0xab726568 p_vaddr = 0x0 p_filesz = 0xb4 p_memsz = 0xb4&lt;BR /&gt;get_crash_notes_per_cpu: crash_notes addr = ab732568, size = 180&lt;BR /&gt;Elf header: p_type = 4, p_offset = 0xab732568 p_paddr = 0xab732568 p_vaddr = 0x0 p_filesz = 0xb4 p_memsz = 0xb4&lt;BR /&gt;vmcoreinfo header: p_type = 4, p_offset = 0x80bd761c p_paddr = 0x80bd761c p_vaddr = 0x0 p_filesz = 0x1024 p_memsz = 0x1024&lt;BR /&gt;Elf header: p_type = 1, p_offset = 0x80000000 p_paddr = 0x80000000 p_vaddr = 0x80000000 p_filesz = 0x3400000 p_memsz = 0x3400000&lt;BR /&gt;Elf header: p_type = 1, p_offset = 0x93400000 p_paddr = 0x93400000 p_vaddr = 0x93400000 p_filesz = 0x2cc00000 p_memsz = 0x2cc00000&lt;BR /&gt;elfcorehdr 0x93300000-0x933003ff&lt;BR /&gt;crashkernel: [0x83400000 - 0x933fffff] (256M)&lt;BR /&gt;memory range: [0x80000000 - 0x833fffff] (52M)&lt;BR /&gt;memory range: [0x93400000 - 0xbfffffff] (716M)&lt;BR /&gt;kernel command line: "'cat /proc/cmdline' maxcpus=1 reset_devices elfcorehdr=0x93300000 mem=261120K"&lt;BR /&gt;Kernel: address=0x83408000 size=0x01f20c28&lt;BR /&gt;get_cells_size: #address-cells:1 #size-cells:1&lt;BR /&gt;cells_size_fitted: 93300000-933003ff&lt;BR /&gt;cells_size_fitted: 83400000-933fffff&lt;BR /&gt;DT : address=0x8532a000 size=0x0000b053&lt;BR /&gt;kexec_load: entry = 0x83408000 flags = 0x280001&lt;BR /&gt;nr_segments = 3&lt;BR /&gt;segment[0].buf = 0x7676e008&lt;BR /&gt;segment[0].bufsz = 0x628c08&lt;BR /&gt;segment[0].mem = 0x83408000&lt;BR /&gt;segment[0].memsz = 0x629000&lt;BR /&gt;segment[1].buf = 0x1557068&lt;BR /&gt;segment[1].bufsz = 0xb053&lt;BR /&gt;segment[1].mem = 0x8532a000&lt;BR /&gt;segment[1].memsz = 0xc000&lt;BR /&gt;segment[2].buf = 0x1556c60&lt;BR /&gt;segment[2].bufsz = 0x400&lt;BR /&gt;segment[2].mem = 0x93300000&lt;BR /&gt;segment[2].memsz = 0x1000&lt;/P&gt;</description>
    <pubDate>Wed, 16 Aug 2023 04:19:15 GMT</pubDate>
    <dc:creator>shiva_bhargav_y</dc:creator>
    <dc:date>2023-08-16T04:19:15Z</dc:date>
    <item>
      <title>system freeze without logs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1703888#M210684</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using a i.mx 7 dual board with kernel version 4.1.46 with arm architecture, on it the we running Wi-Fi driver.&lt;/P&gt;&lt;P&gt;when we are trying to connect to Wi-Fi with hostapd num_max_sta = 1 and already 1 device connected to Wi-Fi without any problem and trying to connect 2nd device, after trying multiple times the entire system is freezing, to make the system working, we have to turn off power and power on again. before freeze happens no logs shown related to the freeze.&lt;/P&gt;&lt;P&gt;We don't see any logs and no kernel panic.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;tried to install kexec and load secondary kernel but we are getting following error.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN class=""&gt;Could not find a free area of memory of 0x1000 bytes...&lt;BR /&gt;locate_hole failed&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Tried to analyze the driver code didn't find anything.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Please suggest me how to get the logs or configure kexec to find the root of the freeze.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Shiva.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 13 Aug 2023 20:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1703888#M210684</guid>
      <dc:creator>shiva_bhargav_y</dc:creator>
      <dc:date>2023-08-13T20:29:29Z</dc:date>
    </item>
    <item>
      <title>Re: system freeze without logs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1705293#M210853</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221617"&gt;@shiva_bhargav_y&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please enlarge size of kdump reserved memory&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 02:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1705293#M210853</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-08-16T02:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: system freeze without logs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1705369#M210862</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for the reply,&lt;/P&gt;&lt;P&gt;locate_hole failed issue resolved, by giving the 128@25000 crashkernel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I m facing currently below error, please have look into it,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx7d:~# kexec -d --type zImage -p zImage --append="'cat /proc/cmdline' maxcpus=1 reset_devices"&lt;BR /&gt;Try gzip decompression.&lt;BR /&gt;Try LZMA decompression.&lt;BR /&gt;&lt;STRONG&gt;lzma_decompress_file: read on zImage of 65536 bytes failed&lt;/STRONG&gt;&lt;BR /&gt;kernel: 0x7676e008 kernel_size: 0x628c08&lt;BR /&gt;MEMORY RANGES&lt;BR /&gt;0000000080000000-00000000bfffffff (0)&lt;BR /&gt;zImage header: 0x016f2818 0x00000000 0x00628c08&lt;BR /&gt;zImage size 0x628c08, file size 0x628c08&lt;BR /&gt;zImage requires 0x00639c08 bytes&lt;BR /&gt;Reserved memory ranges&lt;BR /&gt;0000000083400000-00000000933fffff (0)&lt;BR /&gt;Coredump memory ranges&lt;BR /&gt;0000000080000000-00000000833fffff (0)&lt;BR /&gt;0000000093400000-00000000bfffffff (0)&lt;BR /&gt;kernel symbol _stext vaddr = 80008280&lt;BR /&gt;phys offset = 0x80000000, page offset = 80000000&lt;BR /&gt;Using 32-bit ELF core format&lt;BR /&gt;get_crash_notes_per_cpu: crash_notes addr = ab726568, size = 180&lt;BR /&gt;Elf header: p_type = 4, p_offset = 0xab726568 p_paddr = 0xab726568 p_vaddr = 0x0 p_filesz = 0xb4 p_memsz = 0xb4&lt;BR /&gt;get_crash_notes_per_cpu: crash_notes addr = ab732568, size = 180&lt;BR /&gt;Elf header: p_type = 4, p_offset = 0xab732568 p_paddr = 0xab732568 p_vaddr = 0x0 p_filesz = 0xb4 p_memsz = 0xb4&lt;BR /&gt;vmcoreinfo header: p_type = 4, p_offset = 0x80bd761c p_paddr = 0x80bd761c p_vaddr = 0x0 p_filesz = 0x1024 p_memsz = 0x1024&lt;BR /&gt;Elf header: p_type = 1, p_offset = 0x80000000 p_paddr = 0x80000000 p_vaddr = 0x80000000 p_filesz = 0x3400000 p_memsz = 0x3400000&lt;BR /&gt;Elf header: p_type = 1, p_offset = 0x93400000 p_paddr = 0x93400000 p_vaddr = 0x93400000 p_filesz = 0x2cc00000 p_memsz = 0x2cc00000&lt;BR /&gt;elfcorehdr 0x93300000-0x933003ff&lt;BR /&gt;crashkernel: [0x83400000 - 0x933fffff] (256M)&lt;BR /&gt;memory range: [0x80000000 - 0x833fffff] (52M)&lt;BR /&gt;memory range: [0x93400000 - 0xbfffffff] (716M)&lt;BR /&gt;kernel command line: "'cat /proc/cmdline' maxcpus=1 reset_devices elfcorehdr=0x93300000 mem=261120K"&lt;BR /&gt;Kernel: address=0x83408000 size=0x01f20c28&lt;BR /&gt;get_cells_size: #address-cells:1 #size-cells:1&lt;BR /&gt;cells_size_fitted: 93300000-933003ff&lt;BR /&gt;cells_size_fitted: 83400000-933fffff&lt;BR /&gt;DT : address=0x8532a000 size=0x0000b053&lt;BR /&gt;kexec_load: entry = 0x83408000 flags = 0x280001&lt;BR /&gt;nr_segments = 3&lt;BR /&gt;segment[0].buf = 0x7676e008&lt;BR /&gt;segment[0].bufsz = 0x628c08&lt;BR /&gt;segment[0].mem = 0x83408000&lt;BR /&gt;segment[0].memsz = 0x629000&lt;BR /&gt;segment[1].buf = 0x1557068&lt;BR /&gt;segment[1].bufsz = 0xb053&lt;BR /&gt;segment[1].mem = 0x8532a000&lt;BR /&gt;segment[1].memsz = 0xc000&lt;BR /&gt;segment[2].buf = 0x1556c60&lt;BR /&gt;segment[2].bufsz = 0x400&lt;BR /&gt;segment[2].mem = 0x93300000&lt;BR /&gt;segment[2].memsz = 0x1000&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 04:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-freeze-without-logs/m-p/1705369#M210862</guid>
      <dc:creator>shiva_bhargav_y</dc:creator>
      <dc:date>2023-08-16T04:19:15Z</dc:date>
    </item>
  </channel>
</rss>