<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8M Mini VPU and GPU Underclocking in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-and-GPU-Underclocking/m-p/1704529#M210764</link>
    <description>&lt;P&gt;I have an i.MX8M Mini where the the votlages for the VDD_VPU, VDD_GPU and VDD_DRAM are all tied together and operating at .95V so the LPDDR can run at 1.5GHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We're trying to lower power consumption by lowering the clocks of the VPU_H1 encoder and GPU which are both being used, but the datasheet for the i.MX8M Mini seems to show a voltage of 0.95V requires the GPU to run at 1000MHz and is too high to run the GPU at 800MHz.&amp;nbsp; The VPU_H1 seems to indicate we can run the VPU_H1 at 650MHz, but the VPU_PLL looks like it can go all the way down to 400MHz.&lt;/P&gt;&lt;P&gt;Can we safely underclock the VPU_H1 and 3D GPU to lower values without having to lower the DDR voltage of 0.95?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;Adam Ford,&lt;/P&gt;&lt;P&gt;Principal Applications Engineer, Beacon EmbeddedWorks.&lt;/P&gt;</description>
    <pubDate>Mon, 14 Aug 2023 21:00:11 GMT</pubDate>
    <dc:creator>adamford</dc:creator>
    <dc:date>2023-08-14T21:00:11Z</dc:date>
    <item>
      <title>i.MX8M Mini VPU and GPU Underclocking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-and-GPU-Underclocking/m-p/1704529#M210764</link>
      <description>&lt;P&gt;I have an i.MX8M Mini where the the votlages for the VDD_VPU, VDD_GPU and VDD_DRAM are all tied together and operating at .95V so the LPDDR can run at 1.5GHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We're trying to lower power consumption by lowering the clocks of the VPU_H1 encoder and GPU which are both being used, but the datasheet for the i.MX8M Mini seems to show a voltage of 0.95V requires the GPU to run at 1000MHz and is too high to run the GPU at 800MHz.&amp;nbsp; The VPU_H1 seems to indicate we can run the VPU_H1 at 650MHz, but the VPU_PLL looks like it can go all the way down to 400MHz.&lt;/P&gt;&lt;P&gt;Can we safely underclock the VPU_H1 and 3D GPU to lower values without having to lower the DDR voltage of 0.95?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;Adam Ford,&lt;/P&gt;&lt;P&gt;Principal Applications Engineer, Beacon EmbeddedWorks.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 21:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-and-GPU-Underclocking/m-p/1704529#M210764</guid>
      <dc:creator>adamford</dc:creator>
      <dc:date>2023-08-14T21:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini VPU and GPU Underclocking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-and-GPU-Underclocking/m-p/1707753#M211074</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/164242"&gt;@adamford&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on the Reference Manual for the iMX8M Mini the GPU clock for that voltage is up to 1000MHz therefore, you might underclock this block.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Brian_Ibarra_0-1692401176307.png" style="width: 589px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/237125i9C502A2472EC3769/image-dimensions/589x106?v=v2" width="589" height="106" role="button" title="Brian_Ibarra_0-1692401176307.png" alt="Brian_Ibarra_0-1692401176307.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;However, for VPU the target frequency for H1 acceleration is 800MHz. For this case, a lower clock might generate low performance.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Brian_Ibarra_1-1692401183949.png" style="width: 572px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/237126iCB1B961AD0C0DE92/image-dimensions/572x176?v=v2" width="572" height="176" role="button" title="Brian_Ibarra_1-1692401183949.png" alt="Brian_Ibarra_1-1692401183949.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards, Brian.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Aug 2023 23:27:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-VPU-and-GPU-Underclocking/m-p/1707753#M211074</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-08-18T23:27:00Z</dc:date>
    </item>
  </channel>
</rss>