<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX7D kernel upgrade 5.4 issue with the console boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1704196#M210721</link>
    <description>&lt;P&gt;Hi ,&lt;BR /&gt;We've upgraded the kernel from 4.14 to 5.4 and we got an issue , we couldn't have access to the console after booting the linux kernel and the init.&lt;BR /&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0&lt;BR /&gt;[ 0.000000] Linux version 5.4.24-hdl-eg4.1+g8cda0a19ad10 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Fri Mar 9 12:34:56 UTC 2018&lt;BR /&gt;[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d&lt;BR /&gt;[ 0.000000] CPU: div instructions available: patching division code&lt;BR /&gt;[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;[ 0.000000] OF: fdt: Machine model: Hanover Displays EG4&lt;BR /&gt;[ 0.000000] Memory policy: Data cache writealloc&lt;BR /&gt;[ 0.000000] cma: Reserved 32 MiB at 0xbe000000&lt;BR /&gt;[ 0.000000] percpu: Embedded 15 pages/cpu s32076 r8192 d21172 u61440&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259840&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc0,115200 vt.global_cursor_default=0 consoleblank=0 caam fbcon=rotate:3 root=/dev/mmcblk2p1 rootwait ro panic=1 watchdog.handle_boot_enabled=0&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)&lt;BR /&gt;[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] Memory: 986704K/1048576K available (11264K kernel code, 867K rwdata, 4068K rodata, 1024K init, 423K bss, 29104K reserved, 32768K cma-reserved, 0K highmem)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.&lt;BR /&gt;[ 0.000000] Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2&lt;BR /&gt;[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x2c8/0x484 with crng_init=0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns&lt;BR /&gt;[ 0.000008] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns&lt;BR /&gt;[ 0.000024] Switching to timer-based delay loop, resolution 125ns&lt;BR /&gt;[ 0.000453] Ignoring duplicate/late registration of read_current_timer delay&lt;BR /&gt;[ 0.000489] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;[ 0.002543] arch_timer: multiple nodes in dt, skipping&lt;BR /&gt;[ 0.003120] Console: colour dummy device 80x30&lt;BR /&gt;[ 0.003158] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=80000)&lt;BR /&gt;[ 0.003176] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.003401] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)&lt;BR /&gt;[ 0.003423] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)&lt;BR /&gt;[ 0.004421] CPU: Testing write buffer coherency: ok&lt;BR /&gt;[ 0.004850] CPU0: update cpu_capacity 1024&lt;BR /&gt;[ 0.004866] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;[ 0.059899] Setting up static identity map for 0x80100000 - 0x80100060&lt;BR /&gt;[ 0.079878] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.119941] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.200366] CPU1: update cpu_capacity 1024&lt;BR /&gt;[ 0.200376] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001&lt;BR /&gt;[ 0.200530] smp: Brought up 1 node, 2 CPUs&lt;BR /&gt;[ 0.200552] SMP: Total of 2 processors activated (32.00 BogoMIPS).&lt;BR /&gt;[ 0.200560] CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;[ 0.201019] devtmpfs: initialized&lt;BR /&gt;[ 0.215660] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;[ 0.216109] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;[ 0.216137] futex hash table entries: 512 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.217877] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.219218] NET: Registered protocol family 16&lt;BR /&gt;[ 0.228450] DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;[ 0.230304] hdl_hw_probe: initialisation&lt;BR /&gt;[ 0.230776] hdl_hw_probe: ID 0 - audio_enet = 3 (value: 421)&lt;BR /&gt;[ 0.230927] hdl_hw_probe: ID 1 - disp = 1 (value: 171)&lt;BR /&gt;[ 0.231074] hdl_hw_probe: ID 2 - plugin1 = 3 (value: 421)&lt;BR /&gt;[ 0.231222] hdl_hw_probe: ID 3 - plugin2 = 5 (value: 677)&lt;BR /&gt;[ 0.231371] hdl_hw_probe: ID 4 - wireless = NF (value: 4047)&lt;BR /&gt;[ 0.231519] hdl_hw_probe: ID 5 - gsm = NF (value: 4071)&lt;BR /&gt;[ 0.231666] hdl_hw_probe: ID 6 - io_plane = 2 (value: 298)&lt;BR /&gt;[ 0.231814] hdl_hw_probe: ID 7 - main_board = 2 (value: 299)&lt;BR /&gt;[ 0.231885] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.231933] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.231984] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232020] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232049] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232359] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232616] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232712] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.235223] hdl_hw_probe: GPIO 0 - sd_card = present&lt;BR /&gt;[ 0.235235] hdl_hw_probe: GPIO 1 - spi_flash = present&lt;BR /&gt;[ 0.235245] hdl_hw_probe: GPIO 2 - i2c_eeprom = present&lt;BR /&gt;[ 0.235254] hdl_hw_probe: GPIO 3 - ser2_rs232 = present&lt;BR /&gt;[ 0.235263] hdl_hw_probe: GPIO 4 - ser3_rs485 = present&lt;BR /&gt;[ 0.235272] hdl_hw_probe: GPIO 5 - ser3_j1708 = not present&lt;BR /&gt;[ 0.235281] hdl_hw_probe: GPIO 6 - ser4_rs485 = present&lt;BR /&gt;[ 0.235290] hdl_hw_probe: GPIO 7 - plugin1 = present&lt;BR /&gt;[ 0.235299] hdl_hw_probe: GPIO 8 - plugin2 = present&lt;BR /&gt;[ 0.235308] hdl_hw_probe: GPIO 9 - usb_otg1 = present&lt;BR /&gt;[ 0.235317] hdl_hw_probe: GPIO 10 - digout0 = present&lt;BR /&gt;[ 0.235326] hdl_hw_probe: GPIO 11 - digout1 = present&lt;BR /&gt;[ 0.235335] hdl_hw_probe: GPIO 12 - rtc_bat = present&lt;BR /&gt;[ 0.235345] hdl_hw_probe: GPIO 13 - amp = present&lt;BR /&gt;[ 0.235354] hdl_hw_probe: GPIO 14 - enet1 = present&lt;BR /&gt;[ 0.235363] hdl_hw_probe: GPIO 15 - enet2 = present&lt;BR /&gt;[ 0.235372] hdl_hw_probe: GPIO 16 - codec = present&lt;BR /&gt;[ 0.235381] hdl_hw_probe: GPIO 17 - mic_in = present&lt;BR /&gt;[ 0.235390] hdl_hw_probe: GPIO 18 - spkr_mic = present&lt;BR /&gt;[ 0.235399] hdl_hw_probe: GPIO 19 - line_out = present&lt;BR /&gt;[ 0.235408] hdl_hw_probe: GPIO 20 - rms_conv = present&lt;BR /&gt;[ 0.235417] hdl_hw_probe: GPIO 21 - enet_m12 = present&lt;BR /&gt;[ 0.235426] hdl_hw_probe: GPIO 22 - can = present&lt;BR /&gt;[ 0.235435] hdl_hw_probe: GPIO 23 - rtc = present&lt;BR /&gt;[ 0.235444] hdl_hw_probe: GPIO 24 - odo = present&lt;BR /&gt;[ 0.235459] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.235709] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.236299] hdl_hw_probe: enabling node: pwm@30680000&lt;BR /&gt;[ 0.236345] hdl_hw_probe: enabling node: pwm@30690000&lt;BR /&gt;[ 0.236383] hdl_hw_probe: enabling node: lcdif@30730000&lt;BR /&gt;[ 0.236436] hdl_hw_probe: enabling node: mipi-dsi@30760000&lt;BR /&gt;[ 0.236481] hdl_hw_probe: enabling node: spi@30830000&lt;BR /&gt;[ 0.236525] hdl_hw_probe: enabling node: serial@30890000&lt;BR /&gt;[ 0.236564] hdl_hw_probe: enabling node: serial@30880000&lt;BR /&gt;[ 0.236632] hdl_hw_probe: enabling node: sai@308b0000&lt;BR /&gt;[ 0.236679] hdl_hw_probe: enabling node: can@30a00000&lt;BR /&gt;[ 0.236847] hdl_hw_probe: applying overlay to i2c@30a40000&lt;BR /&gt;[ 0.237001] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237062] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237213] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237271] hdl_hw_probe: applying inner overlay to i2c@30a50000/pcf85063@51&lt;BR /&gt;[ 0.237421] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237566] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237661] hdl_hw_probe: enabling node: serial@30a60000&lt;BR /&gt;[ 0.237711] hdl_hw_probe: enabling node: serial@30a80000&lt;BR /&gt;[ 0.237750] hdl_hw_probe: applying overlay to serial@30a80000&lt;BR /&gt;[ 0.237862] hdl_hw_probe: enabling node: serial@30a90000&lt;BR /&gt;[ 0.237967] hdl_hw_probe: enabling node: usb@30b10000&lt;BR /&gt;[ 0.238043] hdl_hw_probe: enabling node: usdhc@30b40000&lt;BR /&gt;[ 0.238091] hdl_hw_probe: enabling node: ethernet@30be0000&lt;BR /&gt;[ 0.238132] hdl_hw_probe: applying overlay to ethernet@30be0000&lt;BR /&gt;[ 0.238192] hdl_hw_probe: applying overlay to mdio&lt;BR /&gt;[ 0.238363] hdl_hw_probe: applying overlay to mdio&lt;BR /&gt;[ 0.238556] hdl_hw_probe: enabling node: ethernet@30bf0000&lt;BR /&gt;[ 0.238665] hdl_hw_probe: enabling node: backlight&lt;BR /&gt;[ 0.238706] hdl_hw_probe: enabling node: leds&lt;BR /&gt;[ 0.238743] hdl_hw_probe: enabling node: pxp_v4l2_out&lt;BR /&gt;[ 0.238777] hdl_hw_probe: enabling node: sound-codec&lt;BR /&gt;[ 0.239228] cpuidle: using governor menu&lt;BR /&gt;[ 0.246574] vdd1p0d: supplied by regulator-dummy&lt;BR /&gt;[ 0.247268] vdd1p2: supplied by regulator-dummy&lt;BR /&gt;[ 0.251308] DDR type is DDR3!&lt;BR /&gt;[ 0.265288] hdl-hwprobe hdl-hw-probe: driver initialisation&lt;BR /&gt;[ 0.266995] imx7d_enet_clk_sel: found enet_out clock, assuming internal clock source&lt;BR /&gt;[ 0.267018] No ATAGs?&lt;BR /&gt;[ 0.267155] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.267171] hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;[ 0.269573] imx7d-pinctrl 302c0000.iomuxc-lpsr: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.270468] imx7d-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.286462] imx mu driver is registered.&lt;BR /&gt;[ 0.287134] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.288931] MU is ready for cross core communication!&lt;BR /&gt;[ 0.322732] vgaarb: loaded&lt;BR /&gt;[ 0.323408] SCSI subsystem initialized&lt;BR /&gt;[ 0.324001] usbcore: registered new interface driver usbfs&lt;BR /&gt;[ 0.324084] usbcore: registered new interface driver hub&lt;BR /&gt;[ 0.324191] usbcore: registered new device driver usb&lt;BR /&gt;[ 0.324386] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator&lt;BR /&gt;[ 0.324636] usb_phy_generic usbphynop3: usbphynop3 supply vcc not found, using dummy regulator&lt;BR /&gt;[ 0.325059] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator&lt;BR /&gt;[ 0.326637] i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;[ 0.327710] i2c i2c-2: IMX I2C adapter registered&lt;BR /&gt;[ 0.329093] i2c i2c-3: IMX I2C adapter registered&lt;BR /&gt;[ 0.329649] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.329708] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.329785] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.329796] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;[ 0.329826] PTP clock support registered&lt;BR /&gt;[ 0.331605] MIPI CSI2 driver module loaded&lt;BR /&gt;[ 0.331686] Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;[ 0.332670] Bluetooth: Core ver 2.22&lt;BR /&gt;[ 0.332731] NET: Registered protocol family 31&lt;BR /&gt;[ 0.332742] Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;[ 0.332761] Bluetooth: HCI socket layer initialized&lt;BR /&gt;[ 0.332775] Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;[ 0.332804] Bluetooth: SCO socket layer initialized&lt;BR /&gt;[ 0.333541] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.333784] VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;[ 0.333890] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;[ 0.345219] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.345687] NET: Registered protocol family 2&lt;BR /&gt;[ 0.346422] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)&lt;BR /&gt;[ 0.346467] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.346575] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.346752] TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;[ 0.346885] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.346948] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.347196] NET: Registered protocol family 1&lt;BR /&gt;[ 0.347820] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.347834] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.347843] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.347851] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.348461] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.349420] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available&lt;BR /&gt;[ 0.351355] Bus freq driver module loaded&lt;BR /&gt;[ 0.352644] Initialise system trusted keyrings&lt;BR /&gt;[ 0.352896] workingset: timestamp_bits=14 max_order=18 bucket_order=4&lt;BR /&gt;[ 0.362333] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.362380] Key type id_resolver registered&lt;BR /&gt;[ 0.362389] Key type id_legacy registered&lt;BR /&gt;[ 0.362450] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;[ 0.363074] fuse: init (API version 7.31)&lt;BR /&gt;[ 0.418907] Key type asymmetric registered&lt;BR /&gt;[ 0.418924] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.418951] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.418962] io scheduler kyber registered&lt;BR /&gt;[ 0.424050] pwm-backlight backlight: backlight supply power not found, using dummy regulator&lt;BR /&gt;[ 0.430419] imx-sdma 30bd0000.sdma: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2&lt;BR /&gt;[ 0.430440] imx-sdma 30bd0000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin&lt;BR /&gt;[ 0.433044] mxs-dma 33000000.dma-apbh: initialized&lt;BR /&gt;[ 0.436802] pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1&lt;BR /&gt;[ 0.437486] pfuze100-regulator 0-0008: FAB: 0, FIN: 0&lt;BR /&gt;[ 0.437502] pfuze100-regulator 0-0008: pfuze3000 found.&lt;BR /&gt;[ 0.452561] VLDO4: Bringing 3300000uV into 2800000-2800000uV&lt;BR /&gt;[ 0.456204] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 53, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.663188] printk: console [ttymxc0] enabled&lt;BR /&gt;[ 1.668543] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 54, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.678268] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 55, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.688005] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 63, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.697766] 30a80000.serial: ttymxc5 at MMIO 0x30a80000 (irq = 64, base_baud = 5000000) is a IMX&lt;BR /&gt;[ 1.707468] 30a90000.serial: ttymxc6 at MMIO 0x30a90000 (irq = 65, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.718214] imx sema4 driver is registered.&lt;BR /&gt;[ 1.742321] brd: module loaded&lt;BR /&gt;[ 1.755739] loop: module loaded&lt;BR /&gt;[ 1.760195] at24 2-005c: 16 byte 24cs08 EEPROM, read-only, 0 bytes/write&lt;BR /&gt;[ 1.768605] at24 2-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write&lt;BR /&gt;[ 1.777073] imx ahci driver is registered.&lt;BR /&gt;[ 1.786756] imx-sdma 30bd0000.sdma: sdma firmware not ready!&lt;BR /&gt;[ 1.792441] spi-nor spi1.0: SPI transfer failed: -22&lt;BR /&gt;[ 1.797483] spi_master spi1: failed to transfer one message from queue&lt;BR /&gt;[ 1.804054] spi-nor spi1.0: error -22 reading JEDEC ID&lt;BR /&gt;[ 1.809227] spi-nor: probe of spi1.0 failed with error -2&lt;BR /&gt;[ 1.814680] spi_imx 30830000.spi: probed&lt;BR /&gt;[ 1.819660] libphy: Fixed MDIO Bus: probed&lt;BR /&gt;[ 1.824512] CAN device driver interface&lt;BR /&gt;[ 1.829242] flexcan 30a00000.can: 30a00000.can supply xceiver not found, using dummy regulator&lt;BR /&gt;[ 1.840941] clk: failed to reparent enet1_ipg_root_clk to pll_enet_50m_clk: -22&lt;BR /&gt;[ 1.874913] pps pps0: new PPS source ptp0&lt;BR /&gt;[ 1.880809] libphy: fec_enet_mii_bus: probed&lt;BR /&gt;[ 1.887646] fec 30be0000.ethernet eth0: registered PHC device 0&lt;BR /&gt;[ 1.894092] clk: failed to reparent enet2_ipg_root_clk to pll_enet_50m_clk: -22&lt;BR /&gt;[ 1.923984] pps pps1: new PPS source ptp1&lt;BR /&gt;[ 1.930550] fec 30bf0000.ethernet eth1: registered PHC device 1&lt;BR /&gt;[ 1.936856] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k&lt;BR /&gt;[ 1.942702] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.&lt;BR /&gt;[ 1.949399] PPP generic driver version 2.4.2&lt;BR /&gt;[ 1.953942] PPP BSD Compression module registered&lt;BR /&gt;[ 1.958660] PPP Deflate Compression module registered&lt;BR /&gt;[ 1.963837] usbcore: registered new interface driver asix&lt;BR /&gt;[ 1.969322] usbcore: registered new interface driver ax88179_178a&lt;BR /&gt;[ 1.975504] usbcore: registered new interface driver cdc_ether&lt;BR /&gt;[ 1.981394] usbcore: registered new interface driver net1080&lt;BR /&gt;[ 1.987128] usbcore: registered new interface driver cdc_subset&lt;BR /&gt;[ 1.993103] usbcore: registered new interface driver zaurus&lt;BR /&gt;[ 1.998782] usbcore: registered new interface driver cdc_ncm&lt;BR /&gt;[ 2.004471] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;[ 2.011009] ehci-pci: EHCI PCI platform driver&lt;BR /&gt;[ 2.015581] ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;[ 2.021390] usbcore: registered new interface driver usb-storage&lt;BR /&gt;[ 2.030334] imx_usb 30b10000.usb: No over current polarity defined&lt;BR /&gt;[ 2.040389] ci_hdrc ci_hdrc.0: EHCI Host Controller&lt;BR /&gt;[ 2.045356] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1&lt;BR /&gt;[ 2.073581] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00&lt;BR /&gt;[ 2.079236] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04&lt;BR /&gt;[ 2.087588] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1&lt;BR /&gt;[ 2.094849] usb usb1: Product: EHCI Host Controller&lt;BR /&gt;[ 2.099742] usb usb1: Manufacturer: Linux 5.4.24-hdl-eg4.1+g8cda0a19ad10 ehci_hcd&lt;BR /&gt;[ 2.107256] usb usb1: SerialNumber: ci_hdrc.0&lt;BR /&gt;[ 2.112373] hub 1-0:1.0: USB hub found&lt;BR /&gt;[ 2.116223] hub 1-0:1.0: 1 port detected&lt;BR /&gt;[ 2.121660] imx_usb 30b20000.usb: No over current polarity defined&lt;BR /&gt;[ 2.130925] ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;[ 2.135894] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2&lt;BR /&gt;[ 2.163572] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;[ 2.169209] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04&lt;BR /&gt;[ 2.177523] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1&lt;BR /&gt;[ 2.184781] usb usb2: Product: EHCI Host Controller&lt;BR /&gt;[ 2.189675] usb usb2: Manufacturer: Linux 5.4.24-hdl-eg4.1+g8cda0a19ad10 ehci_hcd&lt;BR /&gt;[ 2.197189] usb usb2: SerialNumber: ci_hdrc.1&lt;BR /&gt;[ 2.202269] hub 2-0:1.0: USB hub found&lt;BR /&gt;[ 2.206115] hub 2-0:1.0: 1 port detected&lt;BR /&gt;[ 2.212933] Goodix-TS 3-005d: 3-005d supply AVDD28 not found, using dummy regulator&lt;BR /&gt;[ 2.220790] Goodix-TS 3-005d: 3-005d supply VDDIO not found, using dummy regulator&lt;BR /&gt;[ 2.345738] Goodix-TS 3-005d: ID 911, version: 1060&lt;BR /&gt;[ 2.350770] Goodix-TS 3-005d: Direct firmware load for goodix_911_cfg.bin failed with error -2&lt;BR /&gt;[ 2.360705] Goodix-TS 3-005d: Falling back to sysfs fallback for: goodix_911_cfg.bin&lt;BR /&gt;[ 2.371524] rtc-pcf85063 3-0051: registered as rtc0&lt;BR /&gt;[ 2.376865] i2c /dev entries driver&lt;BR /&gt;[ 2.384433] watchdog: watchdog0 running and kernel based pre-userspace handler disabled&lt;BR /&gt;[ 2.392464] imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;[ 2.399265] Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;[ 2.403763] Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;[ 2.408913] Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;[ 2.414289] Bluetooth: HCI UART protocol LL registered&lt;BR /&gt;[ 2.419471] Bluetooth: HCI UART protocol Three-wire (H5) registered&lt;BR /&gt;[ 2.425969] Bluetooth: HCI UART protocol Marvell registered&lt;BR /&gt;[ 2.431637] usbcore: registered new interface driver btusb&lt;BR /&gt;[ 2.438248] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 2.444483] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 2.448852] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 2.456439] sdhci-esdhc-imx 30b40000.usdhc: Got CD GPIO&lt;BR /&gt;[ 2.461712] sdhci-esdhc-imx 30b40000.usdhc: Got WP GPIO&lt;BR /&gt;[ 2.573579] usb 2-1: new high-speed USB device number 2 using ci_hdrc&lt;BR /&gt;[ 2.638371] usb 2-1: New USB device found, idVendor=2001, idProduct=1a02, bcdDevice= 0.02&lt;BR /&gt;[ 2.646601] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3&lt;BR /&gt;[ 2.653787] usb 2-1: Product: DUB-E100&lt;BR /&gt;[ 2.657551] usb 2-1: Manufacturer: D-Link Corp.&lt;BR /&gt;[ 2.662442] usb 2-1: SerialNumber: 0023D9&lt;BR /&gt;[ 2.712102] mmc0: SDHCI controller on 30b40000.usdhc [30b40000.usdhc] using ADMA&lt;BR /&gt;[ 2.762957] mmc2: SDHCI controller on 30b60000.usdhc [30b60000.usdhc] using ADMA&lt;BR /&gt;[ 2.774264] caam 30900000.caam: device ID = 0x0a16030000000000 (Era &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;[ 2.780874] caam 30900000.caam: job rings = 3, qi = 0&lt;BR /&gt;[ 2.818598] caam algorithms registered in /proc/crypto&lt;BR /&gt;[ 2.827586] caam 30900000.caam: caam pkc algorithms registered in /proc/crypto&lt;BR /&gt;[ 2.837051] caam_jr 30901000.jr0: registering rng-caam&lt;BR /&gt;[ 2.864696] caam-snvs 30370000.caam-snvs: can't get snvs clock&lt;BR /&gt;[ 2.870625] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state&lt;BR /&gt;[ 2.880133] usbcore: registered new interface driver usbhid&lt;BR /&gt;[ 2.885746] usbhid: USB HID core driver&lt;BR /&gt;[ 2.893258] mmc2: new HS400 MMC card at address 0001&lt;BR /&gt;[ 2.900894] tlv320aic3x-codec 3-0018: Using deprecated property "gpio-reset", please update your DT&lt;BR /&gt;[ 2.904086] mmcblk2: mmc2:0001 Q2J54A 3.59 GiB&lt;BR /&gt;[ 2.910106] tlv320aic3x-codec 3-0018: 3-0018 supply IOVDD not found, using dummy regulator&lt;BR /&gt;[ 2.914998] mmcblk2boot0: mmc2:0001 Q2J54A partition 1 16.0 MiB&lt;BR /&gt;[ 2.922948] tlv320aic3x-codec 3-0018: 3-0018 supply DVDD not found, using dummy regulator&lt;BR /&gt;[ 2.929183] mmcblk2boot1: mmc2:0001 Q2J54A partition 2 16.0 MiB&lt;BR /&gt;[ 2.937147] tlv320aic3x-codec 3-0018: 3-0018 supply AVDD not found, using dummy regulator&lt;BR /&gt;[ 2.943314] mmcblk2rpmb: mmc2:0001 Q2J54A partition 3 512 KiB, chardev (245:0)&lt;BR /&gt;[ 2.951271] tlv320aic3x-codec 3-0018: 3-0018 supply DRVDD not found, using dummy regulator&lt;BR /&gt;[ 2.966851] tlv320aic3x-codec 3-0018: Invalid supply voltage(s) AVDD: -22, DVDD: -22&lt;BR /&gt;[ 2.972005] mmcblk2: p1 p2 p3 &amp;lt; p5 p6 p7 &amp;gt;&lt;BR /&gt;[ 2.980091] fsl-sai 308a0000.sai: failed to get mclk0 clock: -2&lt;BR /&gt;[ 2.991946] fsl-sai 308b0000.sai: failed to get mclk0 clock: -2&lt;BR /&gt;[ 3.006132] NET: Registered protocol family 26&lt;BR /&gt;[ 3.011511] NET: Registered protocol family 10&lt;BR /&gt;[ 3.027460] Segment Routing with IPv6&lt;BR /&gt;[ 3.031239] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver&lt;BR /&gt;[ 3.038068] NET: Registered protocol family 17&lt;BR /&gt;[ 3.042542] can: controller area network core (rev 20170425 abi 9)&lt;BR /&gt;[ 3.048867] NET: Registered protocol family 29&lt;BR /&gt;[ 3.053327] can: raw protocol (rev 20170425)&lt;BR /&gt;[ 3.057641] can: broadcast manager protocol (rev 20170425 t)&lt;BR /&gt;[ 3.063320] can: netlink gateway (rev 20190810) max_hops=1&lt;BR /&gt;[ 3.069144] Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;[ 3.074090] Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;[ 3.079293] Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;[ 3.083067] Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;[ 3.088416] Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;[ 3.093678] Bluetooth: BNEP socket layer initialized&lt;BR /&gt;[ 3.098654] Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;[ 3.104607] Bluetooth: HIDP socket layer initialized&lt;BR /&gt;[ 3.109650] lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;[ 3.114842] random: fast init done&lt;BR /&gt;[ 3.118790] Key type dns_resolver registered&lt;BR /&gt;[ 3.122861] asix 2-1:1.0 eth2: register 'asix' at usb-ci_hdrc.1-1, ASIX AX88772 USB 2.0 Ethernet, a8:63:7d:61:1b:40&lt;BR /&gt;[ 3.134316] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 1 supported-hw 0x4 0x2&lt;BR /&gt;[ 3.144216] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 648000 KHz&lt;BR /&gt;[ 3.152989] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 792000 KHz&lt;BR /&gt;[ 3.161805] Registering SWP/SWPB emulation handler&lt;BR /&gt;[ 3.166887] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 3.207927] imx_thermal tempmon: Extended Commercial CPU temperature grade - max:105C critical:100C passive:95C&lt;BR /&gt;[ 3.222139] rtc-pcf85063 3-0051: setting system clock to 2018-03-13T09:49:57 UTC (1520934597)&lt;BR /&gt;[ 3.231043] cfg80211: Loading compiled-in X.509 certificates for regulatory database&lt;BR /&gt;[ 3.241094] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'&lt;BR /&gt;[ 3.247811] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2&lt;BR /&gt;[ 3.256973] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db&lt;BR /&gt;[ 3.286271] ALSA device list:&lt;BR /&gt;[ 3.289250] No soundcards found.&lt;BR /&gt;[ 3.301881] EXT4-fs (mmcblk2p1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 3.310183] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.&lt;BR /&gt;[ 3.317526] devtmpfs: mounted&lt;BR /&gt;[ 3.321853] Freeing unused kernel memory: 1024K&lt;BR /&gt;[ 3.353834] Run /sbin/init as init process&lt;BR /&gt;INIT: version 2.96 booting&lt;BR /&gt;Framebuffer /dev/fb0 not detected&lt;BR /&gt;Boot splashscreen disabled&lt;BR /&gt;[ 3.839617] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.115764] EXT4-fs (mmcblk2p5): recovery complete&lt;BR /&gt;[ 4.121101] EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.129313] ext4 filesystem being mounted at /mnt/hos-state supports timestamps until 2038 (0x7fffffff)&lt;BR /&gt;[ 4.143868] EXT4-fs (mmcblk2p6): recovery complete&lt;BR /&gt;[ 4.148680] EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.161992] EXT4-fs (mmcblk2p7): recovery complete&lt;BR /&gt;[ 4.166842] EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.174991] ext4 filesystem being mounted at /mnt/hos-volatile supports timestamps until 2038 (0x7fffffff)&lt;BR /&gt;Starting udev&lt;BR /&gt;[ 4.270274] udevd[288]: starting version 3.2.9&lt;BR /&gt;[ 4.283003] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.290005] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.297011] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.322600] udevd[289]: starting eudev-3.2.9&lt;BR /&gt;[ 4.579432] input: Goodix Capacitive TouchScreen as /devices/soc0/soc/30800000.aips-bus/30a50000.i2c/i2c-3/3-005d/input/input0&lt;BR /&gt;[ 4.632964] imx-sdma 30bd0000.sdma: loaded firmware 4.5&lt;BR /&gt;[ 5.349073] urandom_read: 4 callbacks suppressed&lt;BR /&gt;[ 5.349082] random: python3: uninitialized urandom read (24 bytes read)&lt;BR /&gt;[ 8.891462] random: dd: uninitialized urandom read (512 bytes read)&lt;BR /&gt;[ 9.142463] fec 30be0000.ethernet eth0: Unable to connect to phy&lt;BR /&gt;[ 9.212304] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 9.325802] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready&lt;BR /&gt;[ 9.413269] random: dbus-uuidgen: uninitialized urandom read (12 bytes read)&lt;BR /&gt;[ 9.573304] IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready&lt;BR /&gt;[ 9.582997] asix 2-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0xC1E1&lt;BR /&gt;[ 13.343621] random: crng init done&lt;/P&gt;&lt;P&gt;The board reboot after some seconds , Could you please help to fix that or do we miss something ?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Imy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Aug 2023 08:39:15 GMT</pubDate>
    <dc:creator>ibenhassen</dc:creator>
    <dc:date>2023-08-14T08:39:15Z</dc:date>
    <item>
      <title>IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1704196#M210721</link>
      <description>&lt;P&gt;Hi ,&lt;BR /&gt;We've upgraded the kernel from 4.14 to 5.4 and we got an issue , we couldn't have access to the console after booting the linux kernel and the init.&lt;BR /&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0&lt;BR /&gt;[ 0.000000] Linux version 5.4.24-hdl-eg4.1+g8cda0a19ad10 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Fri Mar 9 12:34:56 UTC 2018&lt;BR /&gt;[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d&lt;BR /&gt;[ 0.000000] CPU: div instructions available: patching division code&lt;BR /&gt;[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;[ 0.000000] OF: fdt: Machine model: Hanover Displays EG4&lt;BR /&gt;[ 0.000000] Memory policy: Data cache writealloc&lt;BR /&gt;[ 0.000000] cma: Reserved 32 MiB at 0xbe000000&lt;BR /&gt;[ 0.000000] percpu: Embedded 15 pages/cpu s32076 r8192 d21172 u61440&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259840&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc0,115200 vt.global_cursor_default=0 consoleblank=0 caam fbcon=rotate:3 root=/dev/mmcblk2p1 rootwait ro panic=1 watchdog.handle_boot_enabled=0&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)&lt;BR /&gt;[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] Memory: 986704K/1048576K available (11264K kernel code, 867K rwdata, 4068K rodata, 1024K init, 423K bss, 29104K reserved, 32768K cma-reserved, 0K highmem)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.&lt;BR /&gt;[ 0.000000] Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2&lt;BR /&gt;[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x2c8/0x484 with crng_init=0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns&lt;BR /&gt;[ 0.000008] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns&lt;BR /&gt;[ 0.000024] Switching to timer-based delay loop, resolution 125ns&lt;BR /&gt;[ 0.000453] Ignoring duplicate/late registration of read_current_timer delay&lt;BR /&gt;[ 0.000489] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;[ 0.002543] arch_timer: multiple nodes in dt, skipping&lt;BR /&gt;[ 0.003120] Console: colour dummy device 80x30&lt;BR /&gt;[ 0.003158] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=80000)&lt;BR /&gt;[ 0.003176] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.003401] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)&lt;BR /&gt;[ 0.003423] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)&lt;BR /&gt;[ 0.004421] CPU: Testing write buffer coherency: ok&lt;BR /&gt;[ 0.004850] CPU0: update cpu_capacity 1024&lt;BR /&gt;[ 0.004866] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;[ 0.059899] Setting up static identity map for 0x80100000 - 0x80100060&lt;BR /&gt;[ 0.079878] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.119941] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.200366] CPU1: update cpu_capacity 1024&lt;BR /&gt;[ 0.200376] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001&lt;BR /&gt;[ 0.200530] smp: Brought up 1 node, 2 CPUs&lt;BR /&gt;[ 0.200552] SMP: Total of 2 processors activated (32.00 BogoMIPS).&lt;BR /&gt;[ 0.200560] CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;[ 0.201019] devtmpfs: initialized&lt;BR /&gt;[ 0.215660] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;[ 0.216109] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;[ 0.216137] futex hash table entries: 512 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.217877] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.219218] NET: Registered protocol family 16&lt;BR /&gt;[ 0.228450] DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;[ 0.230304] hdl_hw_probe: initialisation&lt;BR /&gt;[ 0.230776] hdl_hw_probe: ID 0 - audio_enet = 3 (value: 421)&lt;BR /&gt;[ 0.230927] hdl_hw_probe: ID 1 - disp = 1 (value: 171)&lt;BR /&gt;[ 0.231074] hdl_hw_probe: ID 2 - plugin1 = 3 (value: 421)&lt;BR /&gt;[ 0.231222] hdl_hw_probe: ID 3 - plugin2 = 5 (value: 677)&lt;BR /&gt;[ 0.231371] hdl_hw_probe: ID 4 - wireless = NF (value: 4047)&lt;BR /&gt;[ 0.231519] hdl_hw_probe: ID 5 - gsm = NF (value: 4071)&lt;BR /&gt;[ 0.231666] hdl_hw_probe: ID 6 - io_plane = 2 (value: 298)&lt;BR /&gt;[ 0.231814] hdl_hw_probe: ID 7 - main_board = 2 (value: 299)&lt;BR /&gt;[ 0.231885] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.231933] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.231984] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232020] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232049] hdl_hw_probe: applying inner overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232359] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232616] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.232712] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.235223] hdl_hw_probe: GPIO 0 - sd_card = present&lt;BR /&gt;[ 0.235235] hdl_hw_probe: GPIO 1 - spi_flash = present&lt;BR /&gt;[ 0.235245] hdl_hw_probe: GPIO 2 - i2c_eeprom = present&lt;BR /&gt;[ 0.235254] hdl_hw_probe: GPIO 3 - ser2_rs232 = present&lt;BR /&gt;[ 0.235263] hdl_hw_probe: GPIO 4 - ser3_rs485 = present&lt;BR /&gt;[ 0.235272] hdl_hw_probe: GPIO 5 - ser3_j1708 = not present&lt;BR /&gt;[ 0.235281] hdl_hw_probe: GPIO 6 - ser4_rs485 = present&lt;BR /&gt;[ 0.235290] hdl_hw_probe: GPIO 7 - plugin1 = present&lt;BR /&gt;[ 0.235299] hdl_hw_probe: GPIO 8 - plugin2 = present&lt;BR /&gt;[ 0.235308] hdl_hw_probe: GPIO 9 - usb_otg1 = present&lt;BR /&gt;[ 0.235317] hdl_hw_probe: GPIO 10 - digout0 = present&lt;BR /&gt;[ 0.235326] hdl_hw_probe: GPIO 11 - digout1 = present&lt;BR /&gt;[ 0.235335] hdl_hw_probe: GPIO 12 - rtc_bat = present&lt;BR /&gt;[ 0.235345] hdl_hw_probe: GPIO 13 - amp = present&lt;BR /&gt;[ 0.235354] hdl_hw_probe: GPIO 14 - enet1 = present&lt;BR /&gt;[ 0.235363] hdl_hw_probe: GPIO 15 - enet2 = present&lt;BR /&gt;[ 0.235372] hdl_hw_probe: GPIO 16 - codec = present&lt;BR /&gt;[ 0.235381] hdl_hw_probe: GPIO 17 - mic_in = present&lt;BR /&gt;[ 0.235390] hdl_hw_probe: GPIO 18 - spkr_mic = present&lt;BR /&gt;[ 0.235399] hdl_hw_probe: GPIO 19 - line_out = present&lt;BR /&gt;[ 0.235408] hdl_hw_probe: GPIO 20 - rms_conv = present&lt;BR /&gt;[ 0.235417] hdl_hw_probe: GPIO 21 - enet_m12 = present&lt;BR /&gt;[ 0.235426] hdl_hw_probe: GPIO 22 - can = present&lt;BR /&gt;[ 0.235435] hdl_hw_probe: GPIO 23 - rtc = present&lt;BR /&gt;[ 0.235444] hdl_hw_probe: GPIO 24 - odo = present&lt;BR /&gt;[ 0.235459] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.235709] hdl_hw_probe: applying overlay to hdl-hw-probe&lt;BR /&gt;[ 0.236299] hdl_hw_probe: enabling node: pwm@30680000&lt;BR /&gt;[ 0.236345] hdl_hw_probe: enabling node: pwm@30690000&lt;BR /&gt;[ 0.236383] hdl_hw_probe: enabling node: lcdif@30730000&lt;BR /&gt;[ 0.236436] hdl_hw_probe: enabling node: mipi-dsi@30760000&lt;BR /&gt;[ 0.236481] hdl_hw_probe: enabling node: spi@30830000&lt;BR /&gt;[ 0.236525] hdl_hw_probe: enabling node: serial@30890000&lt;BR /&gt;[ 0.236564] hdl_hw_probe: enabling node: serial@30880000&lt;BR /&gt;[ 0.236632] hdl_hw_probe: enabling node: sai@308b0000&lt;BR /&gt;[ 0.236679] hdl_hw_probe: enabling node: can@30a00000&lt;BR /&gt;[ 0.236847] hdl_hw_probe: applying overlay to i2c@30a40000&lt;BR /&gt;[ 0.237001] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237062] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237213] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237271] hdl_hw_probe: applying inner overlay to i2c@30a50000/pcf85063@51&lt;BR /&gt;[ 0.237421] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237566] hdl_hw_probe: applying overlay to i2c@30a50000&lt;BR /&gt;[ 0.237661] hdl_hw_probe: enabling node: serial@30a60000&lt;BR /&gt;[ 0.237711] hdl_hw_probe: enabling node: serial@30a80000&lt;BR /&gt;[ 0.237750] hdl_hw_probe: applying overlay to serial@30a80000&lt;BR /&gt;[ 0.237862] hdl_hw_probe: enabling node: serial@30a90000&lt;BR /&gt;[ 0.237967] hdl_hw_probe: enabling node: usb@30b10000&lt;BR /&gt;[ 0.238043] hdl_hw_probe: enabling node: usdhc@30b40000&lt;BR /&gt;[ 0.238091] hdl_hw_probe: enabling node: ethernet@30be0000&lt;BR /&gt;[ 0.238132] hdl_hw_probe: applying overlay to ethernet@30be0000&lt;BR /&gt;[ 0.238192] hdl_hw_probe: applying overlay to mdio&lt;BR /&gt;[ 0.238363] hdl_hw_probe: applying overlay to mdio&lt;BR /&gt;[ 0.238556] hdl_hw_probe: enabling node: ethernet@30bf0000&lt;BR /&gt;[ 0.238665] hdl_hw_probe: enabling node: backlight&lt;BR /&gt;[ 0.238706] hdl_hw_probe: enabling node: leds&lt;BR /&gt;[ 0.238743] hdl_hw_probe: enabling node: pxp_v4l2_out&lt;BR /&gt;[ 0.238777] hdl_hw_probe: enabling node: sound-codec&lt;BR /&gt;[ 0.239228] cpuidle: using governor menu&lt;BR /&gt;[ 0.246574] vdd1p0d: supplied by regulator-dummy&lt;BR /&gt;[ 0.247268] vdd1p2: supplied by regulator-dummy&lt;BR /&gt;[ 0.251308] DDR type is DDR3!&lt;BR /&gt;[ 0.265288] hdl-hwprobe hdl-hw-probe: driver initialisation&lt;BR /&gt;[ 0.266995] imx7d_enet_clk_sel: found enet_out clock, assuming internal clock source&lt;BR /&gt;[ 0.267018] No ATAGs?&lt;BR /&gt;[ 0.267155] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.267171] hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;[ 0.269573] imx7d-pinctrl 302c0000.iomuxc-lpsr: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.270468] imx7d-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.286462] imx mu driver is registered.&lt;BR /&gt;[ 0.287134] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.288931] MU is ready for cross core communication!&lt;BR /&gt;[ 0.322732] vgaarb: loaded&lt;BR /&gt;[ 0.323408] SCSI subsystem initialized&lt;BR /&gt;[ 0.324001] usbcore: registered new interface driver usbfs&lt;BR /&gt;[ 0.324084] usbcore: registered new interface driver hub&lt;BR /&gt;[ 0.324191] usbcore: registered new device driver usb&lt;BR /&gt;[ 0.324386] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator&lt;BR /&gt;[ 0.324636] usb_phy_generic usbphynop3: usbphynop3 supply vcc not found, using dummy regulator&lt;BR /&gt;[ 0.325059] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator&lt;BR /&gt;[ 0.326637] i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;[ 0.327710] i2c i2c-2: IMX I2C adapter registered&lt;BR /&gt;[ 0.329093] i2c i2c-3: IMX I2C adapter registered&lt;BR /&gt;[ 0.329649] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.329708] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.329785] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.329796] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;[ 0.329826] PTP clock support registered&lt;BR /&gt;[ 0.331605] MIPI CSI2 driver module loaded&lt;BR /&gt;[ 0.331686] Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;[ 0.332670] Bluetooth: Core ver 2.22&lt;BR /&gt;[ 0.332731] NET: Registered protocol family 31&lt;BR /&gt;[ 0.332742] Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;[ 0.332761] Bluetooth: HCI socket layer initialized&lt;BR /&gt;[ 0.332775] Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;[ 0.332804] Bluetooth: SCO socket layer initialized&lt;BR /&gt;[ 0.333541] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.333784] VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;[ 0.333890] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;[ 0.345219] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.345687] NET: Registered protocol family 2&lt;BR /&gt;[ 0.346422] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)&lt;BR /&gt;[ 0.346467] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.346575] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.346752] TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;[ 0.346885] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.346948] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.347196] NET: Registered protocol family 1&lt;BR /&gt;[ 0.347820] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.347834] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.347843] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.347851] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.348461] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.349420] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available&lt;BR /&gt;[ 0.351355] Bus freq driver module loaded&lt;BR /&gt;[ 0.352644] Initialise system trusted keyrings&lt;BR /&gt;[ 0.352896] workingset: timestamp_bits=14 max_order=18 bucket_order=4&lt;BR /&gt;[ 0.362333] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.362380] Key type id_resolver registered&lt;BR /&gt;[ 0.362389] Key type id_legacy registered&lt;BR /&gt;[ 0.362450] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;[ 0.363074] fuse: init (API version 7.31)&lt;BR /&gt;[ 0.418907] Key type asymmetric registered&lt;BR /&gt;[ 0.418924] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.418951] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.418962] io scheduler kyber registered&lt;BR /&gt;[ 0.424050] pwm-backlight backlight: backlight supply power not found, using dummy regulator&lt;BR /&gt;[ 0.430419] imx-sdma 30bd0000.sdma: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2&lt;BR /&gt;[ 0.430440] imx-sdma 30bd0000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin&lt;BR /&gt;[ 0.433044] mxs-dma 33000000.dma-apbh: initialized&lt;BR /&gt;[ 0.436802] pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1&lt;BR /&gt;[ 0.437486] pfuze100-regulator 0-0008: FAB: 0, FIN: 0&lt;BR /&gt;[ 0.437502] pfuze100-regulator 0-0008: pfuze3000 found.&lt;BR /&gt;[ 0.452561] VLDO4: Bringing 3300000uV into 2800000-2800000uV&lt;BR /&gt;[ 0.456204] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 53, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.663188] printk: console [ttymxc0] enabled&lt;BR /&gt;[ 1.668543] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 54, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.678268] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 55, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.688005] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 63, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.697766] 30a80000.serial: ttymxc5 at MMIO 0x30a80000 (irq = 64, base_baud = 5000000) is a IMX&lt;BR /&gt;[ 1.707468] 30a90000.serial: ttymxc6 at MMIO 0x30a90000 (irq = 65, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.718214] imx sema4 driver is registered.&lt;BR /&gt;[ 1.742321] brd: module loaded&lt;BR /&gt;[ 1.755739] loop: module loaded&lt;BR /&gt;[ 1.760195] at24 2-005c: 16 byte 24cs08 EEPROM, read-only, 0 bytes/write&lt;BR /&gt;[ 1.768605] at24 2-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write&lt;BR /&gt;[ 1.777073] imx ahci driver is registered.&lt;BR /&gt;[ 1.786756] imx-sdma 30bd0000.sdma: sdma firmware not ready!&lt;BR /&gt;[ 1.792441] spi-nor spi1.0: SPI transfer failed: -22&lt;BR /&gt;[ 1.797483] spi_master spi1: failed to transfer one message from queue&lt;BR /&gt;[ 1.804054] spi-nor spi1.0: error -22 reading JEDEC ID&lt;BR /&gt;[ 1.809227] spi-nor: probe of spi1.0 failed with error -2&lt;BR /&gt;[ 1.814680] spi_imx 30830000.spi: probed&lt;BR /&gt;[ 1.819660] libphy: Fixed MDIO Bus: probed&lt;BR /&gt;[ 1.824512] CAN device driver interface&lt;BR /&gt;[ 1.829242] flexcan 30a00000.can: 30a00000.can supply xceiver not found, using dummy regulator&lt;BR /&gt;[ 1.840941] clk: failed to reparent enet1_ipg_root_clk to pll_enet_50m_clk: -22&lt;BR /&gt;[ 1.874913] pps pps0: new PPS source ptp0&lt;BR /&gt;[ 1.880809] libphy: fec_enet_mii_bus: probed&lt;BR /&gt;[ 1.887646] fec 30be0000.ethernet eth0: registered PHC device 0&lt;BR /&gt;[ 1.894092] clk: failed to reparent enet2_ipg_root_clk to pll_enet_50m_clk: -22&lt;BR /&gt;[ 1.923984] pps pps1: new PPS source ptp1&lt;BR /&gt;[ 1.930550] fec 30bf0000.ethernet eth1: registered PHC device 1&lt;BR /&gt;[ 1.936856] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k&lt;BR /&gt;[ 1.942702] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.&lt;BR /&gt;[ 1.949399] PPP generic driver version 2.4.2&lt;BR /&gt;[ 1.953942] PPP BSD Compression module registered&lt;BR /&gt;[ 1.958660] PPP Deflate Compression module registered&lt;BR /&gt;[ 1.963837] usbcore: registered new interface driver asix&lt;BR /&gt;[ 1.969322] usbcore: registered new interface driver ax88179_178a&lt;BR /&gt;[ 1.975504] usbcore: registered new interface driver cdc_ether&lt;BR /&gt;[ 1.981394] usbcore: registered new interface driver net1080&lt;BR /&gt;[ 1.987128] usbcore: registered new interface driver cdc_subset&lt;BR /&gt;[ 1.993103] usbcore: registered new interface driver zaurus&lt;BR /&gt;[ 1.998782] usbcore: registered new interface driver cdc_ncm&lt;BR /&gt;[ 2.004471] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;[ 2.011009] ehci-pci: EHCI PCI platform driver&lt;BR /&gt;[ 2.015581] ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;[ 2.021390] usbcore: registered new interface driver usb-storage&lt;BR /&gt;[ 2.030334] imx_usb 30b10000.usb: No over current polarity defined&lt;BR /&gt;[ 2.040389] ci_hdrc ci_hdrc.0: EHCI Host Controller&lt;BR /&gt;[ 2.045356] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1&lt;BR /&gt;[ 2.073581] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00&lt;BR /&gt;[ 2.079236] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04&lt;BR /&gt;[ 2.087588] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1&lt;BR /&gt;[ 2.094849] usb usb1: Product: EHCI Host Controller&lt;BR /&gt;[ 2.099742] usb usb1: Manufacturer: Linux 5.4.24-hdl-eg4.1+g8cda0a19ad10 ehci_hcd&lt;BR /&gt;[ 2.107256] usb usb1: SerialNumber: ci_hdrc.0&lt;BR /&gt;[ 2.112373] hub 1-0:1.0: USB hub found&lt;BR /&gt;[ 2.116223] hub 1-0:1.0: 1 port detected&lt;BR /&gt;[ 2.121660] imx_usb 30b20000.usb: No over current polarity defined&lt;BR /&gt;[ 2.130925] ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;[ 2.135894] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2&lt;BR /&gt;[ 2.163572] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;[ 2.169209] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04&lt;BR /&gt;[ 2.177523] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1&lt;BR /&gt;[ 2.184781] usb usb2: Product: EHCI Host Controller&lt;BR /&gt;[ 2.189675] usb usb2: Manufacturer: Linux 5.4.24-hdl-eg4.1+g8cda0a19ad10 ehci_hcd&lt;BR /&gt;[ 2.197189] usb usb2: SerialNumber: ci_hdrc.1&lt;BR /&gt;[ 2.202269] hub 2-0:1.0: USB hub found&lt;BR /&gt;[ 2.206115] hub 2-0:1.0: 1 port detected&lt;BR /&gt;[ 2.212933] Goodix-TS 3-005d: 3-005d supply AVDD28 not found, using dummy regulator&lt;BR /&gt;[ 2.220790] Goodix-TS 3-005d: 3-005d supply VDDIO not found, using dummy regulator&lt;BR /&gt;[ 2.345738] Goodix-TS 3-005d: ID 911, version: 1060&lt;BR /&gt;[ 2.350770] Goodix-TS 3-005d: Direct firmware load for goodix_911_cfg.bin failed with error -2&lt;BR /&gt;[ 2.360705] Goodix-TS 3-005d: Falling back to sysfs fallback for: goodix_911_cfg.bin&lt;BR /&gt;[ 2.371524] rtc-pcf85063 3-0051: registered as rtc0&lt;BR /&gt;[ 2.376865] i2c /dev entries driver&lt;BR /&gt;[ 2.384433] watchdog: watchdog0 running and kernel based pre-userspace handler disabled&lt;BR /&gt;[ 2.392464] imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;[ 2.399265] Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;[ 2.403763] Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;[ 2.408913] Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;[ 2.414289] Bluetooth: HCI UART protocol LL registered&lt;BR /&gt;[ 2.419471] Bluetooth: HCI UART protocol Three-wire (H5) registered&lt;BR /&gt;[ 2.425969] Bluetooth: HCI UART protocol Marvell registered&lt;BR /&gt;[ 2.431637] usbcore: registered new interface driver btusb&lt;BR /&gt;[ 2.438248] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 2.444483] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 2.448852] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 2.456439] sdhci-esdhc-imx 30b40000.usdhc: Got CD GPIO&lt;BR /&gt;[ 2.461712] sdhci-esdhc-imx 30b40000.usdhc: Got WP GPIO&lt;BR /&gt;[ 2.573579] usb 2-1: new high-speed USB device number 2 using ci_hdrc&lt;BR /&gt;[ 2.638371] usb 2-1: New USB device found, idVendor=2001, idProduct=1a02, bcdDevice= 0.02&lt;BR /&gt;[ 2.646601] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3&lt;BR /&gt;[ 2.653787] usb 2-1: Product: DUB-E100&lt;BR /&gt;[ 2.657551] usb 2-1: Manufacturer: D-Link Corp.&lt;BR /&gt;[ 2.662442] usb 2-1: SerialNumber: 0023D9&lt;BR /&gt;[ 2.712102] mmc0: SDHCI controller on 30b40000.usdhc [30b40000.usdhc] using ADMA&lt;BR /&gt;[ 2.762957] mmc2: SDHCI controller on 30b60000.usdhc [30b60000.usdhc] using ADMA&lt;BR /&gt;[ 2.774264] caam 30900000.caam: device ID = 0x0a16030000000000 (Era &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;[ 2.780874] caam 30900000.caam: job rings = 3, qi = 0&lt;BR /&gt;[ 2.818598] caam algorithms registered in /proc/crypto&lt;BR /&gt;[ 2.827586] caam 30900000.caam: caam pkc algorithms registered in /proc/crypto&lt;BR /&gt;[ 2.837051] caam_jr 30901000.jr0: registering rng-caam&lt;BR /&gt;[ 2.864696] caam-snvs 30370000.caam-snvs: can't get snvs clock&lt;BR /&gt;[ 2.870625] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state&lt;BR /&gt;[ 2.880133] usbcore: registered new interface driver usbhid&lt;BR /&gt;[ 2.885746] usbhid: USB HID core driver&lt;BR /&gt;[ 2.893258] mmc2: new HS400 MMC card at address 0001&lt;BR /&gt;[ 2.900894] tlv320aic3x-codec 3-0018: Using deprecated property "gpio-reset", please update your DT&lt;BR /&gt;[ 2.904086] mmcblk2: mmc2:0001 Q2J54A 3.59 GiB&lt;BR /&gt;[ 2.910106] tlv320aic3x-codec 3-0018: 3-0018 supply IOVDD not found, using dummy regulator&lt;BR /&gt;[ 2.914998] mmcblk2boot0: mmc2:0001 Q2J54A partition 1 16.0 MiB&lt;BR /&gt;[ 2.922948] tlv320aic3x-codec 3-0018: 3-0018 supply DVDD not found, using dummy regulator&lt;BR /&gt;[ 2.929183] mmcblk2boot1: mmc2:0001 Q2J54A partition 2 16.0 MiB&lt;BR /&gt;[ 2.937147] tlv320aic3x-codec 3-0018: 3-0018 supply AVDD not found, using dummy regulator&lt;BR /&gt;[ 2.943314] mmcblk2rpmb: mmc2:0001 Q2J54A partition 3 512 KiB, chardev (245:0)&lt;BR /&gt;[ 2.951271] tlv320aic3x-codec 3-0018: 3-0018 supply DRVDD not found, using dummy regulator&lt;BR /&gt;[ 2.966851] tlv320aic3x-codec 3-0018: Invalid supply voltage(s) AVDD: -22, DVDD: -22&lt;BR /&gt;[ 2.972005] mmcblk2: p1 p2 p3 &amp;lt; p5 p6 p7 &amp;gt;&lt;BR /&gt;[ 2.980091] fsl-sai 308a0000.sai: failed to get mclk0 clock: -2&lt;BR /&gt;[ 2.991946] fsl-sai 308b0000.sai: failed to get mclk0 clock: -2&lt;BR /&gt;[ 3.006132] NET: Registered protocol family 26&lt;BR /&gt;[ 3.011511] NET: Registered protocol family 10&lt;BR /&gt;[ 3.027460] Segment Routing with IPv6&lt;BR /&gt;[ 3.031239] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver&lt;BR /&gt;[ 3.038068] NET: Registered protocol family 17&lt;BR /&gt;[ 3.042542] can: controller area network core (rev 20170425 abi 9)&lt;BR /&gt;[ 3.048867] NET: Registered protocol family 29&lt;BR /&gt;[ 3.053327] can: raw protocol (rev 20170425)&lt;BR /&gt;[ 3.057641] can: broadcast manager protocol (rev 20170425 t)&lt;BR /&gt;[ 3.063320] can: netlink gateway (rev 20190810) max_hops=1&lt;BR /&gt;[ 3.069144] Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;[ 3.074090] Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;[ 3.079293] Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;[ 3.083067] Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;[ 3.088416] Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;[ 3.093678] Bluetooth: BNEP socket layer initialized&lt;BR /&gt;[ 3.098654] Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;[ 3.104607] Bluetooth: HIDP socket layer initialized&lt;BR /&gt;[ 3.109650] lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;[ 3.114842] random: fast init done&lt;BR /&gt;[ 3.118790] Key type dns_resolver registered&lt;BR /&gt;[ 3.122861] asix 2-1:1.0 eth2: register 'asix' at usb-ci_hdrc.1-1, ASIX AX88772 USB 2.0 Ethernet, a8:63:7d:61:1b:40&lt;BR /&gt;[ 3.134316] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 1 supported-hw 0x4 0x2&lt;BR /&gt;[ 3.144216] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 648000 KHz&lt;BR /&gt;[ 3.152989] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 792000 KHz&lt;BR /&gt;[ 3.161805] Registering SWP/SWPB emulation handler&lt;BR /&gt;[ 3.166887] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 3.207927] imx_thermal tempmon: Extended Commercial CPU temperature grade - max:105C critical:100C passive:95C&lt;BR /&gt;[ 3.222139] rtc-pcf85063 3-0051: setting system clock to 2018-03-13T09:49:57 UTC (1520934597)&lt;BR /&gt;[ 3.231043] cfg80211: Loading compiled-in X.509 certificates for regulatory database&lt;BR /&gt;[ 3.241094] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'&lt;BR /&gt;[ 3.247811] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2&lt;BR /&gt;[ 3.256973] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db&lt;BR /&gt;[ 3.286271] ALSA device list:&lt;BR /&gt;[ 3.289250] No soundcards found.&lt;BR /&gt;[ 3.301881] EXT4-fs (mmcblk2p1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 3.310183] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.&lt;BR /&gt;[ 3.317526] devtmpfs: mounted&lt;BR /&gt;[ 3.321853] Freeing unused kernel memory: 1024K&lt;BR /&gt;[ 3.353834] Run /sbin/init as init process&lt;BR /&gt;INIT: version 2.96 booting&lt;BR /&gt;Framebuffer /dev/fb0 not detected&lt;BR /&gt;Boot splashscreen disabled&lt;BR /&gt;[ 3.839617] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.115764] EXT4-fs (mmcblk2p5): recovery complete&lt;BR /&gt;[ 4.121101] EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.129313] ext4 filesystem being mounted at /mnt/hos-state supports timestamps until 2038 (0x7fffffff)&lt;BR /&gt;[ 4.143868] EXT4-fs (mmcblk2p6): recovery complete&lt;BR /&gt;[ 4.148680] EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.161992] EXT4-fs (mmcblk2p7): recovery complete&lt;BR /&gt;[ 4.166842] EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[ 4.174991] ext4 filesystem being mounted at /mnt/hos-volatile supports timestamps until 2038 (0x7fffffff)&lt;BR /&gt;Starting udev&lt;BR /&gt;[ 4.270274] udevd[288]: starting version 3.2.9&lt;BR /&gt;[ 4.283003] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.290005] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.297011] random: udevd: uninitialized urandom read (16 bytes read)&lt;BR /&gt;[ 4.322600] udevd[289]: starting eudev-3.2.9&lt;BR /&gt;[ 4.579432] input: Goodix Capacitive TouchScreen as /devices/soc0/soc/30800000.aips-bus/30a50000.i2c/i2c-3/3-005d/input/input0&lt;BR /&gt;[ 4.632964] imx-sdma 30bd0000.sdma: loaded firmware 4.5&lt;BR /&gt;[ 5.349073] urandom_read: 4 callbacks suppressed&lt;BR /&gt;[ 5.349082] random: python3: uninitialized urandom read (24 bytes read)&lt;BR /&gt;[ 8.891462] random: dd: uninitialized urandom read (512 bytes read)&lt;BR /&gt;[ 9.142463] fec 30be0000.ethernet eth0: Unable to connect to phy&lt;BR /&gt;[ 9.212304] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 9.325802] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready&lt;BR /&gt;[ 9.413269] random: dbus-uuidgen: uninitialized urandom read (12 bytes read)&lt;BR /&gt;[ 9.573304] IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready&lt;BR /&gt;[ 9.582997] asix 2-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0xC1E1&lt;BR /&gt;[ 13.343621] random: crng init done&lt;/P&gt;&lt;P&gt;The board reboot after some seconds , Could you please help to fix that or do we miss something ?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Imy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 08:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1704196#M210721</guid>
      <dc:creator>ibenhassen</dc:creator>
      <dc:date>2023-08-14T08:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1705761#M210907</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208874"&gt;@ibenhassen&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please make sure to follow the OTA document properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please make sure to check that you have followed all the steps to do over the air properly, Please validate that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN12900" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://www.nxp.com/webapp/Download?colCode%3DAN12900&amp;amp;source=gmail&amp;amp;ust=1692259725483000&amp;amp;usg=AOvVaw2g8nPsdp1nJD97Yc9dmj3G"&gt;https://www.nxp.com/webapp/&lt;WBR /&gt;Download?colCode=AN12900&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please refer to this link for reference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope it helps!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sanket Parekh&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 12:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1705761#M210907</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-08-16T12:19:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1706664#M210998</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;Thanks for the response but We don't use OPTEE and the issue is not that . In fact , you gave a response for something&amp;nbsp; else than my issue . WE have an issue related to serial console which blocked the getty to start.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 13:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1706664#M210998</guid>
      <dc:creator>ibenhassen</dc:creator>
      <dc:date>2023-08-17T13:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1707595#M211065</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208874"&gt;@ibenhassen&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;I hope you are doing well&lt;/DIV&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;DIV&gt;My sincere apology for not getting your query.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;If you are using the EVK, kindly try the demo images from the&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&amp;amp;source=gmail&amp;amp;ust=1692450307383000&amp;amp;usg=AOvVaw0wSI3R49nKVLUzWdTDkRHT"&gt;Embedded Linux for i.MX Applications Processors&lt;/A&gt;&amp;nbsp;and share the result.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;In case of failure, kindly check the power/clock-related information from&amp;nbsp;&lt;U&gt;section 4. Avoiding board bring-up problems&lt;/U&gt;&amp;nbsp;from the&amp;nbsp;&lt;U&gt;Hardware Development Guide for i.MX7Dual&lt;/U&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;U&gt;and 7Solo Applications Processors&lt;/U&gt;&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX7DSHDG" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://www.nxp.com/webapp/Download?colCode%3DIMX7DSHDG&amp;amp;source=gmail&amp;amp;ust=1692450307383000&amp;amp;usg=AOvVaw10BDH8ot1ex680mC3RD_we"&gt;IMX7DSHDG&lt;/A&gt;&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;If the issue is not yet resolved kindly share the device tree you are using to further&amp;nbsp;debug the issue.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Thanks &amp;amp; Regards&lt;/DIV&gt;
&lt;DIV&gt;Sanket Parekh&lt;/DIV&gt;</description>
      <pubDate>Fri, 18 Aug 2023 14:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1707595#M211065</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-08-18T14:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1748695#M214909</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Unfortunately, the issue is not fixed&amp;nbsp; and I got this:&lt;/P&gt;&lt;P&gt;[ 5.928652] RAMDISK: gzip image found at block 0&lt;BR /&gt;[ 5.933380] RAMDISK: gzip decompressor not configured!&lt;BR /&gt;[ 5.938526] Invalid ramdisk decompression routine. Select appropriate config option.&lt;BR /&gt;[ 5.946386] Kernel panic - not syncing: Could not decompress initial ramdisk image.&lt;BR /&gt;[ 5.954067] CPU0: stopping&lt;BR /&gt;[ 5.956789] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.4.24-hdl-eg4.1+g0c20292c4d44 #1&lt;BR /&gt;[ 5.964796] Hardware name: Freescale i.MX7 Dual (Device Tree)&lt;BR /&gt;[ 5.970545] Backtrace:&lt;BR /&gt;[ 5.973016] [&amp;lt;8010e59c&amp;gt;] (dump_backtrace) from [&amp;lt;8010e930&amp;gt;] (show_stack+0x20/0x24)&lt;BR /&gt;[ 5.980594] r7:812053f4 r6:60000193 r5:00000000 r4:81312478&lt;BR /&gt;[ 5.986266] [&amp;lt;8010e910&amp;gt;] (show_stack) from [&amp;lt;80bc34b0&amp;gt;] (dump_stack+0x98/0xac)&lt;BR /&gt;[ 5.993500] [&amp;lt;80bc3418&amp;gt;] (dump_stack) from [&amp;lt;8011202c&amp;gt;] (handle_IPI+0x3e4/0x410)&lt;BR /&gt;[ 6.000903] r7:812053f4 r6:00000004 r5:81317cc4 r4:81123ed4&lt;BR /&gt;[ 6.006574] [&amp;lt;80111c48&amp;gt;] (handle_IPI) from [&amp;lt;80102364&amp;gt;] (gic_handle_irq+0x9c/0xa0)&lt;BR /&gt;[ 6.014153] r10:00000001 r9:81201e60 r8:c0803000 r7:c0802000 r6:c080200c r5:81257334&lt;BR /&gt;[ 6.021985] r4:812056dc&lt;BR /&gt;[ 6.024528] [&amp;lt;801022c8&amp;gt;] (gic_handle_irq) from [&amp;lt;80101a8c&amp;gt;] (__irq_svc+0x6c/0xa8)&lt;BR /&gt;[ 6.032015] Exception stack(0x81201e60 to 0x81201ea8)&lt;BR /&gt;[ 6.037077] 1e60: 00000000 bf6bd900 00000001 81200000 8120b02c 00000001 62e39f23 813184d0&lt;BR /&gt;[ 6.045264] 1e80: 00000001 bf6b9778 00000001 81201efc 81201e78 81201eb0 801ba91c 808ca360&lt;BR /&gt;[ 6.053446] 1ea0: 20000113 ffffffff&lt;BR /&gt;[ 6.056946] r9:81200000 r8:00000001 r7:81201e94 r6:ffffffff r5:20000113 r4:808ca360&lt;BR /&gt;[ 6.064700] [&amp;lt;808ca1e4&amp;gt;] (cpuidle_enter_state) from [&amp;lt;808ca83c&amp;gt;] (cpuidle_enter+0x38/0x48)&lt;BR /&gt;[ 6.072974] r10:bf6b9778 r9:8120b02c r8:81123770 r7:81204f64 r6:00000002 r5:8120b02c&lt;BR /&gt;[ 6.080806] r4:bf6b9778&lt;BR /&gt;[ 6.083352] [&amp;lt;808ca804&amp;gt;] (cpuidle_enter) from [&amp;lt;80164e00&amp;gt;] (call_cpuidle+0x30/0x48)&lt;BR /&gt;[ 6.091016] r7:81204f64 r6:81204f28 r5:00000000 r4:81200000&lt;BR /&gt;[ 6.096685] [&amp;lt;80164dd0&amp;gt;] (call_cpuidle) from [&amp;lt;8016521c&amp;gt;] (do_idle+0x1fc/0x2a8)&lt;BR /&gt;[ 6.104006] [&amp;lt;80165020&amp;gt;] (do_idle) from [&amp;lt;801655f0&amp;gt;] (cpu_startup_entry+0x28/0x2c)&lt;BR /&gt;[ 6.111585] r10:bfffca00 r9:81074a40 r8:00000001 r7:00000000 r6:8131b880 r5:00000002&lt;BR /&gt;[ 6.119418] r4:000000ce&lt;BR /&gt;[ 6.121963] [&amp;lt;801655c8&amp;gt;] (cpu_startup_entry) from [&amp;lt;80bdb428&amp;gt;] (rest_init+0xd4/0xdc)&lt;BR /&gt;[ 6.129718] [&amp;lt;80bdb354&amp;gt;] (rest_init) from [&amp;lt;81000b74&amp;gt;] (arch_call_rest_init+0x18/0x1c)&lt;BR /&gt;[ 6.137639] r5:00000001 r4:8131b8d4&lt;BR /&gt;[ 6.141225] [&amp;lt;81000b5c&amp;gt;] (arch_call_rest_init) from [&amp;lt;810010c0&amp;gt;] (start_kernel+0x4d0/0x508)&lt;BR /&gt;[ 6.149585] [&amp;lt;81000bf0&amp;gt;] (start_kernel) from [&amp;lt;00000000&amp;gt;] (0x0)&lt;BR /&gt;[ 6.155516] r10:10c5387d r9:410fc075 r8:bd606000 r7:00000000 r6:10c0387d r5:00000051&lt;BR /&gt;[ 6.163348] r4:81000330&lt;BR /&gt;[ 6.165898] ---[ end Kernel panic - not syncing: Could not decompress initial ramdisk image. ]---&lt;/P&gt;&lt;P&gt;Any help please ?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 11:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1748695#M214909</guid>
      <dc:creator>ibenhassen</dc:creator>
      <dc:date>2023-10-30T11:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1748697#M214910</link>
      <description>&lt;P&gt;there is the device tree,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 11:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1748697#M214910</guid>
      <dc:creator>ibenhassen</dc:creator>
      <dc:date>2023-10-30T11:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D kernel upgrade 5.4 issue with the console boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1749134#M214956</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208874"&gt;@ibenhassen&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;This usually happens when the kernel can't decompress the initial ramdisk image during the boot process.&lt;BR /&gt;Please make sure to check the ramdisk configuration matches in the kernel.&lt;BR /&gt;Please make sure to check these configurations in the defconfig file.&lt;BR /&gt;If possible can you check the same using the latest kernel by rebuilding that and then check it?&lt;/P&gt;
&lt;P&gt;Thanks and regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Tue, 31 Oct 2023 04:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-kernel-upgrade-5-4-issue-with-the-console-boot/m-p/1749134#M214956</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-31T04:11:38Z</dc:date>
    </item>
  </channel>
</rss>