<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VMware Ubuntu LTIB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VMware-Ubuntu-LTIB/m-p/155226#M2106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just downloaded the Ubuntu VMware image (&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;IMX53_QSB_UBUNTU_VM&lt;/A&gt;)&amp;nbsp;from:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The documentation says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The LTIB directory for the i.MX53 Linux BSP is located at:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/home/lucid/ltib/"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've looked in the /home/lucid directory but ltib is not there. The documentation suggests that it should be there and already configured for the i.MX53 board ready to output the images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have I got something wrong here? Hope someone can help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Apr 2012 19:42:51 GMT</pubDate>
    <dc:creator>contra</dc:creator>
    <dc:date>2012-04-19T19:42:51Z</dc:date>
    <item>
      <title>VMware Ubuntu LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VMware-Ubuntu-LTIB/m-p/155226#M2106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just downloaded the Ubuntu VMware image (&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;IMX53_QSB_UBUNTU_VM&lt;/A&gt;)&amp;nbsp;from:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The documentation says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The LTIB directory for the i.MX53 Linux BSP is located at:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/home/lucid/ltib/"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've looked in the /home/lucid directory but ltib is not there. The documentation suggests that it should be there and already configured for the i.MX53 board ready to output the images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have I got something wrong here? Hope someone can help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2012 19:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VMware-Ubuntu-LTIB/m-p/155226#M2106</guid>
      <dc:creator>contra</dc:creator>
      <dc:date>2012-04-19T19:42:51Z</dc:date>
    </item>
  </channel>
</rss>