<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: No Output on HDMI Signal for IMX8MP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1697693#M210146</link>
    <description>&lt;P&gt;pls share the logfile and give me the result when you use command dmesg | grep drm&lt;/P&gt;</description>
    <pubDate>Wed, 02 Aug 2023 14:22:37 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-08-02T14:22:37Z</dc:date>
    <item>
      <title>No Output on HDMI Signal for IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1697622#M210136</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;my team and I are using a 7" display from Actron (Model No. ETML070023UDRA, Resolution 800x480@60) and a Phytec i.MX8MP board running a Yocto system (&lt;EM&gt;Yogurt Vendor xwayland (Phytec Vendor Distribution) BSP-Yocto-FSL-i.MX8MP-PD21.1.3&lt;/EM&gt;).&lt;/P&gt;&lt;P&gt;The display works fine when we plug it in on a laptop and the board also correctly displays output on our monitors (benq) but when we connect the display with the board it does not react at all.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;xrandr &lt;/EM&gt;and &lt;EM&gt;xrandr --listmonitors&lt;/EM&gt; only prints&lt;EM&gt; "Can't open Display"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;We've also tried setting the mode within the &lt;EM&gt;/etc/xdg/weston/weston.ini&lt;/EM&gt; file and restarting weston/ the board but that did not have any effect either.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[output]
name=HDMI-A-1
mode=800x480&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another idea we tried is updating the u-boot environment via:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;env set video HDMI-A-1:800x640M@60D
env save
boot&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But that did not have any effect on the system. We also tried different options like the following with no luck either.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;env set video mxcfb0,dev=hdmi,800x480@60,if=RGB24&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have any ideas what we missed or what we can try? We can also provide further information if needed. Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 12:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1697622#M210136</guid>
      <dc:creator>bc_th</dc:creator>
      <dc:date>2023-08-02T12:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: No Output on HDMI Signal for IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1697693#M210146</link>
      <description>&lt;P&gt;pls share the logfile and give me the result when you use command dmesg | grep drm&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 14:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1697693#M210146</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-02T14:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: No Output on HDMI Signal for IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1698262#M210182</link>
      <description>&lt;P&gt;This is the log you mentioned&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    4.062709] imx-drm display-subsystem: trying to bring up master
[    4.062714] imx-drm display-subsystem: Looking for component 0
[    4.062721] imx-drm display-subsystem: Looking for component 1
[    4.062732] imx-drm display-subsystem: found component imx-lcdifv3-crtc.1, duplicate 0
[    4.062739] imx-drm display-subsystem: Looking for component 2
[    4.062745] imx-drm display-subsystem: Looking for component 3
[    4.062879] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    4.069525] [drm] No driver support for vblank timestamp query.
[    4.075490] imx-drm display-subsystem: binding imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    4.075538] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    4.083489] imx-drm display-subsystem: binding imx-lcdifv3-crtc.1 (ops lcdifv3_crtc_ops)
[    4.083556] imx-drm display-subsystem: bound imx-lcdifv3-crtc.1 (ops lcdifv3_crtc_ops)
[    4.091511] imx-drm display-subsystem: binding 32c00000.bus:ldb@32ec005c (ops imx8mp_ldb_ops)
[    4.098185] imx-drm display-subsystem: bound 32c00000.bus:ldb@32ec005c (ops imx8mp_ldb_ops)
[    4.106620] imx-drm display-subsystem: binding 32fd8000.hdmi (ops dw_hdmi_imx_ops)
[    4.126191] imx-drm display-subsystem: bound 32fd8000.hdmi (ops dw_hdmi_imx_ops)
[    4.134412] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[    4.525235] imx-drm display-subsystem: HDMI-A-1: EDID is invalid:
[    4.706411] imx-drm display-subsystem: fb0: imx-drmdrmfb frame buffer device&lt;/LI-CODE&gt;</description>
      <pubDate>Thu, 03 Aug 2023 05:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1698262#M210182</guid>
      <dc:creator>bc_th</dc:creator>
      <dc:date>2023-08-03T05:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: No Output on HDMI Signal for IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1698363#M210195</link>
      <description>&lt;P&gt;did you use nxp bsp or your own SW? refer to your logfile:&lt;/P&gt;
&lt;PRE class="lia-code-sample  language-markup"&gt;&lt;CODE&gt;imx-drm display-subsystem: HDMI-A-1: EDID is invalid:&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;for HDMI, you don't need add this in the uboot, pls share dtb file you use and tell me what pixel clock of your HDMI you use&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 07:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1698363#M210195</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-08-03T07:11:09Z</dc:date>
    </item>
    <item>
      <title>Re: No Output on HDMI Signal for IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1698572#M210214</link>
      <description>&lt;P&gt;We fixed the issue. The default mode line that we got from connecting the display to the board was incorrect.&lt;BR /&gt;We created a mode with&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;cvt 800 480 60&lt;/LI-CODE&gt;&lt;P&gt;and then put the &lt;STRONG&gt;whole&lt;/STRONG&gt; resulting String into the &lt;EM&gt;weston.ini&lt;/EM&gt; so it looks like this:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[output]
name=HDMI-A-1
mode=29.50  800 824 896 992  480 483 493 500 -hsync +vsync&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;After a restart the board could interact with the display via HDMI.&lt;BR /&gt;&lt;BR /&gt;Thanks for the previous help!&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 11:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Output-on-HDMI-Signal-for-IMX8MP/m-p/1698572#M210214</guid>
      <dc:creator>bc_th</dc:creator>
      <dc:date>2023-08-03T11:24:12Z</dc:date>
    </item>
  </channel>
</rss>