<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx28   DDR 256 MB 2.6.35.13 fsl</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244494#M21009</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if tried what you said&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;./ltib -m prep -p imx-bootlets-src&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;After editing :&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;./ltib -m scbuild -p imx-bootlets-src&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;./ltib -m scdeploy -p imx-bootlets-src&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt; I did not modify anything but&amp;nbsp; it happened that now the system try to boot in mDDR instead of DDR2 and dont work anymore anymore .do you know why ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then i came back to old version of VM that i had stored : what i want to do is to change kernel command line ( add&amp;nbsp;&amp;nbsp; mem=256K ) . if tried to change the four bootstream line in ltib&amp;nbsp; but&amp;nbsp; when i build on a sdcard , modification does not appears&amp;nbsp; .&lt;/P&gt;&lt;P&gt;do you know why ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Feb 2014 16:04:34 GMT</pubDate>
    <dc:creator>jeanletutour</dc:creator>
    <dc:date>2014-02-21T16:04:34Z</dc:date>
    <item>
      <title>imx28   DDR 256 MB 2.6.35.13 fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244492#M21007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i don't manage to configurate ltib , and&amp;nbsp; linux software , to be able to see the 256 MB&amp;nbsp; of ram.&amp;nbsp;&amp;nbsp; the system is still seeing&amp;nbsp; 128 MB &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;has anybody had this problem ?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 11:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244492#M21007</guid>
      <dc:creator>jeanletutour</dc:creator>
      <dc:date>2014-02-19T11:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx28   DDR 256 MB 2.6.35.13 fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244493#M21008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Generally (for DRAM initialization when stand alone applications are debugged) &lt;/P&gt;&lt;P&gt;one can use the DDR tool, mentioned under item 3. below.&lt;/P&gt;&lt;P&gt;But often customers need to adapt Freescale BSP(s)&amp;nbsp; for their boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://www.freescale.com/webapp/Download?colCode=L2.6.35_1.1.0_ER_SOURCE&amp;amp;appType=license&amp;amp;location=null"&gt;https://www.freescale.com/webapp/Download?colCode=L2.6.35_1.1.0_ER_SOURCE&amp;amp;appType=license&amp;amp;location=null&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at the following hints how to change i.MX28 DDR seetings in Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. DDR initialization.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I.MX28 DRAM system under Linux is initialized in bootlets.&lt;/P&gt;&lt;P&gt;Source codes are located in &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;ltib&amp;gt;/rpm/BUILD/imx-bootlets-src/boot_prep/init-mx28.c&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To get it, please use the next commands&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;./ltib -m prep -p imx-bootlets-src&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After editing :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;./ltib -m scbuild -p imx-bootlets-src&lt;/P&gt;&lt;P&gt;./ltib -m scdeploy -p imx-bootlets-src&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Linux kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following kernel files contain support for Linux CPUFREQ (frequency&lt;/P&gt;&lt;P&gt;scaling) feature :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;ltib&amp;gt;/rpm/BUILD/linux-2.6.31/arch/arm/mach-mx28/emi_settings.c&lt;/P&gt;&lt;P&gt;&amp;lt;ltib&amp;gt;/rpm/BUILD/linux-2.6.31/arch/arm/mach-mx28/emi.S &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Tools. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use the tool, linked below, to get optimal settings for Your SDRAM :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board_bring-up_and_DDR_initialization_tools :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="1455" data-objecttype="102" href="https://community.freescale.com/docs/DOC-1455"&gt;https://community.freescale.com/docs/DOC-1455&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.&lt;/P&gt;&lt;P&gt;To apply the MFG tool for firmware update, please use option&amp;nbsp; Build mfg firmware &lt;/P&gt;&lt;P&gt;under LTIB. It builds special Linux version, that is intended to be loaded by the MFG tool &lt;/P&gt;&lt;P&gt;to SDRAM of a target system and interface with the MFG in order to get target &lt;/P&gt;&lt;P&gt;images and write them to SD or NAND. This version is based on the same DRAM &lt;/P&gt;&lt;P&gt;settings as the main one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also please look at section 2.5 (Building the Manufacturing Firmware) of the &lt;/P&gt;&lt;P&gt;"i.MX28_Linux_BSP_UG.pdf."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After LTIB completes the build, updater.sb, updater_ivt.sb, and &lt;/P&gt;&lt;P&gt;initramfs.cpio.gz should be created.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;File updater_ivt.sb and initramfs.cpio.gz should be located in &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Mfgtools&amp;gt;\Profiles\MX28 Linux Update\OS Firmware\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Files imx28_ivt_linux.sb, imx28_ivt_uboot.sb (if needed), and rootfs.tar.bz2 &lt;/P&gt;&lt;P&gt;should be located in&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Mfgtools&amp;gt;\Profiles\MX28 Linux Update\OS Firmware\files\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5. Process for updating Linux DRAM configuration :&lt;/P&gt;&lt;P&gt;- please use the mentioned DDR initialization tool to get optimal settings for&lt;/P&gt;&lt;P&gt;&amp;nbsp; the SDRAM ;&lt;/P&gt;&lt;P&gt;- update all the required parameters in the file init-mx28.c, based on tools&lt;/P&gt;&lt;P&gt;&amp;nbsp; results ;&lt;/P&gt;&lt;P&gt;- update all the required parameters in the file emi_settings.c, based on tools &lt;/P&gt;&lt;P&gt;&amp;nbsp; results ;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;- rebuild the kernel, bootloader, and mfg firmware.&amp;nbsp; &lt;/P&gt;&lt;P&gt;- copy updater_ivt.sb, imx28_ivt_linux.sb, initramfs.cpio.gz, and rootfs.tar.bz2 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; to&amp;nbsp;&amp;nbsp; proper directories of the MFG tool.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 03:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244493#M21008</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-02-20T03:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx28   DDR 256 MB 2.6.35.13 fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244494#M21009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if tried what you said&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;./ltib -m prep -p imx-bootlets-src&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;After editing :&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;./ltib -m scbuild -p imx-bootlets-src&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;./ltib -m scdeploy -p imx-bootlets-src&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt; I did not modify anything but&amp;nbsp; it happened that now the system try to boot in mDDR instead of DDR2 and dont work anymore anymore .do you know why ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then i came back to old version of VM that i had stored : what i want to do is to change kernel command line ( add&amp;nbsp;&amp;nbsp; mem=256K ) . if tried to change the four bootstream line in ltib&amp;nbsp; but&amp;nbsp; when i build on a sdcard , modification does not appears&amp;nbsp; .&lt;/P&gt;&lt;P&gt;do you know why ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 16:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244494#M21009</guid>
      <dc:creator>jeanletutour</dc:creator>
      <dc:date>2014-02-21T16:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx28   DDR 256 MB 2.6.35.13 fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244495#M21010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Memory initialization and size are configured in bootlets ; available kernel command line parameters are &lt;BR /&gt;described in section 5.1.1 (Setting Up Kernel Command Line) of "MX28_EVK_Linux_User_Guide.pdf".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jun 2014 03:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-DDR-256-MB-2-6-35-13-fsl/m-p/244495#M21010</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-06-02T03:40:15Z</dc:date>
    </item>
  </channel>
</rss>