<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MP FlexSPI drivers in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-FlexSPI-drivers/m-p/1695345#M209891</link>
    <description>&lt;P&gt;you can refer to the flexSPI driver in the imxRT SDK&lt;/P&gt;</description>
    <pubDate>Sun, 30 Jul 2023 03:55:26 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-07-30T03:55:26Z</dc:date>
    <item>
      <title>IMX8MP FlexSPI drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-FlexSPI-drivers/m-p/1695329#M209889</link>
      <description>&lt;P&gt;Good afternoon.&lt;/P&gt;&lt;P&gt;Can you please tell me if there are ready-made drivers for working with FlexSPI (+ DMA) for IMX8MP for CortexM7? I found a similar implementation and examples for iMXRT11xx (fsl_flexspi_nor_flash.c). Is it possible to adapt these libraries for the current platform or there may be some problems with this besides hardware defenitions? Or maybe somewhere there are similar examples for working with QuadSPI using FlexSPI?&lt;/P&gt;</description>
      <pubDate>Sat, 29 Jul 2023 09:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-FlexSPI-drivers/m-p/1695329#M209889</guid>
      <dc:creator>Stan88</dc:creator>
      <dc:date>2023-07-29T09:47:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP FlexSPI drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-FlexSPI-drivers/m-p/1695345#M209891</link>
      <description>&lt;P&gt;you can refer to the flexSPI driver in the imxRT SDK&lt;/P&gt;</description>
      <pubDate>Sun, 30 Jul 2023 03:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-FlexSPI-drivers/m-p/1695345#M209891</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-07-30T03:55:26Z</dc:date>
    </item>
  </channel>
</rss>