<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX8 X Secure Debug Usage Guide</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1693188#M209726</link>
    <description>&lt;P&gt;Thanks, good to know that the IMX8X secure debug is similar in function to the IMX8M.&lt;BR /&gt;&lt;BR /&gt;Looking into this more it appears that steps are provided for secure debug usage in the application note AN12631 (section 6)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12631.pdf" target="_blank" rel="nofollow noopener noreferrer"&gt;&lt;STRONG&gt;Normal and Secure Debug for i.MX8/8X Family of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Though that application note references Lauterbach debugger scripts for handling the secure debug handshaking. Which sounds like those scripts are only available via direct contact to Lauterbach or by opening a support request with NXP for those script files.&lt;/P&gt;&lt;P&gt;That info was found here: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 15:12:27 GMT</pubDate>
    <dc:creator>wdcrith</dc:creator>
    <dc:date>2023-07-26T15:12:27Z</dc:date>
    <item>
      <title>iMX8 X Secure Debug Usage Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1692493#M209678</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I am working on a custom piece of hardware which uses the iMX8 X (specifically the IMX8 DX) SOC. I am looking for guidance on how to test out the secure debug (secure JTAG) function of the processor.&lt;/P&gt;&lt;P&gt;I have found references to other application notes aimed at the IMX8M, but no such document for the IMX8 X.&lt;/P&gt;&lt;P&gt;Help in locating the correct document or usage guide would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 21:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1692493#M209678</guid>
      <dc:creator>wdcrith</dc:creator>
      <dc:date>2023-07-25T21:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 X Secure Debug Usage Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1693158#M209725</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is security reference manual that need nda to access but in general the JTAG is the same as MX8M.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 14:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1693158#M209725</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-07-26T14:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 X Secure Debug Usage Guide</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1693188#M209726</link>
      <description>&lt;P&gt;Thanks, good to know that the IMX8X secure debug is similar in function to the IMX8M.&lt;BR /&gt;&lt;BR /&gt;Looking into this more it appears that steps are provided for secure debug usage in the application note AN12631 (section 6)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12631.pdf" target="_blank" rel="nofollow noopener noreferrer"&gt;&lt;STRONG&gt;Normal and Secure Debug for i.MX8/8X Family of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Though that application note references Lauterbach debugger scripts for handling the secure debug handshaking. Which sounds like those scripts are only available via direct contact to Lauterbach or by opening a support request with NXP for those script files.&lt;/P&gt;&lt;P&gt;That info was found here: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 15:12:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-X-Secure-Debug-Usage-Guide/m-p/1693188#M209726</guid>
      <dc:creator>wdcrith</dc:creator>
      <dc:date>2023-07-26T15:12:27Z</dc:date>
    </item>
  </channel>
</rss>