<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8MP operating range details confirmation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-operating-range-details-confirmation/m-p/1692764#M209697</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;I would like to know about different modes like&amp;nbsp;nominal,&amp;nbsp;overdrive, and Super overdrive which are for VDD_ARM. There is a specific frequency mentioned for each mode. So I just need to ensure that it is okay to reduce the frequency to 1.2GHz while using the&amp;nbsp;Super overdrive mode. Please confirm.&lt;BR /&gt;Also, if I am using&amp;nbsp;Super overdrive mode for VDD_ARM then is there any issue/dependency to use the nominal mode in other power rails like&amp;nbsp;Arm PLL supply voltage?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Bino Mani&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 06:55:37 GMT</pubDate>
    <dc:creator>bino</dc:creator>
    <dc:date>2023-07-26T06:55:37Z</dc:date>
    <item>
      <title>i.MX8MP operating range details confirmation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-operating-range-details-confirmation/m-p/1692764#M209697</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;I would like to know about different modes like&amp;nbsp;nominal,&amp;nbsp;overdrive, and Super overdrive which are for VDD_ARM. There is a specific frequency mentioned for each mode. So I just need to ensure that it is okay to reduce the frequency to 1.2GHz while using the&amp;nbsp;Super overdrive mode. Please confirm.&lt;BR /&gt;Also, if I am using&amp;nbsp;Super overdrive mode for VDD_ARM then is there any issue/dependency to use the nominal mode in other power rails like&amp;nbsp;Arm PLL supply voltage?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Bino Mani&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 06:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-operating-range-details-confirmation/m-p/1692764#M209697</guid>
      <dc:creator>bino</dc:creator>
      <dc:date>2023-07-26T06:55:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP operating range details confirmation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-operating-range-details-confirmation/m-p/1693771#M209745</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183605"&gt;@bino&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;While using the super overdrive mode, one can reduce the frequency but cannot exceed the operating range of the frequency.&lt;/P&gt;
&lt;P&gt;Also, when&amp;nbsp;the super overdrive mode is used for VDD_ARM, &lt;SPAN&gt;&lt;SPAN class="ui-provider fz b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;VDD_ARM_PLL_0P8 shall be set as 0.95V. However, since&amp;nbsp;VDD_ARM_PLL_0P8 comes from the same power source -VDD_SOC for all 0P8 peripherals, all PLL and peripherals will be powered from the same 0.95V power source no matter whether they are running at overdrive mode or not.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider fz b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;I hope it helps.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jul 2023 04:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-operating-range-details-confirmation/m-p/1693771#M209745</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-07-27T04:16:09Z</dc:date>
    </item>
  </channel>
</rss>