<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USBCompositeHost Example in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USBCompositeHost-Example/m-p/1692752#M209696</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMXRT1170-EVK board.In SDK file,&lt;/P&gt;&lt;P&gt;I run this example "Usb_device_composite_cdc_vcom_cdc_vcom".It's working fine.but my requirment is to run USB Host as Compostie.In SDK I didn't find related compostie usb host example.&lt;/P&gt;&lt;P&gt;Q1. Is there any example related to Composite Host?&lt;/P&gt;&lt;P&gt;Q2. If not, what can be modified in the existing above example?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thankyou&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 06:45:09 GMT</pubDate>
    <dc:creator>smartpavan333</dc:creator>
    <dc:date>2023-07-26T06:45:09Z</dc:date>
    <item>
      <title>USBCompositeHost Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USBCompositeHost-Example/m-p/1692752#M209696</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMXRT1170-EVK board.In SDK file,&lt;/P&gt;&lt;P&gt;I run this example "Usb_device_composite_cdc_vcom_cdc_vcom".It's working fine.but my requirment is to run USB Host as Compostie.In SDK I didn't find related compostie usb host example.&lt;/P&gt;&lt;P&gt;Q1. Is there any example related to Composite Host?&lt;/P&gt;&lt;P&gt;Q2. If not, what can be modified in the existing above example?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thankyou&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 06:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USBCompositeHost-Example/m-p/1692752#M209696</guid>
      <dc:creator>smartpavan333</dc:creator>
      <dc:date>2023-07-26T06:45:09Z</dc:date>
    </item>
    <item>
      <title>Re: USBCompositeHost Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USBCompositeHost-Example/m-p/1693306#M209731</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206672"&gt;@smartpavan333&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;What do you mean with a "composite host"? I believe that, by definition, only a device is capable of having two interfaces, which a host will then manage separately as two devices. I don't thing a "composite host" is within USB specification and therefore, it would not be possible. This is why you can't find a USB example code of what you search for.&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 19:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USBCompositeHost-Example/m-p/1693306#M209731</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-07-26T19:22:31Z</dc:date>
    </item>
  </channel>
</rss>