<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: kernel 3.10.9 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/kernel-3-10-9/m-p/244336#M20956</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed to fix it.&lt;/P&gt;&lt;P&gt;The problem was that I was missing the imx6q-sabresd.dtb file in the FAT partition.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Dec 2013 00:53:04 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2013-12-05T00:53:04Z</dc:date>
    <item>
      <title>kernel 3.10.9</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-3-10-9/m-p/244335#M20955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the latest kernel in 1.5 Yocto release (3.10.9) on a Sabre SD board.&lt;/P&gt;&lt;P&gt;I add PREFERRED_VERSION_linux-imx_mx6 = "3.10.9" in my local.conf and everything compiles fine.&lt;/P&gt;&lt;P&gt;But when I bootup I get following (it hangs when the kernel should be started):&lt;/P&gt;&lt;P&gt;reading uImage&lt;/P&gt;&lt;P&gt;5092288 bytes read in 272 ms (17.9 MiB/s)&lt;/P&gt;&lt;P&gt;Booting from mmc ...&lt;/P&gt;&lt;P&gt;reading imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;** Unable to read file imx6q-sabresd.dtb **&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 12000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.10.9-1.0.0_alpha+gdbf364&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 5092224 Bytes = 4.9 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;(hangs here)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to build a kernel direct from the Linux tree (version 3.8.0-rc7) and got the same problem.&lt;/P&gt;&lt;P&gt;reading uImage&lt;/P&gt;&lt;P&gt;3960872 bytes read in 215 ms (17.6 MiB/s)&lt;/P&gt;&lt;P&gt;Booting from mmc ...&lt;/P&gt;&lt;P&gt;reading imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;18526 bytes read in 18 ms (1004.9 KiB/s)&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 12000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.8.0-rc7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 3960808 Bytes = 3.8 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 13000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x13000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 13000000, end 1300785d&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;(hangs here)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone who managed to boot the latest kernel version &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2013 23:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-3-10-9/m-p/244335#M20955</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2013-12-04T23:45:35Z</dc:date>
    </item>
    <item>
      <title>Re: kernel 3.10.9</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-3-10-9/m-p/244336#M20956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed to fix it.&lt;/P&gt;&lt;P&gt;The problem was that I was missing the imx6q-sabresd.dtb file in the FAT partition.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2013 00:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-3-10-9/m-p/244336#M20956</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2013-12-05T00:53:04Z</dc:date>
    </item>
  </channel>
</rss>