<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX clock domain in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1690195#M209483</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I also didn't understand that there are 4 domains.&lt;/P&gt;&lt;P&gt;"3.2.1.1 Features" of Resource Domain COntroller(RDC) in i.MX7D reference manual written as follews.&lt;/P&gt;&lt;P&gt;Assignment of cores, bus masters, peripherals, and memory regions to a resource domain.&lt;/P&gt;&lt;P&gt;Four of these ?&lt;/P&gt;&lt;P&gt;But it dosen't write which one is domain0.&lt;/P&gt;</description>
    <pubDate>Fri, 21 Jul 2023 07:44:47 GMT</pubDate>
    <dc:creator>tamotsu</dc:creator>
    <dc:date>2023-07-21T07:44:47Z</dc:date>
    <item>
      <title>IMX clock domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1377806#M183608</link>
      <description>&lt;P&gt;When I read the datesheet of IMX8mq about the CCM.&lt;/P&gt;&lt;P&gt;1.I can't understand the clock domain usage and why the same clock have 4 domain setting(for example CCM_PLL_CTRLn has setting1 ~setting3).The 4 domain settings of one clock are working at the same time?&lt;/P&gt;&lt;P&gt;2.What is the usage of PLL domain settings and CCGR domain settings?&lt;/P&gt;&lt;P&gt;em......NXP's datasheets are hard to understand! &lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 28 Nov 2021 09:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1377806#M183608</guid>
      <dc:creator>justinfei</dc:creator>
      <dc:date>2021-11-28T09:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX clock domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1377827#M183614</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for domain usage one can look at description in sect.5.1.5.7 Access control, sect.5.1.6.2 PLL Interface,&lt;/P&gt;
&lt;P&gt;sect.5.2.4.2 Low power mode&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_3" href="https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 29 Nov 2021 00:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1377827#M183614</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-29T00:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX clock domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1690195#M209483</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I also didn't understand that there are 4 domains.&lt;/P&gt;&lt;P&gt;"3.2.1.1 Features" of Resource Domain COntroller(RDC) in i.MX7D reference manual written as follews.&lt;/P&gt;&lt;P&gt;Assignment of cores, bus masters, peripherals, and memory regions to a resource domain.&lt;/P&gt;&lt;P&gt;Four of these ?&lt;/P&gt;&lt;P&gt;But it dosen't write which one is domain0.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jul 2023 07:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-clock-domain/m-p/1690195#M209483</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2023-07-21T07:44:47Z</dc:date>
    </item>
  </channel>
</rss>