<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC scaling in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688222#M209293</link>
    <description>&lt;P&gt;I have 1V8 on VREFH and I can't change it.&lt;BR /&gt;The ADC would hypothetically read up to 3.84V, but losing the [3.3, 3.84]V range (thus losing some resolution) will not be a problem.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What I'm worried about is whether this scaling factor introduces a voltage divider, forcing me to use a voltage buffer not to distort the signal.&lt;/P&gt;&lt;P&gt;Please let me know when you have more information.&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jul 2023 07:46:48 GMT</pubDate>
    <dc:creator>stefano-quantic</dc:creator>
    <dc:date>2023-07-14T07:46:48Z</dc:date>
    <item>
      <title>ADC scaling</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1687242#M209208</link>
      <description>&lt;P&gt;In iMXRT1176, when setting the ADCxCMDLy[CSCALE] bit in order to scale the analog signal by 30/64 before converting it, how is the ADC input resistance affected? Does it create a voltage divider on the input signal, so that I would need a voltage buffer on the pin, to avoid distorting the signal?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jul 2023 07:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1687242#M209208</guid>
      <dc:creator>stefano-quantic</dc:creator>
      <dc:date>2023-07-13T07:23:23Z</dc:date>
    </item>
    <item>
      <title>Re: ADC scaling</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688145#M209279</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219981"&gt;@stefano-quantic&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;About the ADC input resistor which is influenced by the&amp;nbsp;&lt;SPAN&gt;CSCALE, we still don't have the data, you can still use the normal input resistor, when select the CSCALE, the internal circuit will&amp;nbsp;reduces the selected ADC analog channel input voltage level by a factor.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;You also need to consider the VREFH situation.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For example: if 3.3V input voltage required then scale factor must be enabled ADC reference must be set to 1.54V (only supported on VREFH).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 06:33:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688145#M209279</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-07-14T06:33:39Z</dc:date>
    </item>
    <item>
      <title>Re: ADC scaling</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688222#M209293</link>
      <description>&lt;P&gt;I have 1V8 on VREFH and I can't change it.&lt;BR /&gt;The ADC would hypothetically read up to 3.84V, but losing the [3.3, 3.84]V range (thus losing some resolution) will not be a problem.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What I'm worried about is whether this scaling factor introduces a voltage divider, forcing me to use a voltage buffer not to distort the signal.&lt;/P&gt;&lt;P&gt;Please let me know when you have more information.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 07:46:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688222#M209293</guid>
      <dc:creator>stefano-quantic</dc:creator>
      <dc:date>2023-07-14T07:46:48Z</dc:date>
    </item>
    <item>
      <title>Re: ADC scaling</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688288#M209298</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219981"&gt;@stefano-quantic&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; I think you need the &lt;SPAN&gt;voltage buffer or at least the voltage limit, which is not higher than the ADC max input voltage. Otherwise, it may influence the pad.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;BR /&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 08:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-scaling/m-p/1688288#M209298</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-07-14T08:32:41Z</dc:date>
    </item>
  </channel>
</rss>