<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1024 Linux DTS for GPIO interrupt in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1688221#M209292</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;- Thanks. No worries. We will check on it.&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jul 2023 07:46:26 GMT</pubDate>
    <dc:creator>sbabu</dc:creator>
    <dc:date>2023-07-14T07:46:26Z</dc:date>
    <item>
      <title>MIMXRT1024 Linux DTS for GPIO interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1687404#M209217</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I want to use GPIO_SD_B1_05 to 08 (GPIO port 3 ) as interrupts which will trigger a interrupt on raising edge on MIMXRT1024 running Linux. Can anybody please share any reference DTS file to achieve the same. Do I need to make any other changes in driver etc other than the DTS entry. Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Babu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 06:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1687404#M209217</guid>
      <dc:creator>sbabu</dc:creator>
      <dc:date>2023-07-14T06:02:52Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1024 Linux DTS for GPIO interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1688159#M209282</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214337"&gt;@sbabu&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Or your use the linux gcc to compile the RT1024 code?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Until now, we still don't have the linux DTS for the RT1024.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 06:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1688159#M209282</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-07-14T06:47:12Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1024 Linux DTS for GPIO interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1688221#M209292</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;- Thanks. No worries. We will check on it.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 07:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1024-Linux-DTS-for-GPIO-interrupt/m-p/1688221#M209292</guid>
      <dc:creator>sbabu</dc:creator>
      <dc:date>2023-07-14T07:46:26Z</dc:date>
    </item>
  </channel>
</rss>