<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: HAB problems on the IMX8MP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HAB-problems-on-the-IMX8MP/m-p/1687688#M209244</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I think the pki tree is not well establish, please read the following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-enable-HAB-in-i-MX6x/ta-p/1101657" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-enable-HAB-in-i-MX6x/ta-p/1101657&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jul 2023 16:03:04 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-07-13T16:03:04Z</dc:date>
    <item>
      <title>HAB problems on the IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-problems-on-the-IMX8MP/m-p/1686726#M209151</link>
      <description>&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x40 0x1f 0xdd 0xc0&lt;BR /&gt;0x00 0x00 0x00 0x20&lt;/P&gt;&lt;P&gt;STS = HAB_FAILURE (0x33)&lt;BR /&gt;RSN = HAB_INV_ASSERTION (0x0C)&lt;BR /&gt;CTX = HAB_CTX_ASSERT (0xA0)&lt;BR /&gt;ENG = HAB_ENG_ANY (0x00)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;--------- HAB Event 2 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x40 0x1f 0xcd 0xc0&lt;BR /&gt;0x00 0x00 0x00 0x04&lt;/P&gt;&lt;P&gt;STS = HAB_FAILURE (0x33)&lt;BR /&gt;RSN = HAB_INV_ASSERTION (0x0C)&lt;BR /&gt;CTX = HAB_CTX_ASSERT (0xA0)&lt;BR /&gt;ENG = HAB_ENG_ANY (0x00)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;--------- HAB Event 3 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x34 0x45 0x33 0x18 0xc0 0x00&lt;BR /&gt;0xca 0x00 0x2c 0x00 0x02 0xc5 0x1d 0x00&lt;BR /&gt;0x00 0x00 0x0b 0x50 0x40 0x1f 0xcd 0xc0&lt;BR /&gt;0x00 0x00 0x10 0x20 0x40 0x20 0x00 0x00&lt;BR /&gt;0x00 0x0c 0x3f 0x30 0x40 0x2c 0x3f 0x30&lt;BR /&gt;0x00 0x00 0xbf 0x20 0x00 0x97 0x00 0x00&lt;BR /&gt;0x00 0x00 0xa1 0x50&lt;/P&gt;&lt;P&gt;STS = HAB_FAILURE (0x33)&lt;BR /&gt;RSN = HAB_INV_SIGNATURE (0x18)&lt;BR /&gt;CTX = HAB_CTX_COMMAND (0xC0)&lt;BR /&gt;ENG = HAB_ENG_ANY (0x00)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;--------- HAB Event 4 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x34 0x45 0x33 0x18 0xc0 0x00&lt;BR /&gt;0xca 0x00 0x2c 0x00 0x02 0xc5 0x1d 0x00&lt;BR /&gt;0x00 0x00 0x0b 0x50 0x40 0x1f 0xcd 0xc0&lt;BR /&gt;0x00 0x00 0x10 0x20 0x40 0x20 0x00 0x00&lt;BR /&gt;0x00 0x0c 0x3f 0x30 0x40 0x2c 0x3f 0x30&lt;BR /&gt;0x00 0x00 0xbf 0x20 0x00 0x97 0x00 0x00&lt;BR /&gt;0x00 0x00 0xa1 0x50&lt;/P&gt;&lt;P&gt;STS = HAB_FAILURE (0x33)&lt;BR /&gt;RSN = HAB_INV_SIGNATURE (0x18)&lt;BR /&gt;CTX = HAB_CTX_COMMAND (0xC0)&lt;BR /&gt;ENG = HAB_ENG_ANY (0x00)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;hello all,&lt;/P&gt;&lt;P&gt;I get these HAB events when tying to secure boot the processor.&lt;/P&gt;&lt;P&gt;looks like there is something wrong with my second stage fit image key judging by the address.&lt;/P&gt;&lt;P&gt;here is the cert file for my second stage fit image&lt;/P&gt;&lt;P&gt;[Install CSFK]&lt;BR /&gt;# Key used to authenticate the CSF data&lt;BR /&gt;File = "../../crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem"&lt;/P&gt;&lt;P&gt;[Authenticate CSF]&lt;/P&gt;&lt;P&gt;[Install Key]&lt;BR /&gt;# Key slot index used to authenticate the key to be installed&lt;BR /&gt;Verification index = 0&lt;BR /&gt;# Target key slot in HAB key store where key will be installed&lt;BR /&gt;Target index = 2&lt;BR /&gt;# Key to install&lt;BR /&gt;File = "../../crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem"&lt;/P&gt;&lt;P&gt;[Authenticate Data]&lt;BR /&gt;# Key slot index used to authenticate the image data&lt;BR /&gt;Verification index = 2&lt;BR /&gt;# Authenticate Start Address, Offset, Length and file&lt;BR /&gt;Blocks = 0x401fcdc0 0x60000 0x1020 "imx-boot", \&lt;BR /&gt;0x40200000 0x53000 0xC3F30 "imx-boot", \&lt;BR /&gt;0x402C3F30 0x116F30 0xBF20 "imx-boot", \&lt;BR /&gt;0x970000 0x122E50 0xA150 "imx-boot"&lt;/P&gt;&lt;P&gt;I have not blown any fuses yet, would this make the error go away? as currently you would expect the key to be wrong as it will be comparing against a random set of data in the fuses.&lt;/P&gt;&lt;P&gt;any help would be much appreciated&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 14:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-problems-on-the-IMX8MP/m-p/1686726#M209151</guid>
      <dc:creator>McCann</dc:creator>
      <dc:date>2023-07-12T14:28:02Z</dc:date>
    </item>
    <item>
      <title>Re: HAB problems on the IMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-problems-on-the-IMX8MP/m-p/1687688#M209244</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I think the pki tree is not well establish, please read the following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-enable-HAB-in-i-MX6x/ta-p/1101657" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-enable-HAB-in-i-MX6x/ta-p/1101657&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jul 2023 16:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-problems-on-the-IMX8MP/m-p/1687688#M209244</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-07-13T16:03:04Z</dc:date>
    </item>
  </channel>
</rss>