<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8QM/8QP MIPI-CSI2 max resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1685978#M209080</link>
    <description>&lt;P&gt;I would like to follow up on the iMX8QM CSI2 Bandwidth.&lt;/P&gt;&lt;P&gt;In the TRM I have the following information about the clocks used in CSI-2 module.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;With a single pixel interface, data_out contains a single pixel every clock that dav_out&lt;BR /&gt;(data valid) is asserted. The single pixel interface must run at a frequency that is equal to&lt;BR /&gt;number of MIPI lanes times the byte lane frequency.&lt;/P&gt;&lt;P&gt;clk :&lt;BR /&gt;RX Controller Core Clock input. This clock must be exactly equal to or faster than the receive byteclock, RxByteClkHS_ln0, from the RX DPHY.&lt;/P&gt;&lt;P&gt;clk: SSSLICE2 : LPCG_MIPI_CSI_LPCG_24&lt;/P&gt;&lt;P&gt;clk_ui:&lt;BR /&gt;User interface clock. The frequency of clk_ui must be such that the data received on the data_out output is greater than or equal to the total bandwidth of the physical MIPI interface. Clk_ui has no relationship requirement with regards to ‘clk’ other than the bandwidth requirement mentioned previously.&lt;/P&gt;&lt;P&gt;clk_ui: SSSLICE2: LPCG_MIPI_CSI_LPCG_24&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;From the clock subsystem, CLK and CLK_UI have the same frequency.&lt;/P&gt;&lt;P&gt;Can the CSI-2 block process all the data when all 4 lanes are receiving at 1.5Gbps ?&lt;/P&gt;&lt;P&gt;clk is generated from&amp;nbsp;DIG_PLL0&amp;nbsp;@ 720 MHZ, a divider provides 360MHz. Can clk be provided a higher frequency ?&lt;/P&gt;&lt;P&gt;Based on the TRM : clk &amp;gt;= lanes * mipi_lane_freq*DDR / 8 &amp;gt;= 4*2/8 * mipi_lane_freq.&lt;BR /&gt;Am I correct to add all the lanes byteclock for the overall&amp;nbsp;receive byteclock ?&lt;/P&gt;&lt;P&gt;Is there a bandwidth limitation at the CSI-2 level ?&lt;/P&gt;&lt;P&gt;CSI-2 6Gbps would need 16.666 x 360MHz. I am not sure of the internal bus width that processes the Rx DPHY data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jul 2023 19:40:53 GMT</pubDate>
    <dc:creator>sbertrand</dc:creator>
    <dc:date>2023-07-11T19:40:53Z</dc:date>
    <item>
      <title>IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1561807#M198170</link>
      <description>&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some community thread were talk about iMX8QM ISI errata&lt;/P&gt;&lt;P&gt;ERR050066: ISI: Data overflows occur when input streams exceed AXI transaction frequency&lt;/P&gt;&lt;P&gt;like this.&lt;/P&gt;&lt;P&gt;&lt;A title="8 x 1080p MIPI CSI2 cameras capture in iMX8QM" href="https://community.nxp.com/t5/i-MX-Processors/8-x-1080p-MIPI-CSI2-cameras-capture-in-iMX8QM/td-p/1036711" target="_blank" rel="noopener"&gt;8 x 1080p MIPI CSI2 cameras capture in iMX8QM&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this errata&lt;/P&gt;&lt;P&gt;"However, combinations of sensors which add&lt;/P&gt;&lt;P&gt;up to less than 2Mpixel are supported with current design."&lt;/P&gt;&lt;P&gt;mean that&lt;/P&gt;&lt;P&gt;1) 2Mpixel mean that 1920x1080 = 2,073,600 is correct?&lt;/P&gt;&lt;P&gt;2) How about frame rate.1920x1080&amp;nbsp;@&lt;FONT color="#FF0000"&gt;60&lt;/FONT&gt;&amp;nbsp;or 1920x1080&amp;nbsp;@&lt;FONT color="#FF0000"&gt;30&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does this apply to each channel individually?&lt;/P&gt;&lt;P&gt;Can it capture for 2ch 1920x1080&amp;nbsp;@60 support?&lt;/P&gt;&lt;TABLE border="1" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="50%"&gt;MIPI-CSI2_0&lt;/TD&gt;&lt;TD width="50%"&gt;1920 x 1080&amp;nbsp;@60&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="50%"&gt;MIPI-CSI2_1&lt;/TD&gt;&lt;TD width="50%"&gt;1920 x 1080&amp;nbsp;@60&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The other hand, i.MX8&lt;FONT color="#FF0000"&gt;QXP_C0&lt;/FONT&gt; silicon have no errata "ERR050066: ISI: Data overflows occur when input streams exceed AXI transaction frequency"..&lt;/P&gt;&lt;P&gt;Is it support &lt;A href="mailto:4K@30" target="_blank"&gt;4K@30&lt;/A&gt;&amp;nbsp;video capture?&lt;/P&gt;&lt;TABLE border="1" width="99.72881368413881%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="33.242876526458616%"&gt;device&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;ch&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;resolution&lt;/TD&gt;&lt;TD width="33.242876526458616%"&gt;fps&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="33.242876526458616%"&gt;i.MX8QM&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;2&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;1920x1080&lt;/TD&gt;&lt;TD width="33.242876526458616%"&gt;60&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="33.242876526458616%"&gt;i.MX8QP&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;2&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;1920x1080&lt;/TD&gt;&lt;TD width="33.242876526458616%"&gt;&lt;P&gt;60&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="33.242876526458616%"&gt;i.MX8QXP&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;1&lt;/TD&gt;&lt;TD width="16.689280868385346%"&gt;3840x2160&lt;/TD&gt;&lt;TD width="33.242876526458616%"&gt;30&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Nov 2022 06:46:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1561807#M198170</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-11-30T06:46:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1565097#M198396</link>
      <description>&lt;P&gt;for mipi csi of imx8qxp or imx8qm, which can supports up to 6Gbps, so can support &lt;A href="mailto:4k@30" target="_blank"&gt;4k@30&lt;/A&gt; or 1080p@60&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 09:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1565097#M198396</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-06T09:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1565222#M198404</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In&amp;nbsp;Figure 15-1. Interconnection Diagram of Reference Manual&amp;nbsp;IMX8QMRM Rev. 0,&lt;/P&gt;&lt;P&gt;MIPI-CSI2 connect to ISI.&lt;/P&gt;&lt;P&gt;So, MIPI-CSI2 can supports 6Gbps so it can capture&amp;nbsp;&lt;A href="mailto:4K@30" target="_blank"&gt;4K@30,&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bat ISI have performance limitation 2MPixel.&lt;/P&gt;&lt;P&gt;I think that it is ok to use i.MX8QXP_C0 silicon because it is fixed this limitation.&lt;/P&gt;&lt;P&gt;But i.MX8QM have no C0 revision.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it can really capture &lt;A href="mailto:4K@30?" target="_blank"&gt;4K@30? &lt;/A&gt;to frame memory on DDR?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,.&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 13:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1565222#M198404</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-06T13:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1565821#M198439</link>
      <description>&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My concern is if the errata ERR050066 will affect the capture with MIPI-CSI2.&lt;BR /&gt;If affected, I am concerned that the maximum capture size will be limited.&lt;/P&gt;&lt;P&gt;Please see attached document.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="takayuki_ishii_2-1670406008739.png" style="width: 592px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/203342i74C109AE94328CCE/image-dimensions/592x281?v=v2" width="592" height="281" role="button" title="takayuki_ishii_2-1670406008739.png" alt="takayuki_ishii_2-1670406008739.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 09:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1565821#M198439</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-07T09:41:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1569259#M198715</link>
      <description>&lt;P&gt;Hello community.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don't you have any update?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 00:57:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1569259#M198715</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-14T00:57:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1570110#M198781</link>
      <description>&lt;P&gt;for ERR050066 , this issue is fixed in imx8qxp C0, for imx8qm, can support &lt;A href="mailto:4k@30" target="_blank"&gt;4k@30&lt;/A&gt; on theory, but we don't tested this, only tested &lt;SPAN&gt;4x1280*800@30Hz successfully, so for &lt;A href="mailto:4k@30," target="_blank"&gt;4k@30,&lt;/A&gt; if&amp;nbsp; system loading is heavy, there is something wrong with capture&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 03:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1570110#M198781</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-15T03:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1570356#M198808</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;We will reply to the customer that max capture size of i.MX8QM is &lt;A href="mailto:4K@30" target="_blank"&gt;4K@30 &lt;/A&gt;are the official specifications.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it correct in my understanding that it works at 4k@30 per channel for MIPI-CSI2?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 09:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1570356#M198808</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-15T09:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1570831#M198832</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please teach me a byte/pixel size of capture test for 4x 1280*800@30Hz&lt;/P&gt;&lt;P&gt;If it is 2byte/pixel = YUYV, the data volume for this test is less than 2 Gbps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4x 1280`800 * 30 * &lt;FONT color="#FF0000"&gt;2byte/pixel&lt;/FONT&gt; = &lt;FONT color="#FF0000"&gt;1.966Gbps&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This result does not prove that 4K capture is possible because it falls within the errata constraints.&lt;/P&gt;&lt;P&gt;I would appreciate your immediate attention to this matter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Dec 2022 00:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1570831#M198832</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-16T00:49:00Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1571583#M198917</link>
      <description>&lt;P&gt;yes, each mipi csi port has this performance&lt;/P&gt;</description>
      <pubDate>Mon, 19 Dec 2022 02:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1571583#M198917</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-19T02:16:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1571587#M198918</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How about color format of tested capture&amp;nbsp;&lt;SPAN&gt;4x1280*800@30Hz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is boundary of ISI limitation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4x1280*800@30Hz*3Byte(RGB24bit) &amp;gt; 2Mpixel(ISI limit) &amp;gt; 4x1280*800@30Hz*2Byte(YUYV16bit)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ishii.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Dec 2022 02:28:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1571587#M198918</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-19T02:28:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572273#M198989</link>
      <description>&lt;P&gt;only tested YUYV16bit&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 05:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572273#M198989</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-20T05:59:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572275#M198990</link>
      <description>&lt;P&gt;only tested YUYV16bit&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 06:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572275#M198990</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-20T06:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572277#M198992</link>
      <description>&lt;P&gt;only tested YUYV16bit&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 06:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572277#M198992</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-20T06:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572505#M199019</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;You say that "&lt;SPAN&gt;only tested&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;4x1280*800@30Hz successfully, so for&amp;nbsp;&lt;A href="mailto:4k@30," target="_blank" rel="nofollow noopener noreferrer"&gt;4k@30,&lt;/A&gt;&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I understand that&amp;nbsp;only tested 4x1280*800@30Hz successfully,&lt;/P&gt;&lt;P&gt;throughput of this condition is lager than 2Gbps, so iMX8QM capture can support more than 2Gbps.&lt;/P&gt;&lt;P&gt;That is, the ISI limit is not affected, so the maximum supported size is &lt;A href="mailto:4K@30" target="_blank" rel="noopener"&gt;4K@30&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But if test condition is&amp;nbsp;4x1280*800@30Hz x 16bit/pixel,&lt;/P&gt;&lt;P&gt;This explanation is not valid. Because throughput of test condition is less than 2Gbps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which is correct?&lt;/P&gt;&lt;P&gt;1) Maximum capture size of iMX8QM is unknown.&lt;/P&gt;&lt;P&gt;2) It has no test but it supports 6Gbps, so it will be 4K@30.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry to keep checking back, but we need accurate information on this specification&lt;/P&gt;&lt;P&gt;as it is an important issue that affects product planning.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 11:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1572505#M199019</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2022-12-20T11:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1575755#M199332</link>
      <description>&lt;P&gt;the mipi csi capture max is 6Gbps, so should can support 4k, but we didn't test this, maybe would have issue when capture 4k, only test resolution is &lt;A href="mailto:1280x800@30," target="_blank"&gt;1280x800@30,&lt;/A&gt; we didn't test 6Gbps, I think 6Gbps maybe cause some bandwidth issue, I only can say we tested max thoughout is 4x1280x800@30&lt;/P&gt;</description>
      <pubDate>Fri, 30 Dec 2022 06:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1575755#M199332</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-12-30T06:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1577520#M199532</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I understand that ISI errata050066 does not affect the capture performance of MIPI-CSI2, so MIPI-CSI2 capture max is 6Gbps and it&lt;SPAN&gt;&amp;nbsp;should can support 4k.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ishii.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 00:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1577520#M199532</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2023-01-05T00:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1685978#M209080</link>
      <description>&lt;P&gt;I would like to follow up on the iMX8QM CSI2 Bandwidth.&lt;/P&gt;&lt;P&gt;In the TRM I have the following information about the clocks used in CSI-2 module.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;With a single pixel interface, data_out contains a single pixel every clock that dav_out&lt;BR /&gt;(data valid) is asserted. The single pixel interface must run at a frequency that is equal to&lt;BR /&gt;number of MIPI lanes times the byte lane frequency.&lt;/P&gt;&lt;P&gt;clk :&lt;BR /&gt;RX Controller Core Clock input. This clock must be exactly equal to or faster than the receive byteclock, RxByteClkHS_ln0, from the RX DPHY.&lt;/P&gt;&lt;P&gt;clk: SSSLICE2 : LPCG_MIPI_CSI_LPCG_24&lt;/P&gt;&lt;P&gt;clk_ui:&lt;BR /&gt;User interface clock. The frequency of clk_ui must be such that the data received on the data_out output is greater than or equal to the total bandwidth of the physical MIPI interface. Clk_ui has no relationship requirement with regards to ‘clk’ other than the bandwidth requirement mentioned previously.&lt;/P&gt;&lt;P&gt;clk_ui: SSSLICE2: LPCG_MIPI_CSI_LPCG_24&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;From the clock subsystem, CLK and CLK_UI have the same frequency.&lt;/P&gt;&lt;P&gt;Can the CSI-2 block process all the data when all 4 lanes are receiving at 1.5Gbps ?&lt;/P&gt;&lt;P&gt;clk is generated from&amp;nbsp;DIG_PLL0&amp;nbsp;@ 720 MHZ, a divider provides 360MHz. Can clk be provided a higher frequency ?&lt;/P&gt;&lt;P&gt;Based on the TRM : clk &amp;gt;= lanes * mipi_lane_freq*DDR / 8 &amp;gt;= 4*2/8 * mipi_lane_freq.&lt;BR /&gt;Am I correct to add all the lanes byteclock for the overall&amp;nbsp;receive byteclock ?&lt;/P&gt;&lt;P&gt;Is there a bandwidth limitation at the CSI-2 level ?&lt;/P&gt;&lt;P&gt;CSI-2 6Gbps would need 16.666 x 360MHz. I am not sure of the internal bus width that processes the Rx DPHY data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 19:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1685978#M209080</guid>
      <dc:creator>sbertrand</dc:creator>
      <dc:date>2023-07-11T19:40:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1864988#M223683</link>
      <description>&lt;P&gt;You have tested &lt;A href="mailto:4x1280x800@30" target="_blank"&gt;4x1280x800@30&lt;/A&gt;. Here what is 4? Is it data lanes?&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 06:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1864988#M223683</guid>
      <dc:creator>ShrithiR</dc:creator>
      <dc:date>2024-05-14T06:16:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM/8QP MIPI-CSI2 max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1865054#M223686</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233477"&gt;@ShrithiR&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;Here what is 4? Is it data lanes?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;No, 4 is a&amp;nbsp; camera input count in this formula.&lt;/P&gt;&lt;P&gt;Please see NXP surround view system web.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-surround-view-system:SURROUND-VIEW-APPLICATION" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-surround-view-system:SURROUND-VIEW-APPLICATION&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 07:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-8QP-MIPI-CSI2-max-resolution/m-p/1865054#M223686</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2024-05-14T07:09:31Z</dc:date>
    </item>
  </channel>
</rss>