<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: USB problem using uuu tool to program imx6UL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-problem-using-uuu-tool-to-program-imx6UL/m-p/1684186#M208894</link>
    <description>&lt;P&gt;Fixed!!!&amp;nbsp; I used the zadig utility to change the utp USB driver from "WinUSB (libusb)" to "libusb-win32".&amp;nbsp; The uuu tool runs smoothly now &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 08 Jul 2023 10:07:11 GMT</pubDate>
    <dc:creator>logman</dc:creator>
    <dc:date>2023-07-08T10:07:11Z</dc:date>
    <item>
      <title>USB problem using uuu tool to program imx6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-problem-using-uuu-tool-to-program-imx6UL/m-p/1684181#M208893</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hello,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;I have a problem flashing my imx6UL device using the UUU tool. I'd appreciate some help please.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I am powering-up the chip with the BM1 pin pulled low as required.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The uuu tool shows the following:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;$ ./uuu.exe uuu_smartcom.auto&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;/P&gt;&lt;P&gt;3:1 1/ 0 [Failure open usb device ]&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is an extract from the uuu_smartcom.auto script:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;uuu_version 1.4.193&lt;/P&gt;&lt;P&gt;SDP: boot -f u-boot.imx-nand&lt;BR /&gt;CFG: FB: -vid 0x0525 -pid 0xA4A5&lt;BR /&gt;CFG: FB: -vid 0x0525 -pid 0x4000&lt;BR /&gt;CFG: FB: -vid 0x0525 -pid 0x4025&lt;BR /&gt;CFG: FB: -vid 0x0525 -pid 0x402F&lt;BR /&gt;CFG: FB: -vid 0x0525 -pid 0x4030&lt;BR /&gt;CFG: FB: -vid 0x0525 -pid 0x4031&lt;BR /&gt;FB: ucmd setenv bootargs "console=ttymxc0,115200 clk_ignore_unused rdinit=/linuxrc mtdparts=gpmi-nand:64m(nandboot),16m(nandkernel),16m(nanddtb),16m(nandtee),-(nandrootfs)"&lt;BR /&gt;#FB: ucmd setenv bootargs "console=ttymxc0,115200 rdinit=/linuxrc mtdparts=gpmi-nand:0x4000000(u-boot_primary),0x1000000(u-boot_secondary),0x1000000(u-boot_Env),0x1000000(kernel_primary),0x1000000(initramfs_kernel),0x1000000(kernel_backup),0x400000(dtb_primary),0x400000(dtb_secondary),0x400000(dtb_backup1),0x400000(dtb_backup2),0x1000000(initramfs_rootfs),0x1f400000(persistent_data),-(rootfs_primary)"&lt;BR /&gt;FB: ucmd setenv fastboot_buffer ${loadaddr}&lt;BR /&gt;FB: download -f zImage&lt;BR /&gt;FB: ucmd setenv fastboot_buffer ${fdt_addr}&lt;BR /&gt;FB: download -f imx6ul-14x14-evk.dtb&lt;BR /&gt;FB: ucmd setenv fastboot_buffer ${initrd_addr}&lt;BR /&gt;FB: download -f fsl-image-mfgtool-initramfs-smartcom.cpio.gz.u-boot&lt;BR /&gt;FB: ucmd setenv bootargs ${bootargs} ${mtdparts}&lt;BR /&gt;FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The uuu tool executes all of the above commands OK, then it hangs on the 'FB: acmd' command before it reports 'Failure open usb device'.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;When I run my uuu script, the device shows the sequence copied below (from --- START OF TERMINAL TEXT) on the Putty COM1 linux terminal. &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;The terminal output indicatse that /dev/utp fails to appear in the device.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;My machine is Windows 10, and I have seen the same behaviour when executing on WSL Ubuntu.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;I have updated the utp USB Windows driver to 6.1.7600.16385 from libwdi.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;My colleague has successfully run the same process on his setup, using the same target hardware and the same firmware and uuu setup. &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;I have run this process successfully last month, but it would appear that something is going wrong with the USB access now.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I have looked at various forum posts, including &lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8-board-recognized-as-SE-blank-815/td-p/1174462" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX8-board-recognized-as-SE-blank-815/td-p/1174462&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can anyone suggest what to try please? I'm out of ideas.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Thanks,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Tom.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;--- START OF TERMINAL TEXT&lt;/P&gt;&lt;P&gt;U-Boot 2021.04-lf_v2021.04+g8b8a0e5567 (Sep 27 2022 - 02:05:23 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX6UL rev1.2 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 39C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;NAND: 2048 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from NAND... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Net: eth0: ethernet@2188000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Getting device i2c bus&lt;BR /&gt;Getting device by address from i2c bus&lt;BR /&gt;Reading from Eeprom device&lt;BR /&gt;Checking Bootflag...!!!&lt;BR /&gt;Boot from NAND primary-Texeconnect (normal boot)&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 86800000 ...&lt;BR /&gt;Unknown image format!&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;Starting download of 7286584 bytes&lt;BR /&gt;.......................................................&lt;BR /&gt;downloading of 7286584 bytes finished&lt;BR /&gt;Starting download of 32572 bytes&lt;/P&gt;&lt;P&gt;downloading of 32572 bytes finished&lt;BR /&gt;Starting download of 12695772 bytes&lt;BR /&gt;..........................................................................&lt;BR /&gt;......................&lt;BR /&gt;downloading of 12695772 bytes finished&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x6f2f38 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 86800000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-smar&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 12695708 Bytes = 12.1 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 83000000, end 8300af3b&lt;BR /&gt;Modify /soc/bus@2000000/tsc@2040000 disabled&lt;BR /&gt;Modify /soc/bus@2100000/lcdif@21c8000 disabled&lt;BR /&gt;Modify /soc/bus@2100000/csi@21c4000 disabled&lt;BR /&gt;Modify /soc/bus@2000000/ethernet@20b4000 disabled&lt;BR /&gt;gpio@209c000: set_value: error: gpio GPIO1_8 not reserved&lt;BR /&gt;gpio@20ac000: set_value: error: gpio GPIO5_9 not reserved&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0&lt;BR /&gt;[ 0.000000] Linux version 5.10.72-lts-5.10.y+g764677fd5b68 (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.36.1.20210209) #1 SMP PREEMPT Tue Oct 25 12:05:04 UTC 2022&lt;BR /&gt;[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d&lt;BR /&gt;[ 0.000000] CPU: div instructions available: patching division code&lt;BR /&gt;[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;[ 0.000000] OF: fdt: Machine model: Texecom: VICTOR-A5150 HUB Board &amp;lt;-&amp;gt; Yocto-HARDKNOTT&lt;BR /&gt;[ 0.000000] Memory policy: Data cache writealloc&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x96000000, size 160 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;/P&gt;&lt;P&gt;etc...&lt;/P&gt;&lt;P&gt;[ 4.359277] mmc1: queuing unknown CIS tuple 0x80 (2 bytes)&lt;BR /&gt;[ 4.366674] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)&lt;BR /&gt;[ 4.377080] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)&lt;BR /&gt;[ 4.383409] Registering SWP/SWPB emulation handler&lt;BR /&gt;[ 4.389217] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 4.396987] mmc1: queuing unknown CIS tuple 0x80 (7 bytes)&lt;BR /&gt;[ 4.415773] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)&lt;BR /&gt;[ 4.436718] mmc1: queuing unknown CIS tuple 0x80 (6 bytes)&lt;BR /&gt;[ 4.456100] imx_usb 2184000.usb: No over current polarity defined&lt;BR /&gt;[ 4.574592] mmc1: new high speed SDIO card at address 0001&lt;BR /&gt;[ 4.744993] ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;[ 4.750063] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;[ 4.784180] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;[ 4.790703] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10&lt;BR /&gt;[ 4.799164] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1&lt;BR /&gt;[ 4.806545] usb usb1: Product: EHCI Host Controller&lt;BR /&gt;[ 4.811480] usb usb1: Manufacturer: Linux 5.10.72-lts-5.10.y+g764677fd5b68 ehci_hcd&lt;BR /&gt;[ 4.819270] usb usb1: SerialNumber: ci_hdrc.1&lt;BR /&gt;[ 4.826551] hub 1-0:1.0: USB hub found&lt;BR /&gt;[ 4.830573] hub 1-0:1.0: 1 port detected&lt;BR /&gt;[ 4.840940] imx_thermal 20c8000.anatop:tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C&lt;BR /&gt;[ 4.853870] clk: Not disabling unused clocks&lt;BR /&gt;[ 4.861396] Freeing unused kernel memory: 1024K&lt;BR /&gt;[ 4.867142] Run /linuxrc as init process&lt;BR /&gt;Found New UDC: ci_hdrc.0&lt;BR /&gt;ci_hdrc.0 0&lt;BR /&gt;ffs.utp0&lt;BR /&gt;[ 5.040530] file system registered&lt;BR /&gt;[ 5.093415] Mass Storage Function, version: 2009/09/11&lt;BR /&gt;[ 5.099028] LUN: removable file: (no medium)&lt;BR /&gt;run utp at /dev/usb-utp0/ep0&lt;BR /&gt;.&lt;BR /&gt;uuu fastboot client 1.0.0 [built [ 5.131365] read descriptors&lt;BR /&gt;Nov 7 2019 19:25:07]&lt;BR /&gt;Start init[ 5.137450] read strings&lt;BR /&gt;usb&lt;BR /&gt;write string&lt;BR /&gt;Start handle command&lt;BR /&gt;uuc /dev/utp&lt;BR /&gt;uuc 0.6 [built Nov 7 2019 19:25:07]&lt;BR /&gt;UTP: Waiting for /dev/utp to appear&lt;/P&gt;&lt;P&gt;--- END OF TERMINAL TEXT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 08 Jul 2023 09:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-problem-using-uuu-tool-to-program-imx6UL/m-p/1684181#M208893</guid>
      <dc:creator>logman</dc:creator>
      <dc:date>2023-07-08T09:13:57Z</dc:date>
    </item>
    <item>
      <title>Re: USB problem using uuu tool to program imx6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-problem-using-uuu-tool-to-program-imx6UL/m-p/1684186#M208894</link>
      <description>&lt;P&gt;Fixed!!!&amp;nbsp; I used the zadig utility to change the utp USB driver from "WinUSB (libusb)" to "libusb-win32".&amp;nbsp; The uuu tool runs smoothly now &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 08 Jul 2023 10:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-problem-using-uuu-tool-to-program-imx6UL/m-p/1684186#M208894</guid>
      <dc:creator>logman</dc:creator>
      <dc:date>2023-07-08T10:07:11Z</dc:date>
    </item>
  </channel>
</rss>