<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMXRT1170 LPI2C FIFO Error Flag (FEF)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/1682950#M208782</link>
    <description>&lt;P&gt;Can someone please explain what is the application of the FIFO error Flag (FEF) in the LPI2C Master Status Register (MSR)? If the start condition is always sent before a write/read request in the driver, do we still need its interrupt?&lt;/P&gt;&lt;P&gt;I am asking because I do not use this status flag right now and when I try to clear it by writing 1 it does not clear. Other status flags are clear by writing 1.&lt;/P&gt;&lt;P&gt;Note: I am also NOT using the auto-stop&amp;nbsp;feature i.e.,&amp;nbsp;MCFGR1[AUTOSTOP] = 0&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jul 2023 08:22:12 GMT</pubDate>
    <dc:creator>ZohaibAli</dc:creator>
    <dc:date>2023-07-06T08:22:12Z</dc:date>
    <item>
      <title>IMXRT1170 LPI2C FIFO Error Flag (FEF)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/1682950#M208782</link>
      <description>&lt;P&gt;Can someone please explain what is the application of the FIFO error Flag (FEF) in the LPI2C Master Status Register (MSR)? If the start condition is always sent before a write/read request in the driver, do we still need its interrupt?&lt;/P&gt;&lt;P&gt;I am asking because I do not use this status flag right now and when I try to clear it by writing 1 it does not clear. Other status flags are clear by writing 1.&lt;/P&gt;&lt;P&gt;Note: I am also NOT using the auto-stop&amp;nbsp;feature i.e.,&amp;nbsp;MCFGR1[AUTOSTOP] = 0&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 08:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/1682950#M208782</guid>
      <dc:creator>ZohaibAli</dc:creator>
      <dc:date>2023-07-06T08:22:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1170 LPI2C FIFO Error Flag (FEF)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/1686829#M209159</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188801"&gt;@ZohaibAli&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This flag is triggered when master starts recieving or sending data without a start condition.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can read this thread for another reason the flag cold be triggered.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE1xF-I2C-FIFO-Error-Flag/m-p/909919" target="_self"&gt;MKE1xF I2C FIFO Error Flag&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The manual does not specify that this flag is needed for the module to work.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 18:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/1686829#M209159</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-07-12T18:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1170 LPI2C FIFO Error Flag (FEF)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/2026980#M232944</link>
      <description>&lt;P&gt;You have to reset the FIFO (via the LPI2C::MCR register) before you can clear the FEF flag&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 19:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1170-LPI2C-FIFO-Error-Flag-FEF/m-p/2026980#M232944</guid>
      <dc:creator>carmeng</dc:creator>
      <dc:date>2025-01-13T19:16:41Z</dc:date>
    </item>
  </channel>
</rss>