<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX53 DDR test - ack failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244036#M20871</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running DDR test application from Windows using the following command on a i.MX53 QSB development board:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;EM&gt;C:\DDR&amp;gt;&lt;/EM&gt; DDR_Stress_Tester.exe -t mx53 -df MX53_TO2_DDR3_LCB_SMD_ARDb.inc -com 1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works fine. Whereas, when I run the same for the customer board the command fails with the following errors:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;C:\DDR&amp;gt; DDR_Stress_Tester.exe -t mx53 -df MX53_TO2_DDR3_LCB_SMD_ARDb.inc -com 1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;rom_check_hab: reading ERROR ack failed 0x00000000&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;rom_check_hab() failed&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this because I am using the wrong initialization file (inc) or it this a hardware issue? How can I debug this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ruchi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Aug 2013 12:28:45 GMT</pubDate>
    <dc:creator>ruchisirauthiya</dc:creator>
    <dc:date>2013-08-07T12:28:45Z</dc:date>
    <item>
      <title>i.MX53 DDR test - ack failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244036#M20871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running DDR test application from Windows using the following command on a i.MX53 QSB development board:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;EM&gt;C:\DDR&amp;gt;&lt;/EM&gt; DDR_Stress_Tester.exe -t mx53 -df MX53_TO2_DDR3_LCB_SMD_ARDb.inc -com 1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works fine. Whereas, when I run the same for the customer board the command fails with the following errors:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;C:\DDR&amp;gt; DDR_Stress_Tester.exe -t mx53 -df MX53_TO2_DDR3_LCB_SMD_ARDb.inc -com 1&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;rom_check_hab: reading ERROR ack failed 0x00000000&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;rom_check_hab() failed&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this because I am using the wrong initialization file (inc) or it this a hardware issue? How can I debug this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ruchi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 12:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244036#M20871</guid>
      <dc:creator>ruchisirauthiya</dc:creator>
      <dc:date>2013-08-07T12:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 DDR test - ack failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244037#M20872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The mentioned "rom_check_hab" messages relate to interface between internal iROM &lt;/P&gt;&lt;P&gt;bootloader of i.MX53 and an application, that tries to load and run (memory) &lt;/P&gt;&lt;P&gt;tests&amp;nbsp; via i.MX53 UART / USB serial boot mode. There are two possible causes of &lt;/P&gt;&lt;P&gt;the issue. &lt;/P&gt;&lt;P&gt;1. The board does not start in the bootstrap (serial download) mode. &lt;/P&gt;&lt;P&gt;2. There is no serial connection between a PC and the i.MX53 board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 03:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244037#M20872</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-08-08T03:11:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 DDR test - ack failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244038#M20873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply. I verified the custom board setup:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- It is not a Serial to Serial cable issue, I have verified the cable with another setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The board is in serial download mode. I tried the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp; a. Used the on-board button to enter serial download mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp; b. To double check I also did a NAND erase so that by default the board will enter serial download mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even after (b) I was not able to get the DDR test tool to work. I am getting the same error on the custom board I used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any other checks to debug this issue? Is there a log at DDR tool side (Windows) or on the board which I can enable to see what is happening?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ruchi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 07:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-DDR-test-ack-failed/m-p/244038#M20873</guid>
      <dc:creator>ruchisirauthiya</dc:creator>
      <dc:date>2013-08-08T07:00:09Z</dc:date>
    </item>
  </channel>
</rss>