<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: memtool support for i.MX8MM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1681842#M208678</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;thanks for your response, it is very useful.&lt;/P&gt;&lt;P&gt;However, I am still wondering if the "macros" (register info mappings) will be implemented any time in the future for the other i.MX8M families in addition to the "Quad". I understand it is not an essential feature but still extremely useful during&amp;nbsp;prototyping and debugging.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matteo&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jul 2023 08:40:50 GMT</pubDate>
    <dc:creator>mattmart</dc:creator>
    <dc:date>2023-07-05T08:40:50Z</dc:date>
    <item>
      <title>memtool support for i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1677999#M208296</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It looks like that memtool, among all the i.MX8M family processors, only supports the i.MX8MQ one &lt;A href="https://github.com/nxp-imx/imx-test/blob/59f8017a582ae166cd2c098e97535c41b81f22ec/test/memtool/memtool.c#L55" target="_blank" rel="noopener"&gt;[ref]&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Are there any plans to extend memtool support to the other i.MX8M processors such as i.MX8MM?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Matteo&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 16:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1677999#M208296</guid>
      <dc:creator>mattmart</dc:creator>
      <dc:date>2023-06-28T16:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: memtool support for i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1678740#M208354</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219587"&gt;@mattmart&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;The memtool is supported for iMX8M.&lt;/P&gt;
&lt;P&gt;The tools are integrated directly into our bsp.&lt;/P&gt;
&lt;P&gt;You can check in the folder /unit_test of our bsp.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chavira_0-1688043849009.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230077iFD72A89B2FE95A06/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chavira_0-1688043849009.png" alt="Chavira_0-1688043849009.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 13:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1678740#M208354</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-06-29T13:04:20Z</dc:date>
    </item>
    <item>
      <title>Re: memtool support for i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1679450#M208417</link>
      <description>&lt;P&gt;It looks like it is not supported on i.MX8MM (Mini):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE&gt;root@imx8mm-icore:/unit_tests# ./memtool IOMUXC.SW_MUX_CTL_PAD_GPIO1_IO03.MUX_MODE
SOC: i.MX8MM
Unknown SOC&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Running on BSP built on&amp;nbsp;imx-5.15.71-2.2.0.xml manifest, kirkstone yocto version.&lt;/P&gt;&lt;P&gt;Also, from the&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-test/blob/59f8017a582ae166cd2c098e97535c41b81f22ec/test/memtool/memtool.c#L344" target="_blank" rel="noopener"&gt;memtool source code&lt;/A&gt;&amp;nbsp;it looks that only the i.MX8MQ (Quad) is supported.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Matteo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 08:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1679450#M208417</guid>
      <dc:creator>mattmart</dc:creator>
      <dc:date>2023-06-30T08:50:50Z</dc:date>
    </item>
    <item>
      <title>Re: memtool support for i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1681413#M208636</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219587"&gt;@mattmart&lt;/a&gt; !&lt;/P&gt;
&lt;P&gt;Sorry for the late response!&lt;/P&gt;
&lt;P&gt;You can use the memtool but for iMX8M is not defined the macros.&lt;/P&gt;
&lt;P&gt;To use the memtool you have to put the direction that you can read/ write instead of the name of the register.&lt;/P&gt;
&lt;P&gt;for the register "IOMUXC_SW_MUX_CTL_PAD_GPIO1_IO03" you can do the next:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chavira_1-1688493725516.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230747i03DA2DDC5F17C5B5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chavira_1-1688493725516.png" alt="Chavira_1-1688493725516.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chavira_0-1688493683827.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230746iAC041B7A756AD728/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chavira_0-1688493683827.png" alt="Chavira_0-1688493683827.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jul 2023 18:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1681413#M208636</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-07-04T18:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: memtool support for i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1681842#M208678</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;thanks for your response, it is very useful.&lt;/P&gt;&lt;P&gt;However, I am still wondering if the "macros" (register info mappings) will be implemented any time in the future for the other i.MX8M families in addition to the "Quad". I understand it is not an essential feature but still extremely useful during&amp;nbsp;prototyping and debugging.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matteo&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 08:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/memtool-support-for-i-MX8MM/m-p/1681842#M208678</guid>
      <dc:creator>mattmart</dc:creator>
      <dc:date>2023-07-05T08:40:50Z</dc:date>
    </item>
  </channel>
</rss>