<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX8MM eMMC Alternate boot.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1681147#M208613</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;Can you please let us know the following:&lt;/P&gt;&lt;P&gt;1) how to use mmc_boot register?&lt;/P&gt;&lt;P&gt;2) and how host handles boot ack and data?&lt;/P&gt;&lt;P&gt;3) Are there any interrupts generated for boot events?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 04 Jul 2023 09:33:23 GMT</pubDate>
    <dc:creator>vignesh-baskaran</dc:creator>
    <dc:date>2023-07-04T09:33:23Z</dc:date>
    <item>
      <title>I.MX8MM eMMC Alternate boot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1680338#M208526</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We trying to boot eMMC in userspace.&lt;/P&gt;&lt;P&gt;First we boot from other interface upto userspace. Now we trying to evaluate the boot operation of eMMC.&lt;/P&gt;&lt;P&gt;is it possible test boot modes in Linux mmc device driver ? and any version of bsp enabled it in Linux kernel?&lt;/P&gt;&lt;P&gt;When we send cmd0 with arg 0xffffffa at 400KHz. We see card responding with boot ack and boot data on oscilloscope. But we are not sure how to handle it mmc host driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 08:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1680338#M208526</guid>
      <dc:creator>vignesh-baskaran</dc:creator>
      <dc:date>2023-07-03T08:56:08Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MM eMMC Alternate boot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1681133#M208612</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209908"&gt;@vignesh-baskaran&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;Yes, one can add a print statement in the particular section of the emmc one wants to debug.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;"Switch to partitions #0, OK" From here one can debug the emmc boot towards the userspace.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;One can make changes to the driver in any Linux bsp one wants.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;After making certain changes please rebuilt the image and one can have the traces of the booting from emmc towards userspace.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Dhruvit Vasavada&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jul 2023 09:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1681133#M208612</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-07-04T09:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MM eMMC Alternate boot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1681147#M208613</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;Can you please let us know the following:&lt;/P&gt;&lt;P&gt;1) how to use mmc_boot register?&lt;/P&gt;&lt;P&gt;2) and how host handles boot ack and data?&lt;/P&gt;&lt;P&gt;3) Are there any interrupts generated for boot events?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jul 2023 09:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1681147#M208613</guid>
      <dc:creator>vignesh-baskaran</dc:creator>
      <dc:date>2023-07-04T09:33:23Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MM eMMC Alternate boot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1682038#M208710</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209908"&gt;@vignesh-baskaran&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="im"&gt;I hope you are doing well.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;mmc_boot -&amp;gt; This register contains the MMC Fast Boot control register.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4th bit = BOOT_ACK -&amp;gt; Boot ACK mode select&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 0b - No ack&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 1b - Ack&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please refer to Section 10.3.7.1.30MMC Boot (MMC_BOOT) from RM for more details.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMRM" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://www.nxp.com/webapp/Download?colCode%3DIMX8MMRM&amp;amp;source=gmail&amp;amp;ust=1688644095937000&amp;amp;usg=AOvVaw0FI6dtD4guUpIjzBfpnRMD"&gt;https://www.nxp.com/webapp/&lt;WBR /&gt;Download?colCode=IMX8MMRM&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There are no interrupts generated for boot events. there is no mention of such in the register field.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 13:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1682038#M208710</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-07-05T13:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MM eMMC Alternate boot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1685267#M208996</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for letting me know.&lt;/P&gt;&lt;P&gt;We were following the same flow.&lt;/P&gt;&lt;P&gt;We were trying to set&amp;nbsp; MSBSEL, DTDSEL and DPSEL in host controller. But&amp;nbsp; we were not able to set it as '1', sometimes we getting core dump error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Why we unable to set these bits?&lt;BR /&gt;2) And how to handle this data transfers?&lt;/P&gt;&lt;P&gt;3) Like what response host expects during booting methods?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if possible can point us any sample source code we could use as reference for eMMC booting as mentioned in the reference manual?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;Vignesh.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 02:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MM-eMMC-Alternate-boot/m-p/1685267#M208996</guid>
      <dc:creator>vignesh-baskaran</dc:creator>
      <dc:date>2023-07-11T02:09:28Z</dc:date>
    </item>
  </channel>
</rss>