<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Could I initialize two SDRAMs by dcd.c? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1680235#M208517</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217913"&gt;@MCW&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Yes, you can enable two SDRAM in dcd. The RT1170 EVK has two SDRAM too, and they are initialized in DCD. It is needn't to write many SEMC register twice in DCD. You can refer to the dcd file in RT1170 SDK examples.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jul 2023 07:05:39 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2023-07-03T07:05:39Z</dc:date>
    <item>
      <title>Could I initialize two SDRAMs by dcd.c?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1678702#M208353</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have two SDRAMs on my customize board. The CS pins are&amp;nbsp;&lt;SPAN&gt;IOMUXC_GPIO_EMC_29_SEMC_CS0 and&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;IOMUXC_GPIO_B0_02_SEMC_CSX03, and the start address are 0x80000000 and 0x8C0000000, respectively.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I used semc_sdram example code to set both of them. And the SDRAMs can be read and written correctly.&lt;/P&gt;&lt;P&gt;Next step, the semc related registers were read out and recorded. So I filled out these values to dcd.c and comment out BOARD_InitSEMC(). However, the values read from the second SDRAM were wrong (the first SDRAM is okay).&amp;nbsp; And I have localized the problem which comes from &lt;STRONG&gt;Mode setting&lt;/STRONG&gt; in dcd.c. But the&amp;nbsp; IPTXDAT of the second one is the same as the first one, so I cannot ffigure out the reason.&lt;/P&gt;&lt;P&gt;There is a question I need to make sure. Could I initialize two SDRAMs&amp;nbsp;by dcd.c, or just one?&lt;/P&gt;&lt;P&gt;my dcd.c:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/*
 * Copyright 2020 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

/***********************************************************************************************************************
 * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file
 * will be overwritten if the respective MCUXpresso Config Tools is used to update this file.
 **********************************************************************************************************************/

#include "dcd.h"

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.xip_board"
#endif

#if defined(XIP_BOOT_HEADER_ENABLE) &amp;amp;&amp;amp; (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(XIP_BOOT_HEADER_DCD_ENABLE) &amp;amp;&amp;amp; (XIP_BOOT_HEADER_DCD_ENABLE == 1)
#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".boot_hdr.dcd_data")))
#elif defined(__ICCARM__)
#pragma location = ".boot_hdr.dcd_data"
#endif

/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: DCDx V2.0
processor: MIMXRT1062xxxxA
package_id: MIMXRT1062DVL6A
mcu_data: ksdk2_0
processor_version: 0.0.0
board: MIMXRT1060-EVK
output_format: c_array
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */
const uint8_t dcd_data[] = {
	/* HEADER */
	/* Tag */
	0xD2,
	/* Image Length limit 1768bytes*/ 
	//0x04, 0x10,
	0x05, 0x4C,
	/* Version */
	0x41,

	/* COMMANDS */
	//set first sdram
	/* group: 'Imported Commands' */
	/* #1.1-113, command header bytes for merged 'Write - value' command */
	0xCC, 0x03, 0x8C, 0x04, //904=113*8+4
	/* #1.1, command: write_value, address: CCM_CCGR0, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x68, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.2, command: write_value, address: CCM_CCGR1, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x6C, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.3, command: write_value, address: CCM_CCGR2, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x70, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.4, command: write_value, address: CCM_CCGR3, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x74, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.5, command: write_value, address: CCM_CCGR4, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x78, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.6, command: write_value, address: CCM_CCGR5, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x7C, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.7, command: write_value, address: CCM_CCGR6, value: 0xFFFFFFFF, size: 4 */
	0x40, 0x0F, 0xC0, 0x80, 0xFF, 0xFF, 0xFF, 0xFF,
	/* #1.8, command: write_value, address: CCM_ANALOG_PLL_SYS, value: 0x2001, size: 4 */
	0x40, 0x0D, 0x80, 0x30, 0x00, 0x00, 0x20, 0x01,
	/* #1.9, command: write_value, address: CCM_ANALOG_PFD_528, value: 0x1D0000, size: 4 */
	0x40, 0x0D, 0x81, 0x00, 0x00, 0x1D, 0x00, 0x00,
	/* #1.10, command: write_value, address: CCM_CBCDR, value: 0x10D40, size: 4 */
	0x40, 0x0F, 0xC0, 0x14, 0x00, 0x01, 0x0D, 0x40,
	/* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_00, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00,
	/* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_01, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00,
	/* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_02, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00,
	/* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_03, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00,
	/* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_04, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00,
	/* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_05, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00,
	/* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_06, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00,
	/* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_07, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00,
	/* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_08, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00,
	/* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_09, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00,
	/* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_10, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00,
	/* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_11, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00,
	/* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_12, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00,
	/* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_13, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00,
	/* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_14, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00,
	/* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_15, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00,
	/* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_16, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00,
	/* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_17, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00,
	/* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_18, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00,
	/* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_19, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00,
	/* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_20, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00,
	/* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_21, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00,
	/* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_22, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00,
	/* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_23, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00,
	/* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_24, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00,
	/* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_25, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00,
	/* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_26, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00,
	/* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_27, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,
	/* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_28, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00,
	/* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_29, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00,
	/* #1.41, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_30, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00,
	/* #1.42, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_31, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00,
	/* #1.43, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_32, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00,
	/* #1.44, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_33, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.45, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_34, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00,
	/* #1.46, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_35, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00,
	/* #1.47, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_36, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00,
	/* #1.48, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_37, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00,
	/* #1.49, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_38, value: 0x00, size: 4 */
	0x40, 0x1F, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x00,
	/* #1.50, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_39, value: 0x10, size: 4 */
	0x40, 0x1F, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x10,
	/* #1.51, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_00, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x04, 0x00, 0x01, 0x10, 0xF9,
	/* #1.52, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_01, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x08, 0x00, 0x01, 0x10, 0xF9,
	/* #1.53, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_02, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x0C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.54, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_03, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x10, 0x00, 0x01, 0x10, 0xF9,
	/* #1.55, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_04, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x14, 0x00, 0x01, 0x10, 0xF9,
	/* #1.56, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_05, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x18, 0x00, 0x01, 0x10, 0xF9,
	/* #1.57, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_06, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x1C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.58, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_07, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x20, 0x00, 0x01, 0x10, 0xF9,
	/* #1.59, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_08, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x24, 0x00, 0x01, 0x10, 0xF9,
	/* #1.60, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_09, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x28, 0x00, 0x01, 0x10, 0xF9,
	/* #1.61, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_10, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x2C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.62, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_11, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x30, 0x00, 0x01, 0x10, 0xF9,
	/* #1.63, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_12, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x34, 0x00, 0x01, 0x10, 0xF9,
	/* #1.64, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_13, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x38, 0x00, 0x01, 0x10, 0xF9,
	/* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_14, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x3C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_15, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x40, 0x00, 0x01, 0x10, 0xF9,
	/* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_16, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x44, 0x00, 0x01, 0x10, 0xF9,
	/* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_17, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x48, 0x00, 0x01, 0x10, 0xF9,
	/* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_18, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x4C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_19, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x50, 0x00, 0x01, 0x10, 0xF9,
	/* #1.71, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_20, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x54, 0x00, 0x01, 0x10, 0xF9,
	/* #1.72, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_21, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x58, 0x00, 0x01, 0x10, 0xF9,
	/* #1.73, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_22, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x5C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.74, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_23, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x60, 0x00, 0x01, 0x10, 0xF9,
	/* #1.75, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_24, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x64, 0x00, 0x01, 0x10, 0xF9,
	/* #1.76, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_25, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x68, 0x00, 0x01, 0x10, 0xF9,
	/* #1.77, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_26, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x6C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.78, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_27, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x70, 0x00, 0x01, 0x10, 0xF9,
	/* #1.79, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_28, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x74, 0x00, 0x01, 0x10, 0xF9,
	/* #1.80, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_29, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x78, 0x00, 0x01, 0x10, 0xF9,
	/* #1.81, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_30, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x7C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.82, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_31, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x80, 0x00, 0x01, 0x10, 0xF9,
	/* #1.83, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_32, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x84, 0x00, 0x01, 0x10, 0xF9,
	/* #1.84, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_33, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x88, 0x00, 0x01, 0x10, 0xF9,
	/* #1.85, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_34, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x8C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.86, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_35, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x90, 0x00, 0x01, 0x10, 0xF9,
	/* #1.87, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_36, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x94, 0x00, 0x01, 0x10, 0xF9,
	/* #1.88, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_37, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x98, 0x00, 0x01, 0x10, 0xF9,
	/* #1.89, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_38, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0x9C, 0x00, 0x01, 0x10, 0xF9,
	/* #1.90, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_39, value: 0x110F9, size: 4 */
	0x40, 0x1F, 0x82, 0xA0, 0x00, 0x01, 0x10, 0xF9,
	/* #1.91, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
	0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04,
	/* #1.92, command: write_value, address: SEMC_BMCR0, value: 0x30524, size: 4 */
	0x40, 0x2F, 0x00, 0x08, 0x00, 0x03, 0x05, 0x24,
	/* #1.93, command: write_value, address: SEMC_BMCR1, value: 0x6030524, size: 4 */
	0x40, 0x2F, 0x00, 0x0C, 0x06, 0x03, 0x05, 0x24,
	/* #1.94, command: write_value, address: SEMC_BR0, value: 0x8000001B, size: 4 */
	0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x1B,
	/* #1.95, command: write_value, address: SEMC_BR1, value: 0x8200001B, size: 4 */
	0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1B,
	/* #1.96, command: write_value, address: SEMC_BR2, value: 0x8400001B, size: 4 */
	0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1B,
	/* #1.97, command: write_value, address: SEMC_BR3, value: 0x8600001B, size: 4 */
	0x40, 0x2F, 0x00, 0x1C, 0x8C, 0x00, 0x00, 0x1B,
	/* #1.98, command: write_value, address: SEMC_BR4, value: 0x90000021, size: 4 */
	0x40, 0x2F, 0x00, 0x20, 0x90, 0x00, 0x00, 0x21,
	/* #1.99, command: write_value, address: SEMC_BR5, value: 0xA0000019, size: 4 */
	0x40, 0x2F, 0x00, 0x24, 0xA0, 0x00, 0x00, 0x19,
	/* #1.100, command: write_value, address: SEMC_BR6, value: 0xA8000017, size: 4 */
	0x40, 0x2F, 0x00, 0x28, 0xA8, 0x00, 0x00, 0x17,
	/* #1.101, command: write_value, address: SEMC_BR7, value: 0xA900001B, size: 4 */
	0x40, 0x2F, 0x00, 0x2C, 0xA9, 0x00, 0x00, 0x1B,
	/* #1.102, command: write_value, address: SEMC_BR8, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x30, 0x00, 0x00, 0x00, 0x21,
	/* #1.103, command: write_value, address: SEMC_IOCR, value: 0x79A8, size: 4 */
	0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x30, 0x00,
	/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF31, size: 4 */
	0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x31,
	/* #1.105, command: write_value, address: SEMC_SDRAMCR1, value: 0x652922, size: 4 */
	0x40, 0x2F, 0x00, 0x44, 0x00, 0x66, 0x4B, 0x22,
	/* #1.106, command: write_value, address: SEMC_SDRAMCR2, value: 0x10920, size: 4 */
	0x40, 0x2F, 0x00, 0x48, 0x00, 0x09, 0x09, 0x0B,
	/* #1.107, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A08, size: 4 */
	0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x00,
	/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21,
	/* #1.109, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */
	0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88,
	/* #1.110, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
	0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02,
	/* #1.111, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
	0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.112, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #1.113, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
	/* #2, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #3.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #3.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
	/* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #5.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
	/* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #7.1-3, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x1C, 0x04,
	/* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
	0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x33,
	/* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
	/* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
	0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
	/* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A09, size: 4 */
	0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x01,
	//1040bytes

	//set second sdram
	0xCC, 0x00, 0xBC, 0x04, //188=23*8+4
	/* #1.91, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
	0x40, 0x2F, 0x00, 0x00, 0x10, 0x00, 0x00, 0x04,
	/* #1.92, command: write_value, address: SEMC_BMCR0, value: 0x30524, size: 4 */
	0x40, 0x2F, 0x00, 0x08, 0x00, 0x03, 0x05, 0x24,
	/* #1.93, command: write_value, address: SEMC_BMCR1, value: 0x6030524, size: 4 */
	0x40, 0x2F, 0x00, 0x0C, 0x06, 0x03, 0x05, 0x24,
	/* #1.94, command: write_value, address: SEMC_BR0, value: 0x8000001B, size: 4 */
	0x40, 0x2F, 0x00, 0x10, 0x80, 0x00, 0x00, 0x1B,
	/* #1.95, command: write_value, address: SEMC_BR1, value: 0x8200001B, size: 4 */
	0x40, 0x2F, 0x00, 0x14, 0x82, 0x00, 0x00, 0x1B,
	/* #1.96, command: write_value, address: SEMC_BR2, value: 0x8400001B, size: 4 */
	0x40, 0x2F, 0x00, 0x18, 0x84, 0x00, 0x00, 0x1B,
	/* #1.97, command: write_value, address: SEMC_BR3, value: 0x8600001B, size: 4 */
	0x40, 0x2F, 0x00, 0x1C, 0x8C, 0x00, 0x00, 0x1B,
	/* #1.98, command: write_value, address: SEMC_BR4, value: 0x90000021, size: 4 */
	0x40, 0x2F, 0x00, 0x20, 0x90, 0x00, 0x00, 0x21,
	/* #1.99, command: write_value, address: SEMC_BR5, value: 0xA0000019, size: 4 */
	0x40, 0x2F, 0x00, 0x24, 0xA0, 0x00, 0x00, 0x19,
	/* #1.100, command: write_value, address: SEMC_BR6, value: 0xA8000017, size: 4 */
	0x40, 0x2F, 0x00, 0x28, 0xA8, 0x00, 0x00, 0x17,
	/* #1.101, command: write_value, address: SEMC_BR7, value: 0xA900001B, size: 4 */
	0x40, 0x2F, 0x00, 0x2C, 0xA9, 0x00, 0x00, 0x1B,
	/* #1.102, command: write_value, address: SEMC_BR8, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x30, 0x00, 0x00, 0x00, 0x21,
	/* #1.103, command: write_value, address: SEMC_IOCR, value: 0x79A8, size: 4 */
	0x40, 0x2F, 0x00, 0x04, 0x00, 0x00, 0x30, 0x00,
	/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF31, size: 4 */
	0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x31,
	/* #1.105, command: write_value, address: SEMC_SDRAMCR1, value: 0x652922, size: 4 */
	0x40, 0x2F, 0x00, 0x44, 0x00, 0x66, 0x4B, 0x22,
	/* #1.106, command: write_value, address: SEMC_SDRAMCR2, value: 0x10920, size: 4 */
	0x40, 0x2F, 0x00, 0x48, 0x00, 0x09, 0x09, 0x0B,
	/* #1.107, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A08, size: 4 */
	0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x00,
	/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */
	0x40, 0x2F, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21,
	/* #1.109, command: write_value, address: SEMC_DBICR1, value: 0x888888, size: 4 */
	0x40, 0x2F, 0x00, 0x84, 0x00, 0x88, 0x88, 0x88,
	/* #1.110, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
	0x40, 0x2F, 0x00, 0x94, 0x00, 0x00, 0x00, 0x02,
	/* #1.111, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
	0x40, 0x2F, 0x00, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.112, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
	0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
	/* #1.113, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
	0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
    /* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #5.1-2, command header bytes for merged 'Write - value' command */
    0xCC, 0x00, 0x14, 0x04,
    /* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
    0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
    /* #3.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
    0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
    /* #4, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #5.1-2, command header bytes for merged 'Write - value' command */
    0xCC, 0x00, 0x14, 0x04,
    /* #5.1, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
    0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
    /* #5.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
    0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
    /* #6, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #7.1-3, command header bytes for merged 'Write - value' command */
    0xCC, 0x00, 0x1C, 0x04,
    /* #7.1, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
    0x40, 0x2F, 0x00, 0xA0, 0x00, 0x00, 0x00, 0x33,
    /* #7.2, command: write_value, address: SEMC_IPCR0, value: 0x8C000000, size: 4 */
    0x40, 0x2F, 0x00, 0x90, 0x8C, 0x00, 0x00, 0x00,
    /* #7.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
    0x40, 0x2F, 0x00, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
    /* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */
    0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,
    /* #9, command: write_value, address: SEMC_SDRAMCR3, value: 0x50210A09, size: 4 */
	0xCC, 0x00, 0x0C, 0x04, 0x40, 0x2F, 0x00, 0x4C, 0x08, 0x07, 0x0A, 0x01};
/* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */
//316 bytes
#else
const uint8_t dcd_data[] = {0x00};
#endif /* XIP_BOOT_HEADER_DCD_ENABLE */
#endif /* XIP_BOOT_HEADER_ENABLE */&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Doris&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 12:07:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1678702#M208353</guid>
      <dc:creator>MCW</dc:creator>
      <dc:date>2023-06-29T12:07:19Z</dc:date>
    </item>
    <item>
      <title>Re: Could I initialize two SDRAMs by dcd.c?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1680235#M208517</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217913"&gt;@MCW&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Yes, you can enable two SDRAM in dcd. The RT1170 EVK has two SDRAM too, and they are initialized in DCD. It is needn't to write many SEMC register twice in DCD. You can refer to the dcd file in RT1170 SDK examples.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 07:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1680235#M208517</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-07-03T07:05:39Z</dc:date>
    </item>
    <item>
      <title>Re: Could I initialize two SDRAMs by dcd.c?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1681665#M208660</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61241"&gt;@jingpan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;It works after I add this code which is related to set&amp;nbsp; &lt;SPAN&gt;IOMUXC_GPIO_B0_02_SEMC_CSX03&amp;nbsp;&lt;/SPAN&gt;in the dcd.c&lt;/P&gt;&lt;LI-CODE lang="c"&gt;0x40, 0x1F, 0x81, 0x44, 0x00, 0x00, 0x00, 0x06,
0x40, 0x1F, 0x83, 0x34, 0x00, 0x01, 0x10, 0xF9,&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Doris&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 06:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1681665#M208660</guid>
      <dc:creator>MCW</dc:creator>
      <dc:date>2023-07-05T06:20:47Z</dc:date>
    </item>
    <item>
      <title>Re: Could I initialize two SDRAMs by dcd.c?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1681746#M208670</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61241"&gt;@jingpan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have one more question. I used the&lt;STRONG&gt; default dcd.c&lt;/STRONG&gt; which &lt;STRONG&gt;IOCR&lt;/STRONG&gt; defualt value is &lt;STRONG&gt;0x79A8&lt;/STRONG&gt;. And then I applied&amp;nbsp;&lt;SPAN&gt;SEMC_ConfigureSDRAM function to set two sdrams. The read/write result of the second SDRAM was wrong. However, the read/write result was correct when I set the value of IOCR as 0x39A8 in the dcd.c. I have checked the datasheet, 15-17 bits of IOCR register are used for&amp;nbsp;SEMC_RDY function selection. For my customize board, I don't use the SEMC_RDY pin because it is assigned for other gpio function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why setting MUX_RDY to 001 has some impacts on the second sdram read/write?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="IOCR_datasheet.png" style="width: 643px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230847i8FB0A0C78806A636/image-dimensions/643x670?v=v2" width="643" height="670" role="button" title="IOCR_datasheet.png" alt="IOCR_datasheet.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;IOCR_datasheet.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Doris&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 07:18:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1681746#M208670</guid>
      <dc:creator>MCW</dc:creator>
      <dc:date>2023-07-05T07:18:39Z</dc:date>
    </item>
    <item>
      <title>Re: Could I initialize two SDRAMs by dcd.c?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1682803#M208767</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217913"&gt;@MCW&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;To MUX_RDY field, 0x00079a8 is same to 0x00039a8. It is bit 17~15, all zero. What different is MUX_CSX3.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 06:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Could-I-initialize-two-SDRAMs-by-dcd-c/m-p/1682803#M208767</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2023-07-06T06:19:27Z</dc:date>
    </item>
  </channel>
</rss>