<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Reading BOOT_MODE[1,0] register</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1680155#M208499</link>
    <description>&lt;P&gt;You are not a software engineer. But you are not an engineer at all.&lt;/P&gt;&lt;P&gt;Till now, you did say which i.MX chip you are using, i.MX6, i.MX8MM or others.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you feel shame of yourself?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jul 2023 05:27:13 GMT</pubDate>
    <dc:creator>Mestkim</dc:creator>
    <dc:date>2023-07-03T05:27:13Z</dc:date>
    <item>
      <title>Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476087#M75508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Can I read in u-boot the BOOT_MODE[1,0] register? How?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thans,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 09:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476087#M75508</guid>
      <dc:creator>shonysinay</dc:creator>
      <dc:date>2016-02-22T09:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476088#M75509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it can be read using register SRC_SBMR2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 10:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476088#M75509</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-02-22T10:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476089#M75510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor, since I am not software engineer I don't even know the exact command. Please write the exact command for reading the SRC_SBMR2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 11:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476089#M75510</guid>
      <dc:creator>shonysinay</dc:creator>
      <dc:date>2016-02-22T11:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476090#M75511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach jtag and read SRC_SBMR2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 12:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476090#M75511</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-02-22T12:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476091#M75512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have JTAG. I download the u-boot through the serial port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can't I some u-boot command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 12:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/476091#M75512</guid>
      <dc:creator>shonysinay</dc:creator>
      <dc:date>2016-02-22T12:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1677852#M208284</link>
      <description>&lt;P&gt;For the IMX8MP, those flags are located at the following address:&lt;/P&gt;&lt;P&gt;```&lt;BR /&gt;# the BOOT_MODE register&lt;BR /&gt;boot_mode_bits_addr=0x30390073&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;You can find the exact address for your variant on its datasheel.&lt;/P&gt;&lt;P&gt;Then I just compared the values on that register to the one I'm expecting:&lt;/P&gt;&lt;P&gt;`cmp.b ${boot_mode_bits_addr} 0x2 1`&lt;/P&gt;&lt;P&gt;I compare the first byte of the content on `boot_mode_bits_addr` with `0x2`, and `test` to see if the result is 0 or 1.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 12:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1677852#M208284</guid>
      <dc:creator>joaofl</dc:creator>
      <dc:date>2023-06-28T12:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1680155#M208499</link>
      <description>&lt;P&gt;You are not a software engineer. But you are not an engineer at all.&lt;/P&gt;&lt;P&gt;Till now, you did say which i.MX chip you are using, i.MX6, i.MX8MM or others.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you feel shame of yourself?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 05:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1680155#M208499</guid>
      <dc:creator>Mestkim</dc:creator>
      <dc:date>2023-07-03T05:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: Reading BOOT_MODE[1,0] register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1680157#M208500</link>
      <description>&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;Till now, you did ask which chip it is.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you also feel shame of yourself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 05:29:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-BOOT-MODE-1-0-register/m-p/1680157#M208500</guid>
      <dc:creator>Mestkim</dc:creator>
      <dc:date>2023-07-03T05:29:26Z</dc:date>
    </item>
  </channel>
</rss>