<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About USB OTG Function in IMX8MP EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680061#M208485</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I connected a USB memory to PORT1 of USB Type-C to check the USB OTG function of EVK of IMX8MP.&lt;BR /&gt;At first the USB memory worked fine and there were no problems.&lt;BR /&gt;Then I connected it to my PC and nothing happened.&lt;BR /&gt;Can't it be used as a USB Device in the standard Linux BSP?&lt;BR /&gt;Or is it a circuit that the hardware cannot use as a USB Device?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;tomo&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jul 2023 02:50:53 GMT</pubDate>
    <dc:creator>tomo</dc:creator>
    <dc:date>2023-07-03T02:50:53Z</dc:date>
    <item>
      <title>About USB OTG Function in IMX8MP EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680061#M208485</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I connected a USB memory to PORT1 of USB Type-C to check the USB OTG function of EVK of IMX8MP.&lt;BR /&gt;At first the USB memory worked fine and there were no problems.&lt;BR /&gt;Then I connected it to my PC and nothing happened.&lt;BR /&gt;Can't it be used as a USB Device in the standard Linux BSP?&lt;BR /&gt;Or is it a circuit that the hardware cannot use as a USB Device?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;tomo&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 02:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680061#M208485</guid>
      <dc:creator>tomo</dc:creator>
      <dc:date>2023-07-03T02:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: About USB OTG Function in IMX8MP EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680543#M208553</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-as-USB-Slave-device/m-p/1664745#M207226" target="_blank"&gt;Solved: Re: i.MX8MM as USB Slave device. - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 13:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680543#M208553</guid>
      <dc:creator>dtony</dc:creator>
      <dc:date>2023-07-03T13:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: About USB OTG Function in IMX8MP EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680731#M208570</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I understood that it works with Device by using the gadget driver.&lt;BR /&gt;Is it possible to achieve Dual Role operation (Host and Device) just by adding a gadget driver?&lt;BR /&gt;If so, is the PTN5110 the only CC controller supported by the standard Linux BSP?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;tomo&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 23:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680731#M208570</guid>
      <dc:creator>tomo</dc:creator>
      <dc:date>2023-07-03T23:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: About USB OTG Function in IMX8MP EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680748#M208573</link>
      <description>&lt;P&gt;I checked a similar question thread below.&lt;BR /&gt;But that is not resolved yet.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Dual-role-testing/m-p/826729" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Dual-role-testing/m-p/826729&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jul 2023 00:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-USB-OTG-Function-in-IMX8MP-EVK/m-p/1680748#M208573</guid>
      <dc:creator>tomo</dc:creator>
      <dc:date>2023-07-04T00:25:03Z</dc:date>
    </item>
  </channel>
</rss>