<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GStreamer and NNStreamer use VX Delegate Fails in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1679796#M208455</link>
    <description>&lt;P&gt;I also tried using v4l2src to get a camera feed and filesrc from an .AVI file. Both attempts resulted in the same error.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jun 2023 19:11:56 GMT</pubDate>
    <dc:creator>KrisJ1</dc:creator>
    <dc:date>2023-06-30T19:11:56Z</dc:date>
    <item>
      <title>GStreamer and NNStreamer use VX Delegate Fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1675148#M208057</link>
      <description>&lt;P&gt;I am using a BoundaryDevices iMX8MP board and want to run predictions using TFLite and VX Delegate on the NPU. Here is my GStreamer command:&lt;/P&gt;&lt;PRE&gt;gst-launch-1.0 \
    videotestsrc is-live=1 ! \      
    video/x-raw,width=640,height=480 ! \
    &lt;SPAN class=""&gt;tee&lt;/SPAN&gt; name=t \    
    t. ! queue name=thread-nn max-size-buffers=2 leaky=2 ! \
    imxvideoconvert_g2d ! video/x-raw,width=300,height=300,format=RGBA ! videoconvert ! video/x-raw,format=RGB ! \      
    tensor_converter ! \
    tensor_transform mode=arithmetic option=typecast:float32,add:-127.5,div:127.5 ! \      
    tensor_filter framework=tensorflow-lite model=/home/root/nxp-nnstreamer-examples/detection/../downloads/models/detection/ssdlite_mobilene
t_v2_coco_no_postprocess.tflite custom=Delegate:External,ExtDelegateLib:libvx_delegate.so ! \      
    tensor_decoder mode=bounding_boxes option1=mobilenet-ssd option2=/home/root/nxp-nnstreamer-examples/detection/../downloads/models/detection/coco_labels_list.txt option3=/home/root/nxp-nnstreamer-examples/detection/../downloads/models/detection/box_priors.txt option4=640:480 option5=300:300 ! \
    videoconvert ! \      
    mix. \
    t. ! queue name=thread-img max-size-buffers=2 leaky=2 ! \      
    videoconvert ! \
    imxcompositor_g2d name=mix sink_0::zorder=2 sink_1::zorder=1 latency=300000000 min-upstream-latency=300000000 ! \      
    fpsdisplaysink video-sink=&lt;SPAN class=""&gt;$VID_SINK&lt;/SPAN&gt; name=&lt;SPAN class=""&gt;test&lt;/SPAN&gt; &lt;SPAN class=""&gt;sync&lt;/SPAN&gt;=&lt;SPAN class=""&gt;false&lt;/SPAN&gt; text-overlay=&lt;SPAN class=""&gt;true&lt;/SPAN&gt; -v 2&amp;gt;&amp;amp;1&lt;/PRE&gt;&lt;P&gt;I am using&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;custom=Delegate:External,ExtDelegateLib:libvx_delegate.so&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;to use the VX Delegate on the NPU. I have confirmed that this dynamic library is there, and it is usable since the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;benchmark-model&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;modelrunner&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;tools all allow the NPU to be used. When I run this GStreamer command, I get the following:&lt;/P&gt;&lt;PRE&gt;...
ERROR: Invoke called on model that is not ready.

** (gst-launch-1.0:1613): CRITICAL **: 21:30:40.018: Failed to invoke

** (gst-launch-1.0:1613): CRITICAL **: 21:30:40.019: /usr/lib/libnnstreamer-single.so(_backtrace_to_string+0x40) [0xffff6edb73c0]/usr/lib/gstreamer-1.0/libnnstreamer.so(+0x3d9ac) [0xffff6ee1d9ac]/usr/lib/libgstbase-1.0.so.0(+0x48704) [0xffff87198704]/usr/lib/libgstbase-1.0.so.0(+0x47dd4) [0xffff87197dd4]/usr/lib/libgstreamer-1.0.so.0(+0x8e908) [0xffff8783e908]/usr/lib/libgstreamer-1.0.so.0(+0x90798) [0xffff87840798]/usr/lib/libgstbase-1.0.so.0(+0x47ee8) [0xffff87197ee8]/usr/lib/libgstreamer-1.0.so.0(+0x8e908) [0xffff8783e908]/usr/lib/libgstreamer-1.0.so.0(+0x90798) [0xffff87840798]/usr/lib/gstreamer-1.0/libnnstreamer.so(+0x1fba0) [0xffff6edffba0]/usr/lib/libgstreamer-1.0.so.0(+0x8e908) [0xffff8783e908]/usr/lib/libgstreamer-1.0.so.0(+0x90798) [0xffff87840798]/usr/lib/libgstbase-1.0.so.0(+0x47ee8) [0xffff87197ee8]/usr/lib/libgstreamer-1.0.so.0(+0x8e908) [0xffff8783e908]/usr/lib/libgstreamer-1.0.so.0(+0x90798) [0xffff87840798]/usr/lib/libgstbase-1.0.so.0(+0x47ee8) [0xffff87197ee8]/usr/lib/libgstreamer-1.0.so.0(+0x8e908) [0xffff8783e908]/usr/lib/libgstreamer-1.0.so.0(+0x90798) [0xffff87840798]/usr/lib/libgstbase-1.0.so.0(+0x47ee8) [0xffff87197ee8]/usr/lib/libgstreamer-1.0.so.0(+0x8e908) [0xffff8783e908]


** (gst-launch-1.0:1613): CRITICAL **: 21:30:40.019: Calling invoke function (inference instance) of the tensor-filter subplugin (tensorflow-lite for /home/root/nxp-nnstreamer-examples/detection/../downloads/models/detection/ssdlite_mobilenet_v2_coco_no_postprocess.tflite) has failed with error code (-1).

ERROR: from element /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0: Internal data stream error.
Additional debug info:
../git/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0:
streaming stopped, reason error (-5)
Execution ended after 0:00:00.063685468
Setting pipeline to NULL ...
ERROR: from element /GstPipeline:pipeline0/GstQueue:thread-nn: Internal data stream error.
Additional debug info:
../git/plugins/elements/gstqueue.c(992): gst_queue_handle_sink_event (): /GstPipeline:pipeline0/GstQueue:thread-nn:
streaming stopped, reason error (-5)
...&lt;/PRE&gt;&lt;P&gt;Any help resolving this will be greatly appreciated. If this is not the right stack exchange to post this question, please inform me where I can post to get an answer. Also, let me know if you need any more information about the system I am running.&lt;/P&gt;&lt;P&gt;More information about the system:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Linux info:&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;Linux nitrogen8mp 5.15.71-2.2.0+yocto+gd4a57b30c1d1&lt;/LI&gt;&lt;LI&gt;Custom Yocto build with GStreamer, NNStreamer, and TFLite VX Delegate installed.&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Fri, 23 Jun 2023 21:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1675148#M208057</guid>
      <dc:creator>KrisJ1</dc:creator>
      <dc:date>2023-06-23T21:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer and NNStreamer use VX Delegate Fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1676704#M208200</link>
      <description>&lt;P&gt;Which kind of video source you want to use? from camera or from video file?&lt;/P&gt;
&lt;P&gt;I can't find you set the valid input source.&lt;/P&gt;
&lt;P&gt;Please refer chapter&amp;nbsp;&lt;STRONG&gt;10 Vision Pipeline with NNStreamer&lt;/STRONG&gt; in this guide: &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 06:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1676704#M208200</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-06-27T06:48:21Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer and NNStreamer use VX Delegate Fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1677997#M208295</link>
      <description>&lt;P&gt;I am using videotestsrc which is random video generated indefinitely by GStreamer and doesn't have a framerate limit allowing me to test the true performance of the model.&amp;nbsp;&lt;A href="https://gstreamer.freedesktop.org/documentation/videotestsrc/index.html?gi-language=c" target="_blank"&gt;https://gstreamer.freedesktop.org/documentation/videotestsrc/index.html?gi-language=c&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 16:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1677997#M208295</guid>
      <dc:creator>KrisJ1</dc:creator>
      <dc:date>2023-06-28T16:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer and NNStreamer use VX Delegate Fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1679796#M208455</link>
      <description>&lt;P&gt;I also tried using v4l2src to get a camera feed and filesrc from an .AVI file. Both attempts resulted in the same error.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 19:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-and-NNStreamer-use-VX-Delegate-Fails/m-p/1679796#M208455</guid>
      <dc:creator>KrisJ1</dc:creator>
      <dc:date>2023-06-30T19:11:56Z</dc:date>
    </item>
  </channel>
</rss>