<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8QXP Ethernet strap options</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676612#M208191</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200437"&gt;@Chethanbg&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;In i.MX8QXP EVK, the strap resistors belong to the Ethernet PHY chip&amp;nbsp;AR8031 and are configured as per the modes mentioned in the Ethernet PHY datasheet.&lt;/P&gt;
&lt;P&gt;So, one can refer to the KSZ8041 datasheet and can configure the strap resistors accordingly in your custom board.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
    <pubDate>Tue, 27 Jun 2023 05:59:26 GMT</pubDate>
    <dc:creator>riteshmpatel</dc:creator>
    <dc:date>2023-06-27T05:59:26Z</dc:date>
    <item>
      <title>IMX8QXP Ethernet strap options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676044#M208151</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As per&amp;nbsp;IMX8QXP eval board there is mode2[3:0] settings strap resistors options&lt;/P&gt;&lt;P&gt;In our custom board we are using IMX8QXP with KSZ8041RNL in RMII (10/100Mbps )&lt;/P&gt;&lt;P&gt;My query is&lt;/P&gt;&lt;P&gt;In eval board these strap resistors are belongs to&amp;nbsp;AR8031 or IMX8QXP?&lt;/P&gt;&lt;P&gt;We are using IMX8QXP with KSZ8041 so any mode settings to be done through hardware to select RMII?&lt;/P&gt;&lt;P&gt;In Datasheet or Reference manual of IMX8QXP there is no information on MODE setting strap resistors&lt;/P&gt;&lt;P&gt;Kindly clarify&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 12:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676044#M208151</guid>
      <dc:creator>Chethanbg</dc:creator>
      <dc:date>2023-06-26T12:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP Ethernet strap options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676612#M208191</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200437"&gt;@Chethanbg&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;In i.MX8QXP EVK, the strap resistors belong to the Ethernet PHY chip&amp;nbsp;AR8031 and are configured as per the modes mentioned in the Ethernet PHY datasheet.&lt;/P&gt;
&lt;P&gt;So, one can refer to the KSZ8041 datasheet and can configure the strap resistors accordingly in your custom board.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 05:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676612#M208191</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-06-27T05:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP Ethernet strap options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676654#M208194</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.Currently in RMII mode we are using 25 Mhz crystal mode&lt;/P&gt;&lt;P&gt;The KSZ8041RNL generates the 50MHz RMII REF_CLK and outputs it to the MAC&lt;/P&gt;&lt;P&gt;attached is the block diagram for your reference.&lt;/P&gt;&lt;P&gt;In pin configuration RGMII_TXC should be configured as ENET0_RCLK50M_IN input&amp;nbsp; right?&lt;/P&gt;&lt;P&gt;IMX8QXP_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;0x06000061&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also let us know the pad settings&amp;nbsp;&amp;nbsp;0x06000061 is correct&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 06:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676654#M208194</guid>
      <dc:creator>Chethanbg</dc:creator>
      <dc:date>2023-06-27T06:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP Ethernet strap options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676661#M208196</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200437"&gt;@Chethanbg&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I request you to please raise a new ticket for the additional questions.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 06:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-Ethernet-strap-options/m-p/1676661#M208196</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-06-27T06:22:50Z</dc:date>
    </item>
  </channel>
</rss>