<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mp can not boot up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675881#M208134</link>
    <description>&lt;P&gt;I am using the 9th version of the DDR tool and configured it according to the chip manual in the attachment&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 09:06:40 GMT</pubDate>
    <dc:creator>xjy198903</dc:creator>
    <dc:date>2023-06-26T09:06:40Z</dc:date>
    <item>
      <title>imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675427#M208088</link>
      <description>&lt;P&gt;I have a self-made imx8mp board, use DDR4 memory, use yocto to compile the image and burn the SD card, the serial port output:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot SPL 2022.04-uboot_v2022.04-2.5.0+g5fb673f885 (Jun 25 2023 - 07:03:55 +0000)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: start DRAM init&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: DRAM rate 3200MTS&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO:ddrphy calibration done&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: ddrmix config done&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;SEC0: RNG instantiated&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Trying to boot from BOOTROM&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Boot Stage: Primary boot&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL31: v2.6(release):lf-5.15.71-2.2.0-0-g3c1583ba0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL31: Built : 11:00:38, Nov 21 2022&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;and stuck here&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 08:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675427#M208088</guid>
      <dc:creator>xjy198903</dc:creator>
      <dc:date>2023-06-25T08:56:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675448#M208090</link>
      <description>&lt;P&gt;did you pass ddr stress test? if no, pls check the document&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 09:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675448#M208090</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-06-25T09:29:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675457#M208091</link>
      <description>&lt;P&gt;No，it can not pass&amp;nbsp;the DDR stress test ,and the uart shows:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Download is complete&lt;BR /&gt;Waiting for the target board boot...&lt;/P&gt;&lt;P&gt;===================hardware_init=====================&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;********Found PMIC PCA9450**********&lt;BR /&gt;hardware_init exit&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;MX8 DDR Stress Test V3.30&lt;BR /&gt;Built on Nov 24 2021 13:52:12&lt;BR /&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;Waiting for board configuration from PC-end...&lt;/P&gt;&lt;P&gt;--Set up the MMU and enable I and D cache--&lt;BR /&gt;- This is the Cortex-A53 core&lt;BR /&gt;- Check if I cache is enabled&lt;BR /&gt;- Enabling I cache since it was disabled&lt;BR /&gt;- Push base address of TTB to TTBR0_EL3&lt;BR /&gt;- Config TCR_EL3&lt;BR /&gt;- Config MAIR_EL3&lt;BR /&gt;- Enable MMU&lt;BR /&gt;- Data Cache has been enabled&lt;BR /&gt;- Check system memory register, only for debug&lt;/P&gt;&lt;P&gt;- VMCR Check:&lt;BR /&gt;- ttbr0_el3: 0x97d000&lt;BR /&gt;- tcr_el3: 0x2051c&lt;BR /&gt;- mair_el3: 0x774400&lt;BR /&gt;- sctlr_el3: 0xc01815&lt;BR /&gt;- id_aa64mmfr0_el1: 0x1122&lt;/P&gt;&lt;P&gt;- MMU and cache setup complete&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM clock(CA53) rate: 1800MHz&lt;BR /&gt;DDR Clock: 1600MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is DDR4&lt;BR /&gt;Data width: 32, bank num: 16&lt;BR /&gt;For DDR4, bank num is the total of 4 bank groups and 4 banks per group&lt;BR /&gt;Row size: 17, col size: 10&lt;BR /&gt;One chip select is used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 8192MB&lt;BR /&gt;Density per controller is: 8192MB&lt;BR /&gt;Total density detected on the board is: 8192MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8M-plus: Cortex-A53 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;============ Step 1: DDRPHY Training... ============&lt;BR /&gt;---DDR 1D-Training @1600Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of read DQ deskew training&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 1D-Training @668Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of read enable training&lt;BR /&gt;[Process] End of fine write leveling&lt;BR /&gt;[Process] End of MPR read delay center optimization&lt;BR /&gt;[Process] End of Write Leveling coarse delay&lt;BR /&gt;[Process] End of write delay center optimization&lt;BR /&gt;[Process] End of read delay center optimization&lt;BR /&gt;[Process] End of max read latency training&lt;BR /&gt;[Result] PASS&lt;BR /&gt;---DDR 2D-Training @1600Mhz...&lt;BR /&gt;[Process] End of initialization&lt;BR /&gt;[Process] End of 2D write delay/voltage center optimization&lt;BR /&gt;[Process] End of 2D read delay/voltage center optimization&lt;BR /&gt;[Result] PASS&lt;/P&gt;&lt;P&gt;============ Step 2: DDR memory accessing... ============&lt;BR /&gt;Verifying DDR frequency point0@1600MHz......Address of failure: 0x0000000040080040&lt;BR /&gt;Data read was: 0x0000000040008040&lt;BR /&gt;But pattern was: 0x0000000040000040&lt;BR /&gt;Failed&lt;BR /&gt;Please modify DDRC/DFI parameters!!!&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 09:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675457#M208091</guid>
      <dc:creator>xjy198903</dc:creator>
      <dc:date>2023-06-25T09:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675852#M208130</link>
      <description>&lt;P&gt;I don't know how you set the PAR files, pls check if you set correct or not, more detailed information, pls refer to the link as below&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 08:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675852#M208130</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-06-26T08:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675881#M208134</link>
      <description>&lt;P&gt;I am using the 9th version of the DDR tool and configured it according to the chip manual in the attachment&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 09:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1675881#M208134</guid>
      <dc:creator>xjy198903</dc:creator>
      <dc:date>2023-06-26T09:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1678360#M208324</link>
      <description>&lt;P&gt;pls refer to this&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Add-DDR4-memory-to-imx8mp/m-p/1610671" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Add-DDR4-memory-to-imx8mp/m-p/1610671&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 05:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1678360#M208324</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-06-29T05:38:47Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1678371#M208327</link>
      <description>&lt;P&gt;I've read that article, followed the tips above, and now my board keeps outputting in a loop:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xjy198903_0-1688017501303.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/229974i4F53D51CE221FBC9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xjy198903_0-1688017501303.png" alt="xjy198903_0-1688017501303.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It feels like the board is stuck in an endless loop&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 05:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1678371#M208327</guid>
      <dc:creator>xjy198903</dc:creator>
      <dc:date>2023-06-29T05:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1678413#M208331</link>
      <description>&lt;P&gt;at first, you need to use the DDR tool to regenerate new DDR script for your memory, then with the new timing file, you can apply it to your memory, btw, try to use&lt;/P&gt;
&lt;P&gt;please set PHY_SDRAM_SIZE to 0xC0000000 and PHY_SDRAM_2_SIZE to 0x140000000&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 06:27:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1678413#M208331</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-06-29T06:27:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp can not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1680550#M208554</link>
      <description>&lt;P&gt;hello&amp;nbsp;&lt;A id="link_48" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217094" target="_self" aria-label="View Profile of xjy198903"&gt;&lt;SPAN class=""&gt;xjy198903&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;How is the current progress, is your board able to access ddr now?&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 13:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-can-not-boot-up/m-p/1680550#M208554</guid>
      <dc:creator>kenli</dc:creator>
      <dc:date>2023-07-03T13:48:00Z</dc:date>
    </item>
  </channel>
</rss>