<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Query on HAB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1675675#M208113</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212905"&gt;@Maheshkadam9922&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Whether it can be debugged has nothing to do with the signature or encryption of the image itself. e.g.,&amp;nbsp;JLINK tool.&amp;nbsp; As long as it is debugged in the attach mode and JTAG is not disabled, it can be debugged.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 06:40:44 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2023-06-26T06:40:44Z</dc:date>
    <item>
      <title>Query on HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1673439#M207941</link>
      <description>&lt;P&gt;we have one query below&lt;/P&gt;&lt;P&gt;suppose we flash the signed or encrypted image image on mxrt1050 evk board using secure provisioning tool after then can we debug the code using MCUxpesso tool ?.&lt;/P&gt;&lt;P&gt;we have only one board so one development team working on CAN code , so they need to debug code using MCUxpresso tool&amp;nbsp;&lt;/P&gt;&lt;P&gt;we also show the demo of HAB signed image .&lt;/P&gt;&lt;P&gt;actually our plan to flash the CAN code using secure tool with activate signed (HAB) feature and debug this code using MCUXpresso tool&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 08:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1673439#M207941</guid>
      <dc:creator>Maheshkadam9922</dc:creator>
      <dc:date>2023-06-21T08:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: Query on HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1673772#M207966</link>
      <description>&lt;P&gt;Our development team is currently working on CAN code for the MXRT1050 EVK board and we want flash a signed or encrypted image using the secure provisioning tool, which activates the High Assurance Boot (HAB) feature.&lt;/P&gt;&lt;P&gt;However, we would like to inquire about the possibility of debugging the same code using the MCUxpresso tool after flashing the HAB-signed image using secure provisioning tool. Since we only have one board available, Can our development team to be able to debug the CAN code using the familiar MCUxpresso tool after flashing CAN code with the HAB-signed image using secure provisioning tool?&lt;/P&gt;&lt;P&gt;Could you kindly confirm whether it is possible to debug the code using the MCUxpresso tool after flashing a HAB-signed image?&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 16:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1673772#M207966</guid>
      <dc:creator>Maheshkadam9922</dc:creator>
      <dc:date>2023-06-21T16:04:04Z</dc:date>
    </item>
    <item>
      <title>Re: Query on HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1675675#M208113</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212905"&gt;@Maheshkadam9922&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Whether it can be debugged has nothing to do with the signature or encryption of the image itself. e.g.,&amp;nbsp;JLINK tool.&amp;nbsp; As long as it is debugged in the attach mode and JTAG is not disabled, it can be debugged.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 06:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Query-on-HAB/m-p/1675675#M208113</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-06-26T06:40:44Z</dc:date>
    </item>
  </channel>
</rss>