<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx8mp ban not boot up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ban-not-boot-up/m-p/1675424#M208086</link>
    <description>&lt;P&gt;I have a self-made imx8mp board, use DDR4 memory, use yocto to compile the image and burn the SD card, the serial port output:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot SPL 2022.04-uboot_v2022.04-2.5.0+g5fb673f885 (Jun 25 2023 - 07:03:55 +0000)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: start DRAM init&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: DRAM rate 3200MTS&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO:ddrphy calibration done&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: ddrmix config done&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;SEC0: RNG instantiated&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Trying to boot from BOOTROM&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Boot Stage: Primary boot&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL31: v2.6(release):lf-5.15.71-2.2.0-0-g3c1583ba0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL31: Built : 11:00:38, Nov 21 2022&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;and stuck here&lt;/P&gt;</description>
    <pubDate>Sun, 25 Jun 2023 08:54:52 GMT</pubDate>
    <dc:creator>xjy198903</dc:creator>
    <dc:date>2023-06-25T08:54:52Z</dc:date>
    <item>
      <title>imx8mp ban not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ban-not-boot-up/m-p/1675424#M208086</link>
      <description>&lt;P&gt;I have a self-made imx8mp board, use DDR4 memory, use yocto to compile the image and burn the SD card, the serial port output:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot SPL 2022.04-uboot_v2022.04-2.5.0+g5fb673f885 (Jun 25 2023 - 07:03:55 +0000)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: start DRAM init&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: DRAM rate 3200MTS&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO:ddrphy calibration done&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDRINFO: ddrmix config done&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;SEC0: RNG instantiated&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Trying to boot from BOOTROM&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Boot Stage: Primary boot&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL31: v2.6(release):lf-5.15.71-2.2.0-0-g3c1583ba0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL31: Built : 11:00:38, Nov 21 2022&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;and stuck here&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 08:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ban-not-boot-up/m-p/1675424#M208086</guid>
      <dc:creator>xjy198903</dc:creator>
      <dc:date>2023-06-25T08:54:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp ban not boot up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ban-not-boot-up/m-p/1675428#M208089</link>
      <description>&lt;P&gt;wrong title&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 08:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ban-not-boot-up/m-p/1675428#M208089</guid>
      <dc:creator>xjy198903</dc:creator>
      <dc:date>2023-06-25T08:57:01Z</dc:date>
    </item>
  </channel>
</rss>