<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8MP EQOS MAC Minimal Required Kernel Configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EQOS-MAC-Minimal-Required-Kernel-Configuration/m-p/1674550#M208007</link>
    <description>&lt;P&gt;Hi, we are using a SOM (VAR-DART-MX8M-PLUS) from Variscite based on &lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;When the kernel (linux-imx v5.15.71) compiled with the default configuration, the board can boot over TFTP/NFS using EQOS (with ADIN1300 PHY) ethernet interface. But when I reconfigure the kernel to disable some features/drivers I don't need, it can't boot due to missing dwmac support (Happened before, dwmac wasn't configured) and hangs until VFS throws an error since it could not mount NFS. I configured STMMAC_ETH as builtin and checked every related configuration that I could think of. (I checked NXP's linux reference manual but couldn't find anything about eqos. I might be checking the wrong document.)&lt;/P&gt;&lt;P&gt;I tried to compare default and my defconfig but since the diff is too big, I couldn't find the issue with my configuration. I believe there is some dependency between a disabled configuration with EQOS Eth interface I couldn't find. I am sharing both default and custom defconfigs. Both are outputs of &lt;EM&gt;savedefconfig&lt;/EM&gt; task of bitbake recipe.&lt;BR /&gt;&lt;BR /&gt;So, what I am missing here? Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Thu, 22 Jun 2023 15:53:56 GMT</pubDate>
    <dc:creator>uediz</dc:creator>
    <dc:date>2023-06-22T15:53:56Z</dc:date>
    <item>
      <title>i.MX8MP EQOS MAC Minimal Required Kernel Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EQOS-MAC-Minimal-Required-Kernel-Configuration/m-p/1674550#M208007</link>
      <description>&lt;P&gt;Hi, we are using a SOM (VAR-DART-MX8M-PLUS) from Variscite based on &lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;When the kernel (linux-imx v5.15.71) compiled with the default configuration, the board can boot over TFTP/NFS using EQOS (with ADIN1300 PHY) ethernet interface. But when I reconfigure the kernel to disable some features/drivers I don't need, it can't boot due to missing dwmac support (Happened before, dwmac wasn't configured) and hangs until VFS throws an error since it could not mount NFS. I configured STMMAC_ETH as builtin and checked every related configuration that I could think of. (I checked NXP's linux reference manual but couldn't find anything about eqos. I might be checking the wrong document.)&lt;/P&gt;&lt;P&gt;I tried to compare default and my defconfig but since the diff is too big, I couldn't find the issue with my configuration. I believe there is some dependency between a disabled configuration with EQOS Eth interface I couldn't find. I am sharing both default and custom defconfigs. Both are outputs of &lt;EM&gt;savedefconfig&lt;/EM&gt; task of bitbake recipe.&lt;BR /&gt;&lt;BR /&gt;So, what I am missing here? Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 15:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EQOS-MAC-Minimal-Required-Kernel-Configuration/m-p/1674550#M208007</guid>
      <dc:creator>uediz</dc:creator>
      <dc:date>2023-06-22T15:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP EQOS MAC Minimal Required Kernel Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EQOS-MAC-Minimal-Required-Kernel-Configuration/m-p/1675005#M208044</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Maybe &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/44188"&gt;@variscite&lt;/a&gt; can help here.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jun 2023 14:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EQOS-MAC-Minimal-Required-Kernel-Configuration/m-p/1675005#M208044</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-06-23T14:15:31Z</dc:date>
    </item>
  </channel>
</rss>