<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Disabling internal pull up in Analog input pin for ADC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1673811#M207968</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I couldn't find an issue as suggested in that thread. I am not using the parameters he found issue with.&lt;/P&gt;&lt;P&gt;Do you have an overlay for adc that is tested and working in i.mx6ul ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shafy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 21 Jun 2023 16:47:55 GMT</pubDate>
    <dc:creator>Shafy</dc:creator>
    <dc:date>2023-06-21T16:47:55Z</dc:date>
    <item>
      <title>Disabling internal pull up in Analog input pin for ADC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1672903#M207881</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have configured the IO09 as analog input pin for ADC in the i.mx6UL processor (myirtech mys-6ul board)&lt;/P&gt;&lt;P&gt;I am using the following pin configuration in the dts&lt;/P&gt;&lt;P&gt;pinctrl_adc1: adc1grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0xb0&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;But the issue is the pin in internally pulled up to 3.3V.&amp;nbsp; So when no external voltage is connected, ADC reading is giving the value 4095.&amp;nbsp;&amp;nbsp; When external voltage is connected, it is causing the reading go wrong.&amp;nbsp; I have tried configuring the IO05 also with the same result.&amp;nbsp; I have confirmed that these pins are not used in any other configuration in the dts.&lt;/P&gt;&lt;P&gt;How can I disable the internal pull up&amp;nbsp; ?&amp;nbsp; I have tried the bias-disable = &amp;lt;1&amp;gt;; in the dts with no effect.&lt;/P&gt;&lt;P&gt;Can some one advise ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Shafy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 16:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1672903#M207881</guid>
      <dc:creator>Shafy</dc:creator>
      <dc:date>2023-06-20T16:44:35Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling internal pull up in Analog input pin for ADC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1673004#M207892</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;I think you can get started with this &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Disabling-default-gpio-pull-down-not-working-imx8mm/m-p/1564486" target="_self"&gt;thread&lt;/A&gt;, likely there is an overlay between its use within other dtb or a driver that uses that pin.&lt;/P&gt;
&lt;P&gt;You can run the tests that he ran, please provide the results.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 20:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1673004#M207892</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-06-20T20:36:15Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling internal pull up in Analog input pin for ADC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1673811#M207968</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I couldn't find an issue as suggested in that thread. I am not using the parameters he found issue with.&lt;/P&gt;&lt;P&gt;Do you have an overlay for adc that is tested and working in i.mx6ul ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shafy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 16:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1673811#M207968</guid>
      <dc:creator>Shafy</dc:creator>
      <dc:date>2023-06-21T16:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling internal pull up in Analog input pin for ADC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1678887#M208370</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It's for debugging, could you verify at userspace that the value isn't overwritten, but I'm attaching a presentation that will be more useful, could you verify the values for the GPIO to see that they're being changed?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 17:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disabling-internal-pull-up-in-Analog-input-pin-for-ADC/m-p/1678887#M208370</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-06-29T17:36:56Z</dc:date>
    </item>
  </channel>
</rss>