<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックyocto package generation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-package-generation/m-p/1673607#M207953</link>
    <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;generating the imx-image-full for iMX8, it seems that the different deb files are generated each time i run the full build, after deleting tmp folder.&lt;/P&gt;&lt;P&gt;for example, i used&amp;nbsp; packagegroup-fsl-gstreamer1.0-base, and it was not created after a rebuild. i made no change to local.conf&lt;/P&gt;</description>
    <pubDate>Wed, 21 Jun 2023 11:49:14 GMT</pubDate>
    <dc:creator>ronjacoby1</dc:creator>
    <dc:date>2023-06-21T11:49:14Z</dc:date>
    <item>
      <title>yocto package generation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-package-generation/m-p/1673607#M207953</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;generating the imx-image-full for iMX8, it seems that the different deb files are generated each time i run the full build, after deleting tmp folder.&lt;/P&gt;&lt;P&gt;for example, i used&amp;nbsp; packagegroup-fsl-gstreamer1.0-base, and it was not created after a rebuild. i made no change to local.conf&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 11:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-package-generation/m-p/1673607#M207953</guid>
      <dc:creator>ronjacoby1</dc:creator>
      <dc:date>2023-06-21T11:49:14Z</dc:date>
    </item>
    <item>
      <title>Re: yocto package generation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-package-generation/m-p/1675752#M208122</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219245"&gt;@ronjacoby1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It should be no such difference when no changes to build configuration or environments, such as&amp;nbsp;&lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;change the target MACHINE?&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;Or do repo sync on the basis of internal xml?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;Best regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;Harvey&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 07:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-package-generation/m-p/1675752#M208122</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-06-26T07:31:11Z</dc:date>
    </item>
  </channel>
</rss>