<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Generate and load a UUU image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672185#M207822</link>
    <description>&lt;P&gt;I am unclear on how UUU works. &amp;nbsp;I have a Compulab that ships with Debian Linux. &amp;nbsp;I have it configured the way I want it, and would like to create an image to burn for UUU. &amp;nbsp;Do I use "dd" to create the image? &amp;nbsp;Do I dd the whole EMMC drive or just the root partition? &amp;nbsp;Do I need to do anything for the EFI boot partition? &amp;nbsp;What is the right command to flash it back to the Compulab? &amp;nbsp;Do I need to flash the boot loader or just leave it?&lt;/P&gt;&lt;P&gt;The documentation about UUU doesn't say anything about where these images are coming from. &amp;nbsp;It's also unclear from the documentation which arguments are files, pre-installed scripts, or what/where they came from. &amp;nbsp;Trying to avoid just playing with this because I don't want to accidentally break anything. &amp;nbsp;I'm very experienced in Linux admin, but not very experienced in the embedded side.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jun 2023 20:44:39 GMT</pubDate>
    <dc:creator>johnnyb61820</dc:creator>
    <dc:date>2023-06-19T20:44:39Z</dc:date>
    <item>
      <title>Generate and load a UUU image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672185#M207822</link>
      <description>&lt;P&gt;I am unclear on how UUU works. &amp;nbsp;I have a Compulab that ships with Debian Linux. &amp;nbsp;I have it configured the way I want it, and would like to create an image to burn for UUU. &amp;nbsp;Do I use "dd" to create the image? &amp;nbsp;Do I dd the whole EMMC drive or just the root partition? &amp;nbsp;Do I need to do anything for the EFI boot partition? &amp;nbsp;What is the right command to flash it back to the Compulab? &amp;nbsp;Do I need to flash the boot loader or just leave it?&lt;/P&gt;&lt;P&gt;The documentation about UUU doesn't say anything about where these images are coming from. &amp;nbsp;It's also unclear from the documentation which arguments are files, pre-installed scripts, or what/where they came from. &amp;nbsp;Trying to avoid just playing with this because I don't want to accidentally break anything. &amp;nbsp;I'm very experienced in Linux admin, but not very experienced in the embedded side.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 20:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672185#M207822</guid>
      <dc:creator>johnnyb61820</dc:creator>
      <dc:date>2023-06-19T20:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Generate and load a UUU image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672854#M207880</link>
      <description>&lt;P&gt;I think I have it figured out.&lt;/P&gt;&lt;P&gt;To get the filesystem image, I did:&lt;/P&gt;&lt;P&gt;dd if=/dev/mmcblk2 | ssh -C &lt;A href="mailto:myuser@mycomputer" target="_blank"&gt;myuser@mycomputer&lt;/A&gt;&amp;nbsp;'cat &amp;gt; disk.img'&lt;/P&gt;&lt;P&gt;Then, I downloaded the U-boot "firmware recovery image" from Compulab. &amp;nbsp;I'm not sure this is correctly named. &amp;nbsp;I decompressed the zip file, and it has two flash files inside the zip file. &amp;nbsp;I'm not 100% sure, but it looks like you choose the flash file based on the amount of memory on your Compulab. &amp;nbsp;I used&amp;nbsp;flash.bin.d2d4.&lt;/P&gt;&lt;P&gt;Then, to flash the system, I plugged into the programming port and restarted the device. &amp;nbsp;Then I ran:&lt;/P&gt;&lt;P&gt;uuu -b emmc_all&amp;nbsp;flash.bin.d2d4 disk.img&lt;/P&gt;&lt;P&gt;This resulted in a fully working system.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 16:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672854#M207880</guid>
      <dc:creator>johnnyb61820</dc:creator>
      <dc:date>2023-06-20T16:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: Generate and load a UUU image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672944#M207886</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;It is good to know that that your process resulted in a fully working system.&lt;/P&gt;
&lt;P&gt;Also, I suggest you check the next links for a more information:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Flashing-Linux-BSP-using-UUU/ta-p/1110679" target="_self"&gt;Flashing Linux BSP using UUU.&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_self"&gt;i.MX Yocto Project User's Guide.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;Jorge.&lt;/P&gt;
&lt;P&gt;Jorge.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 18:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generate-and-load-a-UUU-image/m-p/1672944#M207886</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-06-20T18:11:56Z</dc:date>
    </item>
  </channel>
</rss>