<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Booting from the SD Card in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1668978#M207566</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Dear NXP community,&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;I have faced difficulties trying to boot from the SD Card on the i.MX 8M Mini board.&lt;BR /&gt;&lt;BR /&gt;Currently, I am using the &lt;STRONG&gt;pre-built image&lt;/STRONG&gt; that we downloaded from the Linux download page linked in the Getting Started guide. We successfully loaded this image onto the board's &lt;STRONG&gt;internal memory&lt;/STRONG&gt;. To establish communication with the board, we have set up a serial connection using &lt;STRONG&gt;TeraTerm&lt;/STRONG&gt;.&lt;BR /&gt;&lt;BR /&gt;The SD card contains a &lt;STRONG&gt;.wic file&lt;/STRONG&gt; from the same image, and we have also ensured that the &lt;STRONG&gt;boot switches&lt;/STRONG&gt; are configured properly to boot from the SD Card. However, when we power on the board, the &lt;STRONG&gt;Status LED (D1)&lt;/STRONG&gt; does not glow up, as it normally does when booting from the eMMC, and there is no boot log when booting from SD Card, as there is when booting from the internal memory. D708 is red and D905 is blinking during the booting process.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;I would appreciate your assistance.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Tatiana&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jun 2023 06:52:01 GMT</pubDate>
    <dc:creator>tatianabkirillova</dc:creator>
    <dc:date>2023-06-14T06:52:01Z</dc:date>
    <item>
      <title>Booting from the SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1668978#M207566</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear NXP community,&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;I have faced difficulties trying to boot from the SD Card on the i.MX 8M Mini board.&lt;BR /&gt;&lt;BR /&gt;Currently, I am using the &lt;STRONG&gt;pre-built image&lt;/STRONG&gt; that we downloaded from the Linux download page linked in the Getting Started guide. We successfully loaded this image onto the board's &lt;STRONG&gt;internal memory&lt;/STRONG&gt;. To establish communication with the board, we have set up a serial connection using &lt;STRONG&gt;TeraTerm&lt;/STRONG&gt;.&lt;BR /&gt;&lt;BR /&gt;The SD card contains a &lt;STRONG&gt;.wic file&lt;/STRONG&gt; from the same image, and we have also ensured that the &lt;STRONG&gt;boot switches&lt;/STRONG&gt; are configured properly to boot from the SD Card. However, when we power on the board, the &lt;STRONG&gt;Status LED (D1)&lt;/STRONG&gt; does not glow up, as it normally does when booting from the eMMC, and there is no boot log when booting from SD Card, as there is when booting from the internal memory. D708 is red and D905 is blinking during the booting process.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;I would appreciate your assistance.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Tatiana&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 06:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1668978#M207566</guid>
      <dc:creator>tatianabkirillova</dc:creator>
      <dc:date>2023-06-14T06:52:01Z</dc:date>
    </item>
    <item>
      <title>Re: Booting from the SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1670894#M207711</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214410"&gt;@tatianabkirillova&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you try to re-flash image to SD Card with command uuu -b sd (sd_all) "&lt;STRONG&gt;pre-built image&lt;/STRONG&gt;"? probably images damaged.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 07:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1670894#M207711</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-06-16T07:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: Booting from the SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1680327#M208524</link>
      <description>&lt;P&gt;I solved the problem by using the following command:&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;uuu -b sd_all imx-boot-imx8mm-lpddr4-evk-sd.bin-flash_evk imx-image-full-imx8mmevk.wic&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 08:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-from-the-SD-Card/m-p/1680327#M208524</guid>
      <dc:creator>tatianabkirillova</dc:creator>
      <dc:date>2023-07-03T08:47:11Z</dc:date>
    </item>
  </channel>
</rss>