<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8QM USB2.0 Compliance test in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1668850#M207553</link>
    <description>&lt;P&gt;For the&amp;nbsp;USB2.0 Compliance test you can refer to&amp;nbsp; &lt;A href="https://www.nxp.com/docs/en/application-note/AN12409.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12409.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Here I attach the guide for the i.MX8QXP/8QM.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jun 2023 03:39:04 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2023-06-14T03:39:04Z</dc:date>
    <item>
      <title>i.MX8QM USB2.0 Compliance test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1660498#M206848</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;We are developing a USB host device running Linux OS on iMX8QuadMax.&lt;/P&gt;&lt;P&gt;I want to test USB2.0 compliance tests to verify electrical characteristics.&lt;/P&gt;&lt;P&gt;I saw the following case,&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-USB2-0-Compliance-Test/m-p/1433090" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-USB2-0-Compliance-Test/m-p/1433090&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I have read AN12409. And I understood that in the USB 2.0 host test, the DUT (host) sets the PID corresponding to each test in the test fixture.&lt;/P&gt;&lt;P&gt;We outsource our compliance testing (its too expensive in the testing environment).&amp;nbsp;We need to ensure that the DUT is working correctly before we commission a test.&lt;/P&gt;&lt;P&gt;/We don't have test fixtures, so I guess we have to check the code. Is it a driver? Where can we look to see that it has been implemented correctly? And how can we check that the driver is enabled?&lt;BR /&gt;/Does the device tree limit this?&lt;BR /&gt;/Or do build options ever enable or disable test mode?&lt;BR /&gt;What can you check in advance to perform a compliance test on the USB 2.0 host device?&lt;/P&gt;&lt;P&gt;This is the same that should be checked when each test mode does not work in compliance test. Your help would be appreciated. Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yukio Oyama&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 06:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1660498#M206848</guid>
      <dc:creator>YukioOyama</dc:creator>
      <dc:date>2023-05-31T06:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QM USB2.0 Compliance test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1668850#M207553</link>
      <description>&lt;P&gt;For the&amp;nbsp;USB2.0 Compliance test you can refer to&amp;nbsp; &lt;A href="https://www.nxp.com/docs/en/application-note/AN12409.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12409.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Here I attach the guide for the i.MX8QXP/8QM.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 03:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1668850#M207553</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-06-14T03:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QM USB2.0 Compliance test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1668877#M207557</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think the "i.MX8_8X series USB Certification Guide" you attached seems to satisfy my question.&amp;nbsp;I will try the contents of this file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any new questions arise to me, I will ask them in a new thread. So I will close this case. Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yukio Oyama&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 04:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB2-0-Compliance-test/m-p/1668877#M207557</guid>
      <dc:creator>YukioOyama</dc:creator>
      <dc:date>2023-06-14T04:25:04Z</dc:date>
    </item>
  </channel>
</rss>