<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic We are not able see any gpio in  /sys/class/gpio/export for imx8x (MiMX8QX6AVLFZAC) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/We-are-not-able-see-any-gpio-in-sys-class-gpio-export-for-imx8x/m-p/1668522#M207521</link>
    <description>&lt;P&gt;When we try to do a ls on /sys/class/gpio it shows empty.&lt;BR /&gt;&lt;BR /&gt;We have attached dmesg log.&lt;BR /&gt;&lt;BR /&gt;We also included the libgpiod in the local.conf file.&lt;BR /&gt;&lt;BR /&gt;IMAGE_INSTALL:append = " libgpiod"&lt;/P&gt;&lt;P&gt;When we try to issue "gpiodetect" it shows unknown command&lt;BR /&gt;&lt;BR /&gt;Please help us to access /sys/class/gpio&amp;nbsp; or libgpiod ?&lt;/P&gt;</description>
    <pubDate>Thu, 15 Jun 2023 13:47:52 GMT</pubDate>
    <dc:creator>kishorem</dc:creator>
    <dc:date>2023-06-15T13:47:52Z</dc:date>
    <item>
      <title>We are not able see any gpio in  /sys/class/gpio/export for imx8x (MiMX8QX6AVLFZAC)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/We-are-not-able-see-any-gpio-in-sys-class-gpio-export-for-imx8x/m-p/1668522#M207521</link>
      <description>&lt;P&gt;When we try to do a ls on /sys/class/gpio it shows empty.&lt;BR /&gt;&lt;BR /&gt;We have attached dmesg log.&lt;BR /&gt;&lt;BR /&gt;We also included the libgpiod in the local.conf file.&lt;BR /&gt;&lt;BR /&gt;IMAGE_INSTALL:append = " libgpiod"&lt;/P&gt;&lt;P&gt;When we try to issue "gpiodetect" it shows unknown command&lt;BR /&gt;&lt;BR /&gt;Please help us to access /sys/class/gpio&amp;nbsp; or libgpiod ?&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 13:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/We-are-not-able-see-any-gpio-in-sys-class-gpio-export-for-imx8x/m-p/1668522#M207521</guid>
      <dc:creator>kishorem</dc:creator>
      <dc:date>2023-06-15T13:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: We are not able see any gpio in  /sys/class/gpio/export for imx8x (MiMX8QX6AVLFZAC)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/We-are-not-able-see-any-gpio-in-sys-class-gpio-export-for-imx8x/m-p/1673735#M207962</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Based on your information the problem could be that you are not setting the device tree properly. Please have a look at the following link. Here you will find how to correctly set the device tree to use a GPIO.&lt;/P&gt;
&lt;P&gt;Link:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Toggle-pin-on-i-MX-8M-Mini-Applications-Processor-Evaluation-Kit/ta-p/1418588" target="_blank"&gt;Toggle pin on i.MX 8M Mini Applications Processor ... - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope this information will be helpful.&lt;/P&gt;
&lt;P&gt;Have a great day!&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 15:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/We-are-not-able-see-any-gpio-in-sys-class-gpio-export-for-imx8x/m-p/1673735#M207962</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-06-21T15:15:05Z</dc:date>
    </item>
  </channel>
</rss>