<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMXRT1024-EVK Ethernet CRS Routing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1024-EVK-Ethernet-CRS-Routing/m-p/1666294#M207330</link>
    <description>&lt;P&gt;On the EVK for the xx1024, the schematic shows the ENET_CRS_DV pin being routed from the PHY (U11) to the CPU on pin 97 (GPIO_AD_B0_11). The reference manual (p261) says that the ENET_CRS signal must be routed to GPIO_EMC_34.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this an error in the eval board? Which pin should this signal be routed to?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jun 2023 15:31:00 GMT</pubDate>
    <dc:creator>GUnderdown</dc:creator>
    <dc:date>2023-06-08T15:31:00Z</dc:date>
    <item>
      <title>IMXRT1024-EVK Ethernet CRS Routing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1024-EVK-Ethernet-CRS-Routing/m-p/1666294#M207330</link>
      <description>&lt;P&gt;On the EVK for the xx1024, the schematic shows the ENET_CRS_DV pin being routed from the PHY (U11) to the CPU on pin 97 (GPIO_AD_B0_11). The reference manual (p261) says that the ENET_CRS signal must be routed to GPIO_EMC_34.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this an error in the eval board? Which pin should this signal be routed to?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 15:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1024-EVK-Ethernet-CRS-Routing/m-p/1666294#M207330</guid>
      <dc:creator>GUnderdown</dc:creator>
      <dc:date>2023-06-08T15:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024-EVK Ethernet CRS Routing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1024-EVK-Ethernet-CRS-Routing/m-p/1667445#M207422</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;From RT1024 reference manual page1734 Table 37-44 ENET External Signals description:&lt;/P&gt;
&lt;P&gt;ENET_CRS (GPIO_EMS_34 pad) signal only works for MII mode:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hui_Ma_0-1686553108337.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227134iDAAFBAFAF8E36786/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Hui_Ma_0-1686553108337.png" alt="Hui_Ma_0-1686553108337.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;RT1024 EVK board ENET works at RMII mode, which using RX_EN (GPIO_AD_B0_11 pad) signal as CRS_DV input signal.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hui_Ma_1-1686553272229.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227135i31D9CE3A31238ACF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Hui_Ma_1-1686553272229.png" alt="Hui_Ma_1-1686553272229.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, the RT1024 EVK board ENET_CRS_DV connection is correct.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jun 2023 07:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1024-EVK-Ethernet-CRS-Routing/m-p/1667445#M207422</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-06-12T07:03:06Z</dc:date>
    </item>
  </channel>
</rss>