<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: UUU under windows 10 64 bit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1665437#M207279</link>
    <description>&lt;P&gt;Have u tested to run uuu with some extra parameters?&lt;/P&gt;&lt;P&gt;-v&amp;nbsp; &amp;nbsp;verbose with more screen output. -V should print put more libusb messages&lt;/P&gt;&lt;P&gt;-t Timeout seconds waiting for known usb devices&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-T timeout seconds for wait next known usb devices at stage switch (this option might fix your problem)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-pp usb polling period milliseconds&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jun 2023 19:15:38 GMT</pubDate>
    <dc:creator>boyak75</dc:creator>
    <dc:date>2023-06-07T19:15:38Z</dc:date>
    <item>
      <title>UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032615#M152467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;libuuu_1.3.134-0-g0b47f4d&lt;/P&gt;&lt;P&gt;I am using UUU to flash my iMX8M mini eMMC using:&lt;/P&gt;&lt;P&gt;uuu -b emmc_all imx-boot-imx8mmwasp-emmc.bin fsl-image-qt5-imx8mmwasp.sdcard.bz2/*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This works just fine on my laptop (Windows 10 64bit).&lt;/P&gt;&lt;P&gt;But on another PC (the one I really need to use) ...also Windows 10 64bit it appears to start and makes it through the initial procedure programming the bootloader then makes it SDPV boot jump&lt;/P&gt;&lt;P&gt;then I get:&lt;/P&gt;&lt;P&gt;2:514 1/ 0 [Failure open usb device]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is going on?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Feb 2020 11:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032615#M152467</guid>
      <dc:creator>davidvescovi</dc:creator>
      <dc:date>2020-02-29T11:07:18Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032616#M152468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls check if "Human Interface Devices" detected the new device in the "Device Manager" when you connect board to the PC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 07:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032616#M152468</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-03-02T07:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032617#M152469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;did you not understand the question? It attaches and works fine through the first part of the programming it's only the second part where it apparently forces a reboot then downloads the rest. I bet its some timing issue where UUU is not waiting long enough for the host to reattach or something.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 06:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032617#M152469</guid>
      <dc:creator>davidvescovi</dc:creator>
      <dc:date>2020-03-06T06:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032618#M152470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems your PC doesn't recognized the board when jump, that's why I asked you to checking the device manager, this shouldn't be a uuu tool issue, I don't know if&amp;nbsp; your PC has usb driver issue, maybe you can send the log file to me, I tested download image to board by uuu on my windows10 64bits laptop successfully, but I don't use the same command as yours&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 09:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1032618#M152470</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-03-06T09:48:13Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1651244#M205962</link>
      <description>Does anyone have a solution for this issue?&lt;BR /&gt;I have the same issue, but I am 100% that it worked before and now since a few weeks it fails with exectly the same error.&lt;BR /&gt;Is that probably caused by a Windows Update?</description>
      <pubDate>Tue, 16 May 2023 13:47:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1651244#M205962</guid>
      <dc:creator>schumi_x</dc:creator>
      <dc:date>2023-05-16T13:47:46Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1661647#M206924</link>
      <description>&lt;P&gt;Any ideas why this happens on some Windows Installations (after a while)?&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 08:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1661647#M206924</guid>
      <dc:creator>schumi_x</dc:creator>
      <dc:date>2023-06-01T08:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1665437#M207279</link>
      <description>&lt;P&gt;Have u tested to run uuu with some extra parameters?&lt;/P&gt;&lt;P&gt;-v&amp;nbsp; &amp;nbsp;verbose with more screen output. -V should print put more libusb messages&lt;/P&gt;&lt;P&gt;-t Timeout seconds waiting for known usb devices&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-T timeout seconds for wait next known usb devices at stage switch (this option might fix your problem)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-pp usb polling period milliseconds&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 19:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1665437#M207279</guid>
      <dc:creator>boyak75</dc:creator>
      <dc:date>2023-06-07T19:15:38Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1679486#M208420</link>
      <description>Hi schumi_x, have you sloved it yet? can you help me?</description>
      <pubDate>Fri, 30 Jun 2023 09:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1679486#M208420</guid>
      <dc:creator>thinhses</dc:creator>
      <dc:date>2023-06-30T09:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: UUU under windows 10 64 bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1679494#M208422</link>
      <description>Solution: &lt;A href="https://github.com/nxpfrankli/mfgtoolwiki/blob/master/How-to-use-UUU-on-Windows.md" target="_blank"&gt;https://github.com/nxpfrankli/mfgtoolwiki/blob/master/How-to-use-UUU-on-Windows.md&lt;/A&gt;&lt;BR /&gt;1. Turn on the board&lt;BR /&gt;Connect the USB power supply to the J302 connector (the USB Type-C POWER connector)&lt;BR /&gt;Connect the USB Type-C cable to the serial download connector (J301) to the host machine&lt;BR /&gt;Connect the serial debug (connector J901) to the host machine using a USB micro-B cable&lt;BR /&gt;Set the boot mode switches to the Download Mode (see sticker or silk on the board)&lt;BR /&gt;Turn on the board on ON/OFF switch (SW101)&lt;BR /&gt;2. Open CMD&lt;BR /&gt;3. Navigate to the folder with the uuu.exe, uuu.auto, libusb-1.0.dll, and the images to be installed on the target.&lt;BR /&gt;4. Execute uuu.exe</description>
      <pubDate>Fri, 30 Jun 2023 09:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-under-windows-10-64-bit/m-p/1679494#M208422</guid>
      <dc:creator>thinhses</dc:creator>
      <dc:date>2023-06-30T09:29:50Z</dc:date>
    </item>
  </channel>
</rss>