<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mp uuu emmc failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1664217#M207175</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP Jorge7u7,&amp;nbsp;&lt;/P&gt;&lt;P&gt;uuu -b emmc_all flash.bin u-boot.bin&lt;/P&gt;&lt;P&gt;It seems the build-in script will flash the u-boot to the use partition at offset 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;and burn flash.bin to the boot1 emmc boot partition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And the i.MX8MP bootloader is not u-boot only, it is combined by aft, ddr firmware, u-boot with checksum to make sure its integration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems could not direction replace the u-boot in flash.bin, which is wrapped by imx-mkimage, because of the crc.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To speak frankly, NXP Jorge7u7, your command is totally wrong. And the understanding of i.MX8MP bootloader(flash.bin) is totally wrong.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it is very basic knowledge for you NXP tech support.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;uuu -bshow emmc_all&lt;BR /&gt;uuu_version 1.4.149&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;FB: flash -raw2sparse all _image&lt;BR /&gt;FB: flash -scanterm -scanlimited 0x800000 bootloader _flash.bin&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jun 2023 10:04:05 GMT</pubDate>
    <dc:creator>smithcoba</dc:creator>
    <dc:date>2023-06-06T10:04:05Z</dc:date>
    <item>
      <title>imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1661902#M206948</link>
      <description>&lt;P&gt;hi nxp,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I am a fresher to imx8mp evk board, and i download yocto branch zeus to compile a version of uboot 2020.04 branch , but i find that i can not flash my emmc to bring my board up. the specific operation steps are as follows.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;step1 ,sudo uuu -b emmc imx-boot-imx8mpevk-sd.bin-flash_evk&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuzhu_0-1685623390625.png" style="width: 735px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/225875iED5F741866C35DE1/image-dimensions/735x136?v=v2" width="735" height="136" role="button" title="xuzhu_0-1685623390625.png" alt="xuzhu_0-1685623390625.png" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;LI&gt;step 2 , my serial port print info ,&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee801e (May 25 2023 - 05:07:48 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;Find FIT header 0x&amp;amp;480331a0, size 1031&lt;BR /&gt;Need continue download 1024&lt;BR /&gt;Download 3023360, total fit 3024992&lt;BR /&gt;NOTICE: BL31: v2.2(release):rel_imx_5.4.70_2.3.0-0-gf1d7187f2&lt;BR /&gt;NOTICE: BL31: Built : 05:33:04, May 25 2023&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (May 25 2023 - 05:07:48 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 34C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MPlus LPDDR4 EVK board&lt;BR /&gt;DRAM: 6 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@32e80000, video&lt;BR /&gt;[1] mipi_dsi@32e60000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF f1d7187&lt;BR /&gt;- U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net:&lt;BR /&gt;Error: ethernet@30be0000 address not set.&lt;/P&gt;&lt;P&gt;Error: ethernet@30be0000 address not set.&lt;/P&gt;&lt;P&gt;Error: ethernet@30bf0000 address not set.&lt;/P&gt;&lt;P&gt;Error: ethernet@30bf0000 address not set.&lt;BR /&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;*** Warning - Use default environment for mfgtools&lt;BR /&gt;, using default environment&lt;/P&gt;&lt;P&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 43800000 ...&lt;BR /&gt;Unknown image format!&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;USB init failed: -22&lt;BR /&gt;u-boot=&amp;gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;And My Questions is that uuu cmd not burn in my uboot compiled ? how can i burn the uboot into the emmc on my boards?&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Thu, 01 Jun 2023 12:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1661902#M206948</guid>
      <dc:creator>HelloMather</dc:creator>
      <dc:date>2023-06-01T12:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1661940#M206951</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;The logs show that you are on U-boot.&lt;/P&gt;
&lt;P&gt;To flash it, I suggest use the next command:&lt;/P&gt;
&lt;P&gt;uuu -b emmc_all &amp;lt;Your file name&amp;gt;.bin-flash_evk&lt;/P&gt;
&lt;P&gt;But on your logs, I can see that you are on U-boot.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;Jorge.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 14:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1661940#M206951</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-06-01T14:21:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1662258#M206964</link>
      <description>&lt;P&gt;thank for your reply.&lt;/P&gt;&lt;P&gt;yes i just only want to flash uboot, but actually uuu just send it to ram memory and finally report usb_init failed -22.&lt;/P&gt;&lt;P&gt;is that any place need to be configured or modifyed?&lt;/P&gt;&lt;P&gt;do you encounter similar problems or any directional suggestions can&amp;nbsp; be given?&lt;/P&gt;&lt;P&gt;thank you so much.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 01:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1662258#M206964</guid>
      <dc:creator>HelloMather</dc:creator>
      <dc:date>2023-06-02T01:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1662824#M207023</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It is not needed to modify, using the command on my last post should be enough.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want to try, you can flash U-boot with the next command and attached files:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;uuu -b emmc_all flash.bin u-boot.bin   &lt;/LI-CODE&gt;
&lt;P&gt;But I think you will get the same result, also I will attach the log that I got.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;Jorge.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 18:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1662824#M207023</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-06-02T18:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1663090#M207050</link>
      <description>&lt;P&gt;thank you so much.&lt;/P&gt;&lt;P&gt;yes i get the same error as before. so i enable the DEBUG macro in boot source and capture the more detail message info as attachments.&lt;/P&gt;&lt;P&gt;the difference between your print and mine are mainly:&lt;/P&gt;&lt;P&gt;......&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;switch to partitions #0, OK&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;mmc2(part 0) is current device&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;flash target is MMC:2&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;Net: eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;Fastboot: Normal&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;Normal Boot&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;Hit any key to stop autoboot: 0&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and mine are:&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&lt;STRIKE&gt;Command failed, result=1&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;Run fastboot ...&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;USB init failed: -22&lt;/STRIKE&gt;&lt;BR /&gt;&lt;STRIKE&gt;Command failed, result=1&lt;/STRIKE&gt;&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;could you help me analyze the reason for this difference?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 02:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1663090#M207050</guid>
      <dc:creator>HelloMather</dc:creator>
      <dc:date>2023-06-05T02:39:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1663100#M207052</link>
      <description>&lt;P&gt;here is my test bin&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 02:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1663100#M207052</guid>
      <dc:creator>HelloMather</dc:creator>
      <dc:date>2023-06-05T02:49:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp uuu emmc failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1664217#M207175</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP Jorge7u7,&amp;nbsp;&lt;/P&gt;&lt;P&gt;uuu -b emmc_all flash.bin u-boot.bin&lt;/P&gt;&lt;P&gt;It seems the build-in script will flash the u-boot to the use partition at offset 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;and burn flash.bin to the boot1 emmc boot partition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And the i.MX8MP bootloader is not u-boot only, it is combined by aft, ddr firmware, u-boot with checksum to make sure its integration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems could not direction replace the u-boot in flash.bin, which is wrapped by imx-mkimage, because of the crc.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To speak frankly, NXP Jorge7u7, your command is totally wrong. And the understanding of i.MX8MP bootloader(flash.bin) is totally wrong.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it is very basic knowledge for you NXP tech support.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;uuu -bshow emmc_all&lt;BR /&gt;uuu_version 1.4.149&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;FB: flash -raw2sparse all _image&lt;BR /&gt;FB: flash -scanterm -scanlimited 0x800000 bootloader _flash.bin&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 10:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-uuu-emmc-failed/m-p/1664217#M207175</guid>
      <dc:creator>smithcoba</dc:creator>
      <dc:date>2023-06-06T10:04:05Z</dc:date>
    </item>
  </channel>
</rss>