<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック[iMX8M Plus] Adding machine learning libraries to Yocto reduced firmware image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-Adding-machine-learning-libraries-to-Yocto-reduced/m-p/1663017#M207045</link>
    <description>&lt;P&gt;Dear Community,&lt;/P&gt;&lt;P&gt;I would like to know what is the necessary modification for the &lt;STRONG&gt;conf/local.conf&lt;/STRONG&gt; in order to add the machine learning libraries and stuff for purpose of deploying the AI features on the board without the need of bitbaking imx-image-full, please ? Differently saying, I would like to have a firmware as minimal as possible (for example without the GUI) but it still have enough libraries (ISP, VPU, NPU) for running vision based deep learning features on board.&lt;/P&gt;&lt;P&gt;Thanks in advance and best regards,&lt;/P&gt;&lt;P&gt;Khang&lt;/P&gt;</description>
    <pubDate>Sun, 04 Jun 2023 09:44:19 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2023-06-04T09:44:19Z</dc:date>
    <item>
      <title>[iMX8M Plus] Adding machine learning libraries to Yocto reduced firmware image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-Adding-machine-learning-libraries-to-Yocto-reduced/m-p/1663017#M207045</link>
      <description>&lt;P&gt;Dear Community,&lt;/P&gt;&lt;P&gt;I would like to know what is the necessary modification for the &lt;STRONG&gt;conf/local.conf&lt;/STRONG&gt; in order to add the machine learning libraries and stuff for purpose of deploying the AI features on the board without the need of bitbaking imx-image-full, please ? Differently saying, I would like to have a firmware as minimal as possible (for example without the GUI) but it still have enough libraries (ISP, VPU, NPU) for running vision based deep learning features on board.&lt;/P&gt;&lt;P&gt;Thanks in advance and best regards,&lt;/P&gt;&lt;P&gt;Khang&lt;/P&gt;</description>
      <pubDate>Sun, 04 Jun 2023 09:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-Adding-machine-learning-libraries-to-Yocto-reduced/m-p/1663017#M207045</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2023-06-04T09:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8M Plus] Adding machine learning libraries to Yocto reduced firmware image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-Adding-machine-learning-libraries-to-Yocto-reduced/m-p/1664076#M207158</link>
      <description>&lt;P&gt;did you refer to the user guide before?&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 07:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-Adding-machine-learning-libraries-to-Yocto-reduced/m-p/1664076#M207158</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-06-06T07:51:20Z</dc:date>
    </item>
  </channel>
</rss>