<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to boot Linux directly from UUU in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1661631#M206922</link>
    <description>&lt;P&gt;thank you for your reply. I will check the docs and give it a try.&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jun 2023 08:33:10 GMT</pubDate>
    <dc:creator>Ryo_Aoki</dc:creator>
    <dc:date>2023-06-01T08:33:10Z</dc:date>
    <item>
      <title>How to boot Linux directly from UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1653745#M206167</link>
      <description>&lt;P&gt;Hi community.&lt;/P&gt;&lt;P&gt;I am currently using an i.MX6 SabreAI board.&lt;BR /&gt;I want to boot linux directly from serial downloader mode without writing to emmc or QSPI or SD card.&lt;BR /&gt;Is such usage possible?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have already checked the following documents, but I do not understand the procedure.&lt;BR /&gt;whether it can be used in such a way&lt;BR /&gt;If possible, could you please tell me the command procedure?&lt;/P&gt;&lt;P&gt;　UUU (Universal Update Utility)Document　(uuu.pdf)&lt;BR /&gt;　&lt;A href="https://github.com/nxp-imx/mfgtools" target="_blank"&gt;https://github.com/nxp-imx/mfgtools&lt;/A&gt;&lt;BR /&gt;　LF5.15.71.2.2.0のLinuxUserGuide&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 09:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1653745#M206167</guid>
      <dc:creator>Ryo_Aoki</dc:creator>
      <dc:date>2023-05-19T09:28:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to boot Linux directly from UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1654077#M206197</link>
      <description>&lt;P&gt;i.mx6 can boot up from usb, you can refer to the old community link&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Booting-Linux-through-USB-on-the-i-MX6-sabre-sd-platform-in-a/ta-p/1104434" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Booting-Linux-through-USB-on-the-i-MX6-sabre-sd-platform-in-a/ta-p/1104434&lt;/A&gt;"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 20 May 2023 01:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1654077#M206197</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-05-20T01:30:36Z</dc:date>
    </item>
    <item>
      <title>Re: How to boot Linux directly from UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1661631#M206922</link>
      <description>&lt;P&gt;thank you for your reply. I will check the docs and give it a try.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 08:33:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-boot-Linux-directly-from-UUU/m-p/1661631#M206922</guid>
      <dc:creator>Ryo_Aoki</dc:creator>
      <dc:date>2023-06-01T08:33:10Z</dc:date>
    </item>
  </channel>
</rss>