<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPU libs issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1661498#M206915</link>
    <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;But since i am using the customized kernel based on&amp;nbsp; imx-linux-hardknott manifest with 5.10 kernel , So i have to use the same version BSP libs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;And also its working in the prebuild imx-linux-hardknott manifest image with libEGL.so.1.5.0, So I am expecting it work in the customized kernel also with libs libEGL.so.1.5.0 and libGLESv1 &amp;amp; libGLESv2 libs.&lt;/P&gt;&lt;P&gt;Please help to find the missing steps causing the segmentation fault with libEGL.1.50 or could be other reason.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rk&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jun 2023 05:51:22 GMT</pubDate>
    <dc:creator>rakesh3</dc:creator>
    <dc:date>2023-06-01T05:51:22Z</dc:date>
    <item>
      <title>GPU libs issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1660817#M206873</link>
      <description>&lt;P&gt;Hi team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the imx61sabresd board ,with imx-linux-hardknott manifest 5.10.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am getting the segmentation fault issue in running the qt application. I am suspecting to have wroung&amp;nbsp;&lt;/P&gt;&lt;P&gt;libCLC.so&lt;BR /&gt;libGAL.so&lt;BR /&gt;libGLES_CL.so.1.1.0&lt;BR /&gt;libGLES_CM.so.1.1.0&lt;BR /&gt;libGLESv1_CL.so.1.1.0&lt;BR /&gt;libEGL.so.1.5.0&lt;BR /&gt;libGLESv1_CM.so.1.1.0&lt;BR /&gt;libGLESv2.so.2.0.0&lt;BR /&gt;libGLSLC.so&lt;BR /&gt;libGL.so.1.2.0&lt;BR /&gt;libOpenCL.so.1.2.0&lt;BR /&gt;libOpenVG.2d.so.1.1.0&lt;BR /&gt;libOpenVG.3d.so.1.1.0&lt;BR /&gt;libVDK.so.1.2.0&lt;BR /&gt;libVSC.so&lt;BR /&gt;libGLES_CL.so -&amp;gt; libGLES_CL.so.1.1.0&lt;BR /&gt;libGLES_CL.so.1 -&amp;gt; libGLES_CL.so.1.1.0&lt;BR /&gt;libGLES_CM.so -&amp;gt; libGLES_CM.so.1.1.0&lt;BR /&gt;libGLES_CM.so.1 -&amp;gt; libGLES_CM.so.1.1.0&lt;BR /&gt;libGLESv1_CL.so -&amp;gt; libGLESv1_CL.so.1.1.0&lt;BR /&gt;libGLESv1_CL.so.1 -&amp;gt; libGLESv1_CL.so.1.1.0&lt;BR /&gt;libGLESv1_CM.so -&amp;gt; libGLESv1_CM.so.1.1.0&lt;BR /&gt;libGLESv1_CM.so.1 -&amp;gt; libGLESv1_CM.so.1.1.0&lt;BR /&gt;libGLESv2.so -&amp;gt; libGLESv2.so.2.0.0&lt;BR /&gt;libGLESv2.so.2 -&amp;gt; libGLESv2.so.2.0.0&lt;BR /&gt;libGL.so -&amp;gt; libGL.so.1.2.0&lt;BR /&gt;libGL.so.1 -&amp;gt; libGL.so.1.2.0&lt;BR /&gt;libOpenCL.so -&amp;gt; libOpenCL.so.1.2.0&lt;BR /&gt;libOpenCL.so.1 -&amp;gt; libOpenCL.so.1.2.0&lt;BR /&gt;libOpenVG.so -&amp;gt; libOpenVG.3d.so.1.1.0&lt;BR /&gt;libOpenVG.so.1 -&amp;gt; libOpenVG.3d.so.1.1.0&lt;BR /&gt;libEGL.so -&amp;gt; libEGL.so.1.5.0&lt;BR /&gt;libEGL.so.1 -&amp;gt; libEGL.so.1.5.0&lt;BR /&gt;libVDK.so -&amp;gt; libVDK.so.1.2.0&lt;BR /&gt;libVDK.so.1 -&amp;gt; libVDK.so.1.2.0&lt;/P&gt;&lt;P&gt;Mostly i am getting the segmentation fault at EGL libs .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;below is my bb file of imx-gpu-viv&lt;/P&gt;&lt;P&gt;SRC_URI = "file://${PN}-${PV}-armhf.tar.gz \&lt;BR /&gt;file://debian \&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;SRC_URI[sha256sum] = "4e50fb2f13205ce84062f3bb70ae0b8453f7525f8725355cce3f71d1ce550f82"&lt;/P&gt;&lt;P&gt;S = "${WORKDIR}/${PN}-${PV}-armhf"&lt;/P&gt;&lt;P&gt;PROVIDES = " \&lt;BR /&gt;libclc-imx6q \&lt;BR /&gt;libegl-imx6q \&lt;BR /&gt;libgal-imx6q \&lt;BR /&gt;libgles-imx6q \&lt;BR /&gt;libgles2-imx6q \&lt;BR /&gt;libgl-imx6q \&lt;BR /&gt;libglslc-imx6q \&lt;BR /&gt;libopencl-imx6q \&lt;BR /&gt;libopenvg-imx6q \&lt;BR /&gt;libvdk-imx6q \&lt;BR /&gt;libvivante-dri-imx6q \&lt;BR /&gt;libvsc-imx6q \&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggestion on this issue to stop getting the upstream build and just use the nxp libs only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rk&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 13:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1660817#M206873</guid>
      <dc:creator>rakesh3</dc:creator>
      <dc:date>2023-05-31T13:07:04Z</dc:date>
    </item>
    <item>
      <title>Re: GPU libs issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1660939#M206882</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please download the 5.4.70 BSP from NXP, you must not have segmentation foult and QT.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 15:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1660939#M206882</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-05-31T15:38:33Z</dc:date>
    </item>
    <item>
      <title>Re: GPU libs issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1661498#M206915</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;But since i am using the customized kernel based on&amp;nbsp; imx-linux-hardknott manifest with 5.10 kernel , So i have to use the same version BSP libs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;And also its working in the prebuild imx-linux-hardknott manifest image with libEGL.so.1.5.0, So I am expecting it work in the customized kernel also with libs libEGL.so.1.5.0 and libGLESv1 &amp;amp; libGLESv2 libs.&lt;/P&gt;&lt;P&gt;Please help to find the missing steps causing the segmentation fault with libEGL.1.50 or could be other reason.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rk&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 05:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-libs-issue/m-p/1661498#M206915</guid>
      <dc:creator>rakesh3</dc:creator>
      <dc:date>2023-06-01T05:51:22Z</dc:date>
    </item>
  </channel>
</rss>