<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6 SD throughput rate</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SD-throughput-rate/m-p/1661175#M206893</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to use the Variscite DART6UL board for a project. It has the NXP i.MX 6 Ultralite ARM Cortex-A7 processor. I need to transfer data at 20MB/sec to a SD card.&lt;/P&gt;&lt;P&gt;Does anyone know if that kind of throughput rate is possible with the SD driver running and managing the file structure and writing operation to the SD FLASH memory?&lt;/P&gt;&lt;P&gt;I am concerned about the overhead the driver will impose on the overall data-rate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, am I correct in assuming the data can be moved under DMA from a parallel input port to the SD bus&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;</description>
    <pubDate>Wed, 31 May 2023 20:15:34 GMT</pubDate>
    <dc:creator>dfasano</dc:creator>
    <dc:date>2023-05-31T20:15:34Z</dc:date>
    <item>
      <title>iMX6 SD throughput rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SD-throughput-rate/m-p/1661175#M206893</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to use the Variscite DART6UL board for a project. It has the NXP i.MX 6 Ultralite ARM Cortex-A7 processor. I need to transfer data at 20MB/sec to a SD card.&lt;/P&gt;&lt;P&gt;Does anyone know if that kind of throughput rate is possible with the SD driver running and managing the file structure and writing operation to the SD FLASH memory?&lt;/P&gt;&lt;P&gt;I am concerned about the overhead the driver will impose on the overall data-rate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, am I correct in assuming the data can be moved under DMA from a parallel input port to the SD bus&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 20:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SD-throughput-rate/m-p/1661175#M206893</guid>
      <dc:creator>dfasano</dc:creator>
      <dc:date>2023-05-31T20:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SD throughput rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SD-throughput-rate/m-p/1661985#M206957</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope something of &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/44188"&gt;@variscite&lt;/a&gt; team will help.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 15:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SD-throughput-rate/m-p/1661985#M206957</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-06-01T15:34:33Z</dc:date>
    </item>
  </channel>
</rss>