<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RT1064 EVK programming</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1661162#M206890</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;You might use the onboard debug circuit but an external debugger is also an option.&lt;BR /&gt;1. Yes, configure the EVK with these settings:&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;Remove jumpers J47 and J48, to disconnect the SWD signals from onboard debug circuit, these jumpers are installed by default.&lt;/LI&gt;
&lt;LI&gt;Use default power selection on J1 with pins 5-6 shorted.&lt;/LI&gt;
&lt;LI&gt;Connect the probe to J21, 20-pin dual-row 0.1" header.&lt;/LI&gt;
&lt;LI&gt;Power the EVK with one of the power supply options.&amp;nbsp; Typically USB connector J41 is used to power the board and provides a UART/USB bridge through the onboard debug circuit.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;2. Not necessarily, this option of serial download can be used when your board is bricked but you might use the onboard debugger with J41 and boot mode on internal boot.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 31 May 2023 20:08:07 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2023-05-31T20:08:07Z</dc:date>
    <item>
      <title>RT1064 EVK programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1659280#M206750</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just got RT1064-EVK to try to evaluate the functions for my application.&lt;/P&gt;&lt;P&gt;Before I use P&amp;amp;E Multilink Universal to program the MCU flash for MK66 and KV58 MCU by using MCUXpresso.&lt;/P&gt;&lt;P&gt;My question:&lt;/P&gt;&lt;P&gt;1) Can I use P&amp;amp;E Multilink Universal to program RT1064 QSPI Flash on chip?&lt;/P&gt;&lt;P&gt;2) If not, which tool can I use to program RT1064 QSPI flash?&lt;/P&gt;&lt;P&gt;2) Do I have to use USB/RS232 to program the RT1064 QSPI Flash? If so, do I need to switch the boot mode every time because I want to use default mode(boot from QSPI Flash)?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Mon, 29 May 2023 18:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1659280#M206750</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2023-05-29T18:51:40Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 EVK programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1661162#M206890</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;You might use the onboard debug circuit but an external debugger is also an option.&lt;BR /&gt;1. Yes, configure the EVK with these settings:&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;Remove jumpers J47 and J48, to disconnect the SWD signals from onboard debug circuit, these jumpers are installed by default.&lt;/LI&gt;
&lt;LI&gt;Use default power selection on J1 with pins 5-6 shorted.&lt;/LI&gt;
&lt;LI&gt;Connect the probe to J21, 20-pin dual-row 0.1" header.&lt;/LI&gt;
&lt;LI&gt;Power the EVK with one of the power supply options.&amp;nbsp; Typically USB connector J41 is used to power the board and provides a UART/USB bridge through the onboard debug circuit.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;2. Not necessarily, this option of serial download can be used when your board is bricked but you might use the onboard debugger with J41 and boot mode on internal boot.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 20:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1661162#M206890</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-05-31T20:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 EVK programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1661169#M206891</link>
      <description>&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Here is what I tested, can you tell where I am wrong?&lt;/P&gt;&lt;P&gt;I trying to test RT1064-EVK and have the following issues:&lt;/P&gt;&lt;P&gt;I am using P&amp;amp;E multilink universal to program LED demo application to RT1064-EVK&lt;/P&gt;&lt;P&gt;1) If I use J21(20Pin connector) and remove J47, J48, I can program FlexSPI flash and run properly.&lt;/P&gt;&lt;P&gt;2) If I use&amp;nbsp;J34(10Pin connector) and remove J47, J48, I can't program FlexSPI flash and got the following error&lt;/P&gt;&lt;P&gt;"pegdbserver_console.exe" stop working.....&lt;/P&gt;&lt;P&gt;Can anybody help me to fix this issue?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 20:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1661169#M206891</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2023-05-31T20:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 EVK programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1662093#M206962</link>
      <description>&lt;P&gt;J34 is JTAG/SWD interface for the board debug circuit. If you try to attach a debugger, it will not connect to RT1064.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 18:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1064-EVK-programming/m-p/1662093#M206962</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-06-01T18:41:16Z</dc:date>
    </item>
  </channel>
</rss>