<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Implementing software for Cypress S71 Combo Multi-Chip</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Implementing-software-for-Cypress-S71-Combo-Multi-Chip/m-p/1659287#M206751</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;From my understanding, the device connected to RT1050 is an IC that contains HyperFlash and HyperRAM correct?&lt;BR /&gt;If both memories are connected to the same FlexSPI interface then there are issues when you access both devices at the same time.&lt;BR /&gt;To avoid this, I suggest you execute the code in the internal RAM so the XIP in Flash does not collide with HyperRAM.&lt;/P&gt;
&lt;P&gt;These application notes might be helpful: &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12239.pdf" target="_blank"&gt;How to Enable HyperRAM with i.MX RT (nxp.com)&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13028.pdf" target="_blank"&gt;Advanced HyperRAM/PSRAM Usage on i.MX RT (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 29 May 2023 19:20:08 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2023-05-29T19:20:08Z</dc:date>
    <item>
      <title>Implementing software for Cypress S71 Combo Multi-Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Implementing-software-for-Cypress-S71-Combo-Multi-Chip/m-p/1658478#M206653</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm currently working on the flexspi interface between an I.mx RT1052 and a hyperbus combo device (Infineon S71 - 1,8V - 512Mb HyperFLASH, 64Mb HyperRAM). The board was originally equipped with a hyperFLASH, but was modified to accept a combo chip.&lt;/P&gt;&lt;P&gt;Unfortunately, I can't figure out how to make the chip function correctly. I can access and boot from the hyperflash, but was wondering how to Read/Write in the HyperRAM.&lt;/P&gt;&lt;P&gt;What are the setup steps for the combo chips? Which files do I have to alter to switch from a simple hyperFLASH chip to the combo?&lt;/P&gt;&lt;P&gt;Also, is there an application note somewhere concerning implementation of the MCPs?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 14:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Implementing-software-for-Cypress-S71-Combo-Multi-Chip/m-p/1658478#M206653</guid>
      <dc:creator>dsonderer</dc:creator>
      <dc:date>2023-05-26T14:29:44Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing software for Cypress S71 Combo Multi-Chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Implementing-software-for-Cypress-S71-Combo-Multi-Chip/m-p/1659287#M206751</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;From my understanding, the device connected to RT1050 is an IC that contains HyperFlash and HyperRAM correct?&lt;BR /&gt;If both memories are connected to the same FlexSPI interface then there are issues when you access both devices at the same time.&lt;BR /&gt;To avoid this, I suggest you execute the code in the internal RAM so the XIP in Flash does not collide with HyperRAM.&lt;/P&gt;
&lt;P&gt;These application notes might be helpful: &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12239.pdf" target="_blank"&gt;How to Enable HyperRAM with i.MX RT (nxp.com)&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13028.pdf" target="_blank"&gt;Advanced HyperRAM/PSRAM Usage on i.MX RT (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 29 May 2023 19:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Implementing-software-for-Cypress-S71-Combo-Multi-Chip/m-p/1659287#M206751</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2023-05-29T19:20:08Z</dc:date>
    </item>
  </channel>
</rss>