<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reduce RAM usage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reduce-RAM-usage/m-p/1659179#M206735</link>
    <description>&lt;DIV&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217965"&gt;@himanshubhavani&lt;/a&gt;&amp;nbsp;,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I hope you are doing well.&lt;BR /&gt;&lt;BR /&gt;One can try removing unused reserved memory nodes in the device tree if present.&lt;BR /&gt;&lt;BR /&gt;One can add the below option in the kernel configuration.&lt;BR /&gt;&lt;BR /&gt;CONFIG_CC_OPTIMIZE_FOR_SIZE=y&lt;BR /&gt;&lt;BR /&gt;Please try to get more information about various processes using the below command.&lt;BR /&gt;&lt;BR /&gt;# top&lt;BR /&gt;# ps aux&lt;BR /&gt;&lt;BR /&gt;However, with Wayland build it seems to be normal memory usage.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards,&lt;/DIV&gt;&lt;DIV&gt;Sanket Parekh&lt;/DIV&gt;</description>
    <pubDate>Mon, 29 May 2023 12:07:51 GMT</pubDate>
    <dc:creator>Sanket_Parekh</dc:creator>
    <dc:date>2023-05-29T12:07:51Z</dc:date>
    <item>
      <title>Reduce RAM usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reduce-RAM-usage/m-p/1658735#M206689</link>
      <description>&lt;DIV class=""&gt;&lt;P&gt;Board : iMX6 Quad with 1GB RAM&lt;BR /&gt;Build environment : Yocto-Zeus&lt;BR /&gt;Kernel : 5.4&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX6 Quad 1GB board with x-wayland.&lt;BR /&gt;I have observe the 220MB RAM usage at starting without launching any application.&lt;BR /&gt;I would like to reduce RAM consumption.&lt;BR /&gt;What could be the possible approaches to do that?&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Sun, 28 May 2023 08:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reduce-RAM-usage/m-p/1658735#M206689</guid>
      <dc:creator>himanshubhavani</dc:creator>
      <dc:date>2023-05-28T08:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: Reduce RAM usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reduce-RAM-usage/m-p/1659179#M206735</link>
      <description>&lt;DIV&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217965"&gt;@himanshubhavani&lt;/a&gt;&amp;nbsp;,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I hope you are doing well.&lt;BR /&gt;&lt;BR /&gt;One can try removing unused reserved memory nodes in the device tree if present.&lt;BR /&gt;&lt;BR /&gt;One can add the below option in the kernel configuration.&lt;BR /&gt;&lt;BR /&gt;CONFIG_CC_OPTIMIZE_FOR_SIZE=y&lt;BR /&gt;&lt;BR /&gt;Please try to get more information about various processes using the below command.&lt;BR /&gt;&lt;BR /&gt;# top&lt;BR /&gt;# ps aux&lt;BR /&gt;&lt;BR /&gt;However, with Wayland build it seems to be normal memory usage.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards,&lt;/DIV&gt;&lt;DIV&gt;Sanket Parekh&lt;/DIV&gt;</description>
      <pubDate>Mon, 29 May 2023 12:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reduce-RAM-usage/m-p/1659179#M206735</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-05-29T12:07:51Z</dc:date>
    </item>
  </channel>
</rss>